Represents a Network Diagnostic Connectivity value.

Public Attributes#

int8_t

The priority of the sender as a parent.

uint8_t

Number of neighbors with link of quality 3.

uint8_t

Number of neighbors with link of quality 2.

uint8_t

Number of neighbors with link of quality 1.

uint8_t

Cost to the Leader.

uint8_t

Most recent received ID seq number.

uint8_t

Number of active routers.

uint16_t

Buffer capacity in bytes for SEDs. Optional.

uint8_t

Queue capacity (number of IPv6 datagrams) per SED. Optional.

Public Attribute Documentation#

mParentPriority#

int8_t otNetworkDiagConnectivity::mParentPriority

The priority of the sender as a parent.


Definition at line 98 of file include/openthread/netdiag.h

mLinkQuality3#

uint8_t otNetworkDiagConnectivity::mLinkQuality3

Number of neighbors with link of quality 3.


Definition at line 99 of file include/openthread/netdiag.h

mLinkQuality2#

uint8_t otNetworkDiagConnectivity::mLinkQuality2

Number of neighbors with link of quality 2.


Definition at line 100 of file include/openthread/netdiag.h

mLinkQuality1#

uint8_t otNetworkDiagConnectivity::mLinkQuality1

Number of neighbors with link of quality 1.


Definition at line 101 of file include/openthread/netdiag.h

mLeaderCost#

uint8_t otNetworkDiagConnectivity::mLeaderCost

Cost to the Leader.


Definition at line 102 of file include/openthread/netdiag.h

mIdSequence#

uint8_t otNetworkDiagConnectivity::mIdSequence

Most recent received ID seq number.


Definition at line 103 of file include/openthread/netdiag.h

mActiveRouters#

uint8_t otNetworkDiagConnectivity::mActiveRouters

Number of active routers.


Definition at line 104 of file include/openthread/netdiag.h

mSedBufferSize#

uint16_t otNetworkDiagConnectivity::mSedBufferSize

Buffer capacity in bytes for SEDs. Optional.


Definition at line 105 of file include/openthread/netdiag.h

mSedDatagramCount#

uint8_t otNetworkDiagConnectivity::mSedDatagramCount

Queue capacity (number of IPv6 datagrams) per SED. Optional.


Definition at line 106 of file include/openthread/netdiag.h