Toolchain#

This module defines a toolchain abstraction layer through macros.

Usage:

typedef
OT_TOOL_PACKED_BEGIN
struct
{
    char mField1;
    union
    {
        char mField2;
        long mField3;
    } OT_TOOL_PACKED_FIELD;
} OT_TOOL_PACKED_END packed_struct_t;

Macros#

#define

Compiler-specific indication that a class or enum must be used when it is the return value of a function.

#define

Compiler-specific indication that a class or struct must be byte packed.

#define

Indicate to the compiler a nested struct or union to be packed within byte packed class or struct.

#define
OT_TOOL_WEAK undefined

Compiler-specific weak symbol modifier.

#define
OT_TOOL_PRINTF_STYLE_FORMAT_ARG_CHECK (aFmtIndex, aStartIndex)

Specifies that a function or method takes printf style arguments and should be type-checked against a format string.

#define

Suppress unused variable warning in specific toolchains.

#define

Suppress Unreachable code warning in specific toolchains.

#define
OT_FALL_THROUGH undefined

Suppress fall through warning in specific compiler.

Macro Definition Documentation#

OT_MUST_USE_RESULT#

#define OT_MUST_USE_RESULT

Compiler-specific indication that a class or enum must be used when it is the return value of a function.

Note

  • This is currently only available with clang (C++17 implements it as attribute [[nodiscard]]).

  • To suppress the 'unused-result' warning/error, please use the '-Wno-unused-result' compiler option.


Definition at line 82 of file include/openthread/platform/toolchain.h

OT_TOOL_PACKED_BEGIN#

#define OT_TOOL_PACKED_BEGIN

Compiler-specific indication that a class or struct must be byte packed.


Definition at line 177 of file include/openthread/platform/toolchain.h

OT_TOOL_PACKED_FIELD#

#define OT_TOOL_PACKED_FIELD

Indicate to the compiler a nested struct or union to be packed within byte packed class or struct.


Definition at line 178 of file include/openthread/platform/toolchain.h

OT_TOOL_WEAK#

#define OT_TOOL_WEAK

Compiler-specific weak symbol modifier.


Definition at line 180 of file include/openthread/platform/toolchain.h

OT_TOOL_PRINTF_STYLE_FORMAT_ARG_CHECK#

#define OT_TOOL_PRINTF_STYLE_FORMAT_ARG_CHECK

Specifies that a function or method takes printf style arguments and should be type-checked against a format string.

Must be added after the function/method declaration. For example:

void MyPrintf(void *aObject, const char *aFormat, ...) OT_TOOL_PRINTF_STYLE_FORMAT_ARG_CHECK(2, 3);

The two argument index values indicate format string and first argument to check against it. They start at index 1 for the first parameter in a function and at index 2 for the first parameter in a method.


Definition at line 182 of file include/openthread/platform/toolchain.h

OT_UNUSED_VARIABLE#

#define OT_UNUSED_VARIABLE
Value:
do \
{ \
(void)(VARIABLE); \
} while (false)

Suppress unused variable warning in specific toolchains.


Definition at line 253 of file include/openthread/platform/toolchain.h

OT_UNREACHABLE_CODE#

#define OT_UNREACHABLE_CODE
Value:
(CODE)

Suppress Unreachable code warning in specific toolchains.


Definition at line 259 of file include/openthread/platform/toolchain.h

OT_APPLE_IGNORE_GNU_FOLDING_CONSTANT#

#define OT_APPLE_IGNORE_GNU_FOLDING_CONSTANT
Value:
(...)

Definition at line 285 of file include/openthread/platform/toolchain.h

OT_FALL_THROUGH#

#define OT_FALL_THROUGH
Value:
do \
{ \
} while (false) /* fallthrough */

Suppress fall through warning in specific compiler.


Definition at line 301 of file include/openthread/platform/toolchain.h