Crypto - Platform#

This module includes the platform abstraction for Crypto.

Modules#

otCryptoKey

otCryptoContext

otPlatCryptoSha256Hash

otPlatCryptoEcdsaKeyPair

otPlatCryptoEcdsaPublicKey

otPlatCryptoEcdsaSignature

Enumerations#

enum
OT_CRYPTO_KEY_TYPE_RAW
OT_CRYPTO_KEY_TYPE_AES
OT_CRYPTO_KEY_TYPE_HMAC
OT_CRYPTO_KEY_TYPE_ECDSA
}

Defines the key types.

enum
OT_CRYPTO_KEY_ALG_VENDOR
OT_CRYPTO_KEY_ALG_AES_ECB
OT_CRYPTO_KEY_ALG_HMAC_SHA_256
OT_CRYPTO_KEY_ALG_ECDSA
}

Defines the key algorithms.

enum
@10 {
OT_CRYPTO_KEY_USAGE_NONE = 0
OT_CRYPTO_KEY_USAGE_EXPORT = 1 << 0
OT_CRYPTO_KEY_USAGE_ENCRYPT = 1 << 1
OT_CRYPTO_KEY_USAGE_DECRYPT = 1 << 2
OT_CRYPTO_KEY_USAGE_SIGN_HASH = 1 << 3
OT_CRYPTO_KEY_USAGE_VERIFY_HASH = 1 << 4
}

Defines the key usage flags.

enum
OT_CRYPTO_KEY_STORAGE_VOLATILE
OT_CRYPTO_KEY_STORAGE_PERSISTENT
}

Defines the key storage types.

Typedefs#

typedef uint32_t

This datatype represents the key reference.

typedef struct otCryptoKey
typedef struct otPlatCryptoSha256Hash

Represents a SHA-256 hash.

Functions#

void

Initialize the Crypto module.

otPlatCryptoImportKey(otCryptoKeyRef *aKeyRef, otCryptoKeyType aKeyType, otCryptoKeyAlgorithm aKeyAlgorithm, int aKeyUsage, otCryptoKeyStorage aKeyPersistence, const uint8_t *aKey, size_t aKeyLen)

Import a key into PSA ITS.

otPlatCryptoExportKey(otCryptoKeyRef aKeyRef, uint8_t *aBuffer, size_t aBufferLen, size_t *aKeyLen)

Export a key stored in PSA ITS.

otPlatCryptoDestroyKey(otCryptoKeyRef aKeyRef)

Destroy a key stored in PSA ITS.

bool
otPlatCryptoHasKey(otCryptoKeyRef aKeyRef)

Check if the key ref passed has an associated key in PSA ITS.

otPlatCryptoHmacSha256Init(otCryptoContext *aContext)

Initialize the HMAC operation.

otPlatCryptoHmacSha256Deinit(otCryptoContext *aContext)

Uninitialize the HMAC operation.

otPlatCryptoHmacSha256Start(otCryptoContext *aContext, const otCryptoKey *aKey)

Start HMAC operation.

otPlatCryptoHmacSha256Update(otCryptoContext *aContext, const void *aBuf, uint16_t aBufLength)

Update the HMAC operation with new input.

otPlatCryptoHmacSha256Finish(otCryptoContext *aContext, uint8_t *aBuf, size_t aBufLength)

Complete the HMAC operation.

otPlatCryptoAesInit(otCryptoContext *aContext)

Initialise the AES operation.

otPlatCryptoAesSetKey(otCryptoContext *aContext, const otCryptoKey *aKey)

Set the key for AES operation.

otPlatCryptoAesEncrypt(otCryptoContext *aContext, const uint8_t *aInput, uint8_t *aOutput)

Encrypt the given data.

otPlatCryptoAesFree(otCryptoContext *aContext)

Free the AES context.

otPlatCryptoHkdfInit(otCryptoContext *aContext)

Initialise the HKDF context.

otPlatCryptoHkdfExpand(otCryptoContext *aContext, const uint8_t *aInfo, uint16_t aInfoLength, uint8_t *aOutputKey, uint16_t aOutputKeyLength)

Perform HKDF Expand step.

otPlatCryptoHkdfExtract(otCryptoContext *aContext, const uint8_t *aSalt, uint16_t aSaltLength, const otCryptoKey *aInputKey)

Perform HKDF Extract step.

otPlatCryptoHkdfDeinit(otCryptoContext *aContext)

Uninitialize the HKDF context.

otPlatCryptoSha256Init(otCryptoContext *aContext)

Initialise the SHA-256 operation.

otPlatCryptoSha256Deinit(otCryptoContext *aContext)

Uninitialize the SHA-256 operation.

otPlatCryptoSha256Start(otCryptoContext *aContext)

Start SHA-256 operation.

otPlatCryptoSha256Update(otCryptoContext *aContext, const void *aBuf, uint16_t aBufLength)

Update SHA-256 operation with new input.

otPlatCryptoSha256Finish(otCryptoContext *aContext, uint8_t *aHash, uint16_t aHashSize)

Finish SHA-256 operation.

void

Initialize cryptographically-secure pseudorandom number generator (CSPRNG).

void

Deinitialize cryptographically-secure pseudorandom number generator (CSPRNG).

otPlatCryptoRandomGet(uint8_t *aBuffer, uint16_t aSize)

Fills a given buffer with cryptographically secure random bytes.

otPlatCryptoEcdsaGenerateKey(otPlatCryptoEcdsaKeyPair *aKeyPair)

Generate and populate the output buffer with a new ECDSA key-pair.

otPlatCryptoEcdsaGetPublicKey(const otPlatCryptoEcdsaKeyPair *aKeyPair, otPlatCryptoEcdsaPublicKey *aPublicKey)

Get the associated public key from the input context.

otPlatCryptoEcdsaSign(const otPlatCryptoEcdsaKeyPair *aKeyPair, const otPlatCryptoSha256Hash *aHash, otPlatCryptoEcdsaSignature *aSignature)

Calculate the ECDSA signature for a hashed message using the private key from the input context.

otPlatCryptoEcdsaVerify(const otPlatCryptoEcdsaPublicKey *aPublicKey, const otPlatCryptoSha256Hash *aHash, const otPlatCryptoEcdsaSignature *aSignature)

Use the key from the input context to verify the ECDSA signature of a hashed message.

otPlatCryptoEcdsaSignUsingKeyRef(otCryptoKeyRef aKeyRef, const otPlatCryptoSha256Hash *aHash, otPlatCryptoEcdsaSignature *aSignature)

Calculate the ECDSA signature for a hashed message using the Key reference passed.

otPlatCryptoEcdsaExportPublicKey(otCryptoKeyRef aKeyRef, otPlatCryptoEcdsaPublicKey *aPublicKey)

Get the associated public key from the key reference passed.

Generate and import a new ECDSA key-pair at reference passed.

otPlatCryptoEcdsaVerifyUsingKeyRef(otCryptoKeyRef aKeyRef, const otPlatCryptoSha256Hash *aHash, const otPlatCryptoEcdsaSignature *aSignature)

Use the keyref to verify the ECDSA signature of a hashed message.

otPlatCryptoPbkdf2GenerateKey(const uint8_t *aPassword, uint16_t aPasswordLen, const uint8_t *aSalt, uint16_t aSaltLen, uint32_t aIterationCounter, uint16_t aKeyLen, uint8_t *aKey)

Perform PKCS#5 PBKDF2 using CMAC (AES-CMAC-PRF-128).

Macros#

#define

Length of SHA256 hash (in bytes).

#define

Max buffer size (in bytes) for representing the EDCSA key-pair in DER format.

#define

Buffer size (in bytes) for representing the EDCSA public key.

#define

Buffer size (in bytes) for representing the EDCSA signature.

#define

Max PBKDF2 SALT length: salt prefix (6) + extended panid (8) + network name (16)

Enumeration Documentation#

otCryptoKeyType#

otCryptoKeyType

Defines the key types.

Enumerator
OT_CRYPTO_KEY_TYPE_RAW

Key Type: Raw Data.

OT_CRYPTO_KEY_TYPE_AES

Key Type: AES.

OT_CRYPTO_KEY_TYPE_HMAC

Key Type: HMAC.

OT_CRYPTO_KEY_TYPE_ECDSA

Key Type: ECDSA.


otCryptoKeyAlgorithm#

otCryptoKeyAlgorithm

Defines the key algorithms.

Enumerator
OT_CRYPTO_KEY_ALG_VENDOR

Key Algorithm: Vendor Defined.

OT_CRYPTO_KEY_ALG_AES_ECB

Key Algorithm: AES ECB.

OT_CRYPTO_KEY_ALG_HMAC_SHA_256

Key Algorithm: HMAC SHA-256.

OT_CRYPTO_KEY_ALG_ECDSA

Key Algorithm: ECDSA.


@10#

@10

Defines the key usage flags.

Enumerator
OT_CRYPTO_KEY_USAGE_NONE

Key Usage: Key Usage is empty.

OT_CRYPTO_KEY_USAGE_EXPORT

Key Usage: Key can be exported.

OT_CRYPTO_KEY_USAGE_ENCRYPT

Key Usage: Encryption (vendor defined).

OT_CRYPTO_KEY_USAGE_DECRYPT

Key Usage: AES ECB.

OT_CRYPTO_KEY_USAGE_SIGN_HASH

Key Usage: Sign Hash.

OT_CRYPTO_KEY_USAGE_VERIFY_HASH

Key Usage: Verify Hash.


otCryptoKeyStorage#

otCryptoKeyStorage

Defines the key storage types.

Enumerator
OT_CRYPTO_KEY_STORAGE_VOLATILE

Key Persistence: Key is volatile.

OT_CRYPTO_KEY_STORAGE_PERSISTENT

Key Persistence: Key is persistent.


Typedef Documentation#

otCryptoKeyRef#

typedef uint32_t otCryptoKeyRef

This datatype represents the key reference.


otCryptoKey#

typedef struct otCryptoKey otCryptoKey

otCryptoContext#

typedef struct otCryptoContext otCryptoContext

otPlatCryptoSha256Hash#

typedef struct otPlatCryptoSha256Hash otPlatCryptoSha256Hash

Represents a SHA-256 hash.


otPlatCryptoEcdsaKeyPair#

typedef struct otPlatCryptoEcdsaKeyPair otPlatCryptoEcdsaKeyPair

otPlatCryptoEcdsaPublicKey#

typedef struct otPlatCryptoEcdsaPublicKey otPlatCryptoEcdsaPublicKey

otPlatCryptoEcdsaSignature#

typedef struct otPlatCryptoEcdsaSignature otPlatCryptoEcdsaSignature

Variable Documentation#

OT_TOOL_PACKED_END#

OT_TOOL_PACKED_BEGIN struct otPlatCryptoEcdsaSignature OT_TOOL_PACKED_END

Function Documentation#

otPlatCryptoInit#

void otPlatCryptoInit (void )

Initialize the Crypto module.

Parameters
TypeDirectionArgument NameDescription
voidN/A

otPlatCryptoImportKey#

otError otPlatCryptoImportKey (otCryptoKeyRef * aKeyRef, otCryptoKeyType aKeyType, otCryptoKeyAlgorithm aKeyAlgorithm, int aKeyUsage, otCryptoKeyStorage aKeyPersistence, const uint8_t * aKey, size_t aKeyLen)

Import a key into PSA ITS.

Parameters
TypeDirectionArgument NameDescription
otCryptoKeyRef *[inout]aKeyRef

Pointer to the key ref to be used for crypto operations.

otCryptoKeyType[in]aKeyType

Key Type encoding for the key.

otCryptoKeyAlgorithm[in]aKeyAlgorithm

Key algorithm encoding for the key.

int[in]aKeyUsage

Key Usage encoding for the key (combinations of OT_CRYPTO_KEY_USAGE_*).

otCryptoKeyStorage[in]aKeyPersistence

Key Persistence for this key

const uint8_t *[in]aKey

Actual key to be imported.

size_t[in]aKeyLen

Length of the key to be imported.

Note

  • If OT_CRYPTO_KEY_STORAGE_PERSISTENT is passed for aKeyPersistence then aKeyRef is input and platform should use the given aKeyRef and MUST not change it.

If OT_CRYPTO_KEY_STORAGE_VOLATILE is passed for aKeyPersistence then aKeyRef is output, the initial value does not matter and platform API MUST update it to return the new key ref.

This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.


otPlatCryptoExportKey#

otError otPlatCryptoExportKey (otCryptoKeyRef aKeyRef, uint8_t * aBuffer, size_t aBufferLen, size_t * aKeyLen)

Export a key stored in PSA ITS.

Parameters
TypeDirectionArgument NameDescription
otCryptoKeyRef[in]aKeyRef

The key ref to be used for crypto operations.

uint8_t *[out]aBuffer

Pointer to the buffer where key needs to be exported.

size_t[in]aBufferLen

Length of the buffer passed to store the exported key.

size_t *[out]aKeyLen

Pointer to return the length of the exported key.

Note

  • This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.


otPlatCryptoDestroyKey#

otError otPlatCryptoDestroyKey (otCryptoKeyRef aKeyRef)

Destroy a key stored in PSA ITS.

Parameters
TypeDirectionArgument NameDescription
otCryptoKeyRef[in]aKeyRef

The key ref to be destroyed

Note

  • This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.


otPlatCryptoHasKey#

bool otPlatCryptoHasKey (otCryptoKeyRef aKeyRef)

Check if the key ref passed has an associated key in PSA ITS.

Parameters
TypeDirectionArgument NameDescription
otCryptoKeyRef[in]aKeyRef

The Key Ref to check.

Note

  • This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.


otPlatCryptoHmacSha256Init#

otError otPlatCryptoHmacSha256Init (otCryptoContext * aContext)

Initialize the HMAC operation.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for HMAC operation.

Note

  • The platform driver shall point the context to the correct object such as psa_mac_operation_t or mbedtls_md_context_t.


otPlatCryptoHmacSha256Deinit#

otError otPlatCryptoHmacSha256Deinit (otCryptoContext * aContext)

Uninitialize the HMAC operation.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for HMAC operation.


otPlatCryptoHmacSha256Start#

otError otPlatCryptoHmacSha256Start (otCryptoContext * aContext, const otCryptoKey * aKey)

Start HMAC operation.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for HMAC operation.

const otCryptoKey *[in]aKey

Key material to be used for HMAC operation.


otPlatCryptoHmacSha256Update#

otError otPlatCryptoHmacSha256Update (otCryptoContext * aContext, const void * aBuf, uint16_t aBufLength)

Update the HMAC operation with new input.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for HMAC operation.

const void *[in]aBuf

A pointer to the input buffer.

uint16_t[in]aBufLength

The length of aBuf in bytes.


otPlatCryptoHmacSha256Finish#

otError otPlatCryptoHmacSha256Finish (otCryptoContext * aContext, uint8_t * aBuf, size_t aBufLength)

Complete the HMAC operation.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for HMAC operation.

uint8_t *[out]aBuf

A pointer to the output buffer.

size_t[in]aBufLength

The length of aBuf in bytes.


otPlatCryptoAesInit#

otError otPlatCryptoAesInit (otCryptoContext * aContext)

Initialise the AES operation.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for AES operation.

Note

  • The platform driver shall point the context to the correct object such as psa_key_id or mbedtls_aes_context_t.


otPlatCryptoAesSetKey#

otError otPlatCryptoAesSetKey (otCryptoContext * aContext, const otCryptoKey * aKey)

Set the key for AES operation.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for AES operation.

const otCryptoKey *[out]aKey

Key to use for AES operation.


otPlatCryptoAesEncrypt#

otError otPlatCryptoAesEncrypt (otCryptoContext * aContext, const uint8_t * aInput, uint8_t * aOutput)

Encrypt the given data.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for AES operation.

const uint8_t *[in]aInput

Pointer to the input buffer.

uint8_t *[in]aOutput

Pointer to the output buffer.


otPlatCryptoAesFree#

otError otPlatCryptoAesFree (otCryptoContext * aContext)

Free the AES context.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for AES operation.


otPlatCryptoHkdfInit#

otError otPlatCryptoHkdfInit (otCryptoContext * aContext)

Initialise the HKDF context.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for HKDF operation.

Note

  • The platform driver shall point the context to the correct object such as psa_key_derivation_operation_t or HmacSha256::Hash


otPlatCryptoHkdfExpand#

otError otPlatCryptoHkdfExpand (otCryptoContext * aContext, const uint8_t * aInfo, uint16_t aInfoLength, uint8_t * aOutputKey, uint16_t aOutputKeyLength)

Perform HKDF Expand step.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Operation context for HKDF operation.

const uint8_t *[in]aInfo

Pointer to the Info sequence.

uint16_t[in]aInfoLength

Length of the Info sequence.

uint8_t *[out]aOutputKey

Pointer to the output Key.

uint16_t[in]aOutputKeyLength

Size of the output key buffer.


otPlatCryptoHkdfExtract#

otError otPlatCryptoHkdfExtract (otCryptoContext * aContext, const uint8_t * aSalt, uint16_t aSaltLength, const otCryptoKey * aInputKey)

Perform HKDF Extract step.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Operation context for HKDF operation.

const uint8_t *[in]aSalt

Pointer to the Salt for HKDF.

uint16_t[in]aSaltLength

Length of Salt.

const otCryptoKey *[in]aInputKey

Pointer to the input key.


otPlatCryptoHkdfDeinit#

otError otPlatCryptoHkdfDeinit (otCryptoContext * aContext)

Uninitialize the HKDF context.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for HKDF operation.


otPlatCryptoSha256Init#

otError otPlatCryptoSha256Init (otCryptoContext * aContext)

Initialise the SHA-256 operation.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for SHA-256 operation.

Note

  • The platform driver shall point the context to the correct object such as psa_hash_operation_t or mbedtls_sha256_context.


otPlatCryptoSha256Deinit#

otError otPlatCryptoSha256Deinit (otCryptoContext * aContext)

Uninitialize the SHA-256 operation.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for SHA-256 operation.


otPlatCryptoSha256Start#

otError otPlatCryptoSha256Start (otCryptoContext * aContext)

Start SHA-256 operation.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for SHA-256 operation.


otPlatCryptoSha256Update#

otError otPlatCryptoSha256Update (otCryptoContext * aContext, const void * aBuf, uint16_t aBufLength)

Update SHA-256 operation with new input.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for SHA-256 operation.

const void *[in]aBuf

A pointer to the input buffer.

uint16_t[in]aBufLength

The length of aBuf in bytes.


otPlatCryptoSha256Finish#

otError otPlatCryptoSha256Finish (otCryptoContext * aContext, uint8_t * aHash, uint16_t aHashSize)

Finish SHA-256 operation.

Parameters
TypeDirectionArgument NameDescription
otCryptoContext *[in]aContext

Context for SHA-256 operation.

uint8_t *[in]aHash

A pointer to the output buffer, where hash needs to be stored.

uint16_t[in]aHashSize

The length of aHash in bytes.


otPlatCryptoRandomInit#

void otPlatCryptoRandomInit (void )

Initialize cryptographically-secure pseudorandom number generator (CSPRNG).

Parameters
TypeDirectionArgument NameDescription
voidN/A

otPlatCryptoRandomDeinit#

void otPlatCryptoRandomDeinit (void )

Deinitialize cryptographically-secure pseudorandom number generator (CSPRNG).

Parameters
TypeDirectionArgument NameDescription
voidN/A

otPlatCryptoRandomGet#

otError otPlatCryptoRandomGet (uint8_t * aBuffer, uint16_t aSize)

Fills a given buffer with cryptographically secure random bytes.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[out]aBuffer

A pointer to a buffer to fill with the random bytes.

uint16_t[in]aSize

Size of buffer (number of bytes to fill).


otPlatCryptoEcdsaGenerateKey#

otError otPlatCryptoEcdsaGenerateKey (otPlatCryptoEcdsaKeyPair * aKeyPair)

Generate and populate the output buffer with a new ECDSA key-pair.

Parameters
TypeDirectionArgument NameDescription
otPlatCryptoEcdsaKeyPair *[out]aKeyPair

A pointer to an ECDSA key-pair structure to store the generated key-pair.


otPlatCryptoEcdsaGetPublicKey#

otError otPlatCryptoEcdsaGetPublicKey (const otPlatCryptoEcdsaKeyPair * aKeyPair, otPlatCryptoEcdsaPublicKey * aPublicKey)

Get the associated public key from the input context.

Parameters
TypeDirectionArgument NameDescription
const otPlatCryptoEcdsaKeyPair *[in]aKeyPair

A pointer to an ECDSA key-pair structure where the key-pair is stored.

otPlatCryptoEcdsaPublicKey *[out]aPublicKey

A pointer to an ECDSA public key structure to store the public key.


otPlatCryptoEcdsaSign#

otError otPlatCryptoEcdsaSign (const otPlatCryptoEcdsaKeyPair * aKeyPair, const otPlatCryptoSha256Hash * aHash, otPlatCryptoEcdsaSignature * aSignature)

Calculate the ECDSA signature for a hashed message using the private key from the input context.

Parameters
TypeDirectionArgument NameDescription
const otPlatCryptoEcdsaKeyPair *[in]aKeyPair

A pointer to an ECDSA key-pair structure where the key-pair is stored.

const otPlatCryptoSha256Hash *[in]aHash

A pointer to a SHA-256 hash structure where the hash value for signature calculation is stored.

otPlatCryptoEcdsaSignature *[out]aSignature

A pointer to an ECDSA signature structure to output the calculated signature.

Uses the deterministic digital signature generation procedure from RFC 6979.


otPlatCryptoEcdsaVerify#

otError otPlatCryptoEcdsaVerify (const otPlatCryptoEcdsaPublicKey * aPublicKey, const otPlatCryptoSha256Hash * aHash, const otPlatCryptoEcdsaSignature * aSignature)

Use the key from the input context to verify the ECDSA signature of a hashed message.

Parameters
TypeDirectionArgument NameDescription
const otPlatCryptoEcdsaPublicKey *[in]aPublicKey

A pointer to an ECDSA public key structure where the public key for signature verification is stored.

const otPlatCryptoSha256Hash *[in]aHash

A pointer to a SHA-256 hash structure where the hash value for signature verification is stored.

const otPlatCryptoEcdsaSignature *[in]aSignature

A pointer to an ECDSA signature structure where the signature value to be verified is stored.


otPlatCryptoEcdsaSignUsingKeyRef#

otError otPlatCryptoEcdsaSignUsingKeyRef (otCryptoKeyRef aKeyRef, const otPlatCryptoSha256Hash * aHash, otPlatCryptoEcdsaSignature * aSignature)

Calculate the ECDSA signature for a hashed message using the Key reference passed.

Parameters
TypeDirectionArgument NameDescription
otCryptoKeyRef[in]aKeyRef

Key Reference to the slot where the key-pair is stored.

const otPlatCryptoSha256Hash *[in]aHash

A pointer to a SHA-256 hash structure where the hash value for signature calculation is stored.

otPlatCryptoEcdsaSignature *[out]aSignature

A pointer to an ECDSA signature structure to output the calculated signature.

Uses the deterministic digital signature generation procedure from RFC 6979.

Note

  • This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.


otPlatCryptoEcdsaExportPublicKey#

otError otPlatCryptoEcdsaExportPublicKey (otCryptoKeyRef aKeyRef, otPlatCryptoEcdsaPublicKey * aPublicKey)

Get the associated public key from the key reference passed.

Parameters
TypeDirectionArgument NameDescription
otCryptoKeyRef[in]aKeyRef

Key Reference to the slot where the key-pair is stored.

otPlatCryptoEcdsaPublicKey *[out]aPublicKey

A pointer to an ECDSA public key structure to store the public key.

The public key is stored differently depending on the crypto backend library being used (OPENTHREAD_CONFIG_CRYPTO_LIB).

This API must make sure to return the public key as a byte sequence representation of an uncompressed curve point (RFC 6605 - sec 4)

Note

  • This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.


otPlatCryptoEcdsaGenerateAndImportKey#

otError otPlatCryptoEcdsaGenerateAndImportKey (otCryptoKeyRef aKeyRef)

Generate and import a new ECDSA key-pair at reference passed.

Parameters
TypeDirectionArgument NameDescription
otCryptoKeyRef[in]aKeyRef

Key Reference to the slot where the key-pair is stored.

Note

  • This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.


otPlatCryptoEcdsaVerifyUsingKeyRef#

otError otPlatCryptoEcdsaVerifyUsingKeyRef (otCryptoKeyRef aKeyRef, const otPlatCryptoSha256Hash * aHash, const otPlatCryptoEcdsaSignature * aSignature)

Use the keyref to verify the ECDSA signature of a hashed message.

Parameters
TypeDirectionArgument NameDescription
otCryptoKeyRef[in]aKeyRef

Key Reference to the slot where the key-pair is stored.

const otPlatCryptoSha256Hash *[in]aHash

A pointer to a SHA-256 hash structure where the hash value for signature verification is stored.

const otPlatCryptoEcdsaSignature *[in]aSignature

A pointer to an ECDSA signature structure where the signature value to be verified is stored.

Note

  • This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.


otPlatCryptoPbkdf2GenerateKey#

otError otPlatCryptoPbkdf2GenerateKey (const uint8_t * aPassword, uint16_t aPasswordLen, const uint8_t * aSalt, uint16_t aSaltLen, uint32_t aIterationCounter, uint16_t aKeyLen, uint8_t * aKey)

Perform PKCS#5 PBKDF2 using CMAC (AES-CMAC-PRF-128).

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]aPassword

Password to use when generating key.

uint16_t[in]aPasswordLen

Length of password.

const uint8_t *[in]aSalt

Salt to use when generating key.

uint16_t[in]aSaltLen

Length of salt.

uint32_t[in]aIterationCounter

Iteration count.

uint16_t[in]aKeyLen

Length of generated key in bytes.

uint8_t *[out]aKey

A pointer to the generated key.


Macro Definition Documentation#

OT_CRYPTO_SHA256_HASH_SIZE#

#define OT_CRYPTO_SHA256_HASH_SIZE
Value:
32

Length of SHA256 hash (in bytes).


OT_CRYPTO_ECDSA_MAX_DER_SIZE#

#define OT_CRYPTO_ECDSA_MAX_DER_SIZE
Value:
125

Max buffer size (in bytes) for representing the EDCSA key-pair in DER format.


OT_CRYPTO_ECDSA_PUBLIC_KEY_SIZE#

#define OT_CRYPTO_ECDSA_PUBLIC_KEY_SIZE
Value:
64

Buffer size (in bytes) for representing the EDCSA public key.


OT_CRYPTO_ECDSA_SIGNATURE_SIZE#

#define OT_CRYPTO_ECDSA_SIGNATURE_SIZE
Value:
64

Buffer size (in bytes) for representing the EDCSA signature.


OT_CRYPTO_PBDKF2_MAX_SALT_SIZE#

#define OT_CRYPTO_PBDKF2_MAX_SALT_SIZE
Value:
30

Max PBKDF2 SALT length: salt prefix (6) + extended panid (8) + network name (16)