Raw Link#

This module includes functions that control the raw link-layer configuration.

Typedefs#

typedef void(*
otLinkRawReceiveDone)(otInstance *aInstance, otRadioFrame *aFrame, otError aError)

Pointer on receipt of a IEEE 802.15.4 frame.

typedef void(*
otLinkRawTransmitDone)(otInstance *aInstance, otRadioFrame *aFrame, otRadioFrame *aAckFrame, otError aError)

Pointer on receipt of a IEEE 802.15.4 frame.

typedef void(*
otLinkRawEnergyScanDone)(otInstance *aInstance, int8_t aEnergyScanMaxRssi)

Pointer on receipt of a IEEE 802.15.4 frame.

Functions#

otLinkRawSetReceiveDone(otInstance *aInstance, otLinkRawReceiveDone aCallback)

Enables/disables the raw link-layer.

bool
otLinkRawIsEnabled(otInstance *aInstance)

Indicates whether or not the raw link-layer is enabled.

bool
otLinkRawGetPromiscuous(otInstance *aInstance)

Gets the status of promiscuous mode.

otLinkRawSetPromiscuous(otInstance *aInstance, bool aEnable)

Enables or disables promiscuous mode.

otLinkRawSetShortAddress(otInstance *aInstance, uint16_t aShortAddress)

Set the Short Address for address filtering.

otLinkRawSleep(otInstance *aInstance)

Transition the radio from Receive to Sleep.

otLinkRawReceive(otInstance *aInstance)

Transitioning the radio from Sleep to Receive.

otLinkRawGetTransmitBuffer(otInstance *aInstance)

The radio transitions from Transmit to Receive.

otLinkRawTransmit(otInstance *aInstance, otLinkRawTransmitDone aCallback)

Begins the transmit sequence on the radio.

int8_t
otLinkRawGetRssi(otInstance *aInstance)

Get the most recent RSSI measurement.

otLinkRawGetCaps(otInstance *aInstance)

Get the radio capabilities.

otLinkRawEnergyScan(otInstance *aInstance, uint8_t aScanChannel, uint16_t aScanDuration, otLinkRawEnergyScanDone aCallback)

Begins the energy scan sequence on the radio.

otLinkRawSrcMatchEnable(otInstance *aInstance, bool aEnable)

Enable/Disable source match for frame pending.

otLinkRawSrcMatchAddShortEntry(otInstance *aInstance, uint16_t aShortAddress)

Adding short address to the source match table.

otLinkRawSrcMatchAddExtEntry(otInstance *aInstance, const otExtAddress *aExtAddress)

Adding extended address to the source match table.

otLinkRawSrcMatchClearShortEntry(otInstance *aInstance, uint16_t aShortAddress)

Removing short address to the source match table.

otLinkRawSrcMatchClearExtEntry(otInstance *aInstance, const otExtAddress *aExtAddress)

Removing extended address to the source match table of the radio.

otLinkRawSrcMatchClearShortEntries(otInstance *aInstance)

Removing all the short addresses from the source match table.

otLinkRawSrcMatchClearExtEntries(otInstance *aInstance)

Removing all the extended addresses from the source match table.

otLinkRawSetMacKey(otInstance *aInstance, uint8_t aKeyIdMode, uint8_t aKeyId, const otMacKey *aPrevKey, const otMacKey *aCurrKey, const otMacKey *aNextKey)

Update MAC keys and key index.

otLinkRawSetMacFrameCounter(otInstance *aInstance, uint32_t aMacFrameCounter)

Sets the current MAC frame counter value.

otLinkRawSetMacFrameCounterIfLarger(otInstance *aInstance, uint32_t aMacFrameCounter)

Sets the current MAC frame counter value only if the new value is larger than the current one.

uint64_t
otLinkRawGetRadioTime(otInstance *aInstance)

Get current platform time (64bits width) of the radio chip.

Typedef Documentation#

otLinkRawReceiveDone#

typedef void(* otLinkRawReceiveDone) (otInstance *aInstance, otRadioFrame *aFrame, otError aError) )(otInstance *aInstance, otRadioFrame *aFrame, otError aError)

Pointer on receipt of a IEEE 802.15.4 frame.

Parameters
TypeDirectionArgument NameDescription
[in]aInstance

A pointer to an OpenThread instance.

[in]aFrame

A pointer to the received frame or NULL if the receive operation was aborted.

[in]aError

OT_ERROR_NONE when successfully received a frame. OT_ERROR_ABORT when reception was aborted and a frame was not received.


otLinkRawTransmitDone#

typedef void(* otLinkRawTransmitDone) (otInstance *aInstance, otRadioFrame *aFrame, otRadioFrame *aAckFrame, otError aError) )(otInstance *aInstance, otRadioFrame *aFrame, otRadioFrame *aAckFrame, otError aError)

Pointer on receipt of a IEEE 802.15.4 frame.

Parameters
TypeDirectionArgument NameDescription
[in]aInstance

A pointer to an OpenThread instance.

[in]aFrame

A pointer to the frame that was transmitted.

[in]aAckFrame

A pointer to the ACK frame.

[in]aError

OT_ERROR_NONE when the frame was transmitted. OT_ERROR_NO_ACK when the frame was transmitted but no ACK was received OT_ERROR_CHANNEL_ACCESS_FAILURE when the transmission could not take place due to activity on the channel. OT_ERROR_ABORT when transmission was aborted for other reasons.


otLinkRawEnergyScanDone#

typedef void(* otLinkRawEnergyScanDone) (otInstance *aInstance, int8_t aEnergyScanMaxRssi) )(otInstance *aInstance, int8_t aEnergyScanMaxRssi)

Pointer on receipt of a IEEE 802.15.4 frame.

Parameters
TypeDirectionArgument NameDescription
[in]aInstance

A pointer to an OpenThread instance.

[in]aEnergyScanMaxRssi

The maximum RSSI encountered on the scanned channel.


Function Documentation#

otLinkRawSetReceiveDone#

otError otLinkRawSetReceiveDone (otInstance * aInstance, otLinkRawReceiveDone aCallback)

Enables/disables the raw link-layer.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otLinkRawReceiveDone[in]aCallback

A pointer to a function called on receipt of a IEEE 802.15.4 frame. NULL to disable the raw-link layer.


otLinkRawIsEnabled#

bool otLinkRawIsEnabled (otInstance * aInstance)

Indicates whether or not the raw link-layer is enabled.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otLinkRawGetPromiscuous#

bool otLinkRawGetPromiscuous (otInstance * aInstance)

Gets the status of promiscuous mode.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otLinkRawSetPromiscuous#

otError otLinkRawSetPromiscuous (otInstance * aInstance, bool aEnable)

Enables or disables promiscuous mode.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

bool[in]aEnable

A value to enable or disable promiscuous mode.


otLinkRawSetShortAddress#

otError otLinkRawSetShortAddress (otInstance * aInstance, uint16_t aShortAddress)

Set the Short Address for address filtering.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aShortAddress

The IEEE 802.15.4 Short Address.


otLinkRawSleep#

otError otLinkRawSleep (otInstance * aInstance)

Transition the radio from Receive to Sleep.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Turn off the radio.


otLinkRawReceive#

otError otLinkRawReceive (otInstance * aInstance)

Transitioning the radio from Sleep to Receive.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Turn on the radio.


otLinkRawGetTransmitBuffer#

otRadioFrame * otLinkRawGetTransmitBuffer (otInstance * aInstance)

The radio transitions from Transmit to Receive.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns a pointer to the transmit buffer.

The caller forms the IEEE 802.15.4 frame in this buffer then calls otLinkRawTransmit() to request transmission.

Returns

  • A pointer to the transmit buffer or NULL if the raw link-layer isn't enabled.


otLinkRawTransmit#

otError otLinkRawTransmit (otInstance * aInstance, otLinkRawTransmitDone aCallback)

Begins the transmit sequence on the radio.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otLinkRawTransmitDone[in]aCallback

A pointer to a function called on completion of the transmission.

The caller must form the IEEE 802.15.4 frame in the buffer provided by otLinkRawGetTransmitBuffer() before requesting transmission. The channel and transmit power are also included in the otRadioFrame structure.

The transmit sequence consists of:

  1. Transitioning the radio to Transmit from Receive.

  2. Transmits the PSDU on the given channel and at the given transmit power.


otLinkRawGetRssi#

int8_t otLinkRawGetRssi (otInstance * aInstance)

Get the most recent RSSI measurement.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The RSSI in dBm when it is valid. 127 when RSSI is invalid.


otLinkRawGetCaps#

otRadioCaps otLinkRawGetCaps (otInstance * aInstance)

Get the radio capabilities.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The radio capability bit vector. The stack enables or disables some functions based on this value.


otLinkRawEnergyScan#

otError otLinkRawEnergyScan (otInstance * aInstance, uint8_t aScanChannel, uint16_t aScanDuration, otLinkRawEnergyScanDone aCallback)

Begins the energy scan sequence on the radio.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aScanChannel

The channel to perform the energy scan on.

uint16_t[in]aScanDuration

The duration, in milliseconds, for the channel to be scanned.

otLinkRawEnergyScanDone[in]aCallback

A pointer to a function called on completion of a scanned channel.


otLinkRawSrcMatchEnable#

otError otLinkRawSrcMatchEnable (otInstance * aInstance, bool aEnable)

Enable/Disable source match for frame pending.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

bool[in]aEnable

Enable/disable source match for frame pending.


otLinkRawSrcMatchAddShortEntry#

otError otLinkRawSrcMatchAddShortEntry (otInstance * aInstance, uint16_t aShortAddress)

Adding short address to the source match table.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aShortAddress

The short address to be added.


otLinkRawSrcMatchAddExtEntry#

otError otLinkRawSrcMatchAddExtEntry (otInstance * aInstance, const otExtAddress * aExtAddress)

Adding extended address to the source match table.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otExtAddress *[in]aExtAddress

The extended address to be added.


otLinkRawSrcMatchClearShortEntry#

otError otLinkRawSrcMatchClearShortEntry (otInstance * aInstance, uint16_t aShortAddress)

Removing short address to the source match table.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aShortAddress

The short address to be removed.


otLinkRawSrcMatchClearExtEntry#

otError otLinkRawSrcMatchClearExtEntry (otInstance * aInstance, const otExtAddress * aExtAddress)

Removing extended address to the source match table of the radio.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otExtAddress *[in]aExtAddress

The extended address to be removed.


otLinkRawSrcMatchClearShortEntries#

otError otLinkRawSrcMatchClearShortEntries (otInstance * aInstance)

Removing all the short addresses from the source match table.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otLinkRawSrcMatchClearExtEntries#

otError otLinkRawSrcMatchClearExtEntries (otInstance * aInstance)

Removing all the extended addresses from the source match table.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otLinkRawSetMacKey#

otError otLinkRawSetMacKey (otInstance * aInstance, uint8_t aKeyIdMode, uint8_t aKeyId, const otMacKey * aPrevKey, const otMacKey * aCurrKey, const otMacKey * aNextKey)

Update MAC keys and key index.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aKeyIdMode

The key ID mode.

uint8_t[in]aKeyId

The key index.

const otMacKey *[in]aPrevKey

The previous MAC key.

const otMacKey *[in]aCurrKey

The current MAC key.

const otMacKey *[in]aNextKey

The next MAC key.


otLinkRawSetMacFrameCounter#

otError otLinkRawSetMacFrameCounter (otInstance * aInstance, uint32_t aMacFrameCounter)

Sets the current MAC frame counter value.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint32_t[in]aMacFrameCounter

The MAC frame counter value.

Always sets the MAC counter to the new given value aMacFrameCounter independent of the current value.


otLinkRawSetMacFrameCounterIfLarger#

otError otLinkRawSetMacFrameCounterIfLarger (otInstance * aInstance, uint32_t aMacFrameCounter)

Sets the current MAC frame counter value only if the new value is larger than the current one.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint32_t[in]aMacFrameCounter

The MAC frame counter value.


otLinkRawGetRadioTime#

uint64_t otLinkRawGetRadioTime (otInstance * aInstance)

Get current platform time (64bits width) of the radio chip.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The current radio time in microseconds.