Radio Configuration#

This module includes the platform abstraction for radio configuration.

Functions#

otPlatRadioGetCaps(otInstance *aInstance)

Get the radio capabilities.

const char *
otPlatRadioGetVersionString(otInstance *aInstance)

Get the radio version string.

int8_t
otPlatRadioGetReceiveSensitivity(otInstance *aInstance)

Get the radio receive sensitivity value.

void
otPlatRadioGetIeeeEui64(otInstance *aInstance, uint8_t *aIeeeEui64)

Gets the factory-assigned IEEE EUI-64 for this interface.

void
otPlatRadioSetPanId(otInstance *aInstance, otPanId aPanId)

Set the PAN ID for address filtering.

void
otPlatRadioSetExtendedAddress(otInstance *aInstance, const otExtAddress *aExtAddress)

Set the Extended Address for address filtering.

void
otPlatRadioSetShortAddress(otInstance *aInstance, otShortAddress aShortAddress)

Set the Short Address for address filtering.

otPlatRadioGetTransmitPower(otInstance *aInstance, int8_t *aPower)

Get the radio's transmit power in dBm.

otPlatRadioSetTransmitPower(otInstance *aInstance, int8_t aPower)

Set the radio's transmit power in dBm.

otPlatRadioGetCcaEnergyDetectThreshold(otInstance *aInstance, int8_t *aThreshold)

Get the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.

otPlatRadioSetCcaEnergyDetectThreshold(otInstance *aInstance, int8_t aThreshold)

Set the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.

otPlatRadioGetFemLnaGain(otInstance *aInstance, int8_t *aGain)

Gets the external FEM's Rx LNA gain in dBm.

otPlatRadioSetFemLnaGain(otInstance *aInstance, int8_t aGain)

Sets the external FEM's Rx LNA gain in dBm.

bool
otPlatRadioGetPromiscuous(otInstance *aInstance)

Get the status of promiscuous mode.

void
otPlatRadioSetPromiscuous(otInstance *aInstance, bool aEnable)

Enable or disable promiscuous mode.

void
otPlatRadioSetRxOnWhenIdle(otInstance *aInstance, bool aEnable)

Sets the rx-on-when-idle state to the radio platform.

void
otPlatRadioSetMacKey(otInstance *aInstance, uint8_t aKeyIdMode, uint8_t aKeyId, const otMacKeyMaterial *aPrevKey, const otMacKeyMaterial *aCurrKey, const otMacKeyMaterial *aNextKey, otRadioKeyType aKeyType)

Update MAC keys and key index.

void
otPlatRadioSetMacFrameCounter(otInstance *aInstance, uint32_t aMacFrameCounter)

Sets the current MAC frame counter value.

void
otPlatRadioSetMacFrameCounterIfLarger(otInstance *aInstance, uint32_t aMacFrameCounter)

Sets the current MAC frame counter value only if the new given value is larger than the current value.

uint64_t
otPlatRadioGetNow(otInstance *aInstance)

Get the current time in microseconds referenced to a continuous monotonic local radio clock (64 bits width).

uint32_t
otPlatRadioGetBusSpeed(otInstance *aInstance)

Get the bus speed in bits/second between the host and the radio chip.

Function Documentation#

otPlatRadioGetCaps#

otRadioCaps otPlatRadioGetCaps (otInstance * aInstance)

Get the radio capabilities.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

Returns

  • The radio capability bit vector (see OT_RADIO_CAP_* definitions).


otPlatRadioGetVersionString#

const char * otPlatRadioGetVersionString (otInstance * aInstance)

Get the radio version string.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

This is an optional radio driver platform function. If not provided by platform radio driver, OpenThread uses the OpenThread version instead (See Also

Returns

  • A pointer to the OpenThread radio version.


otPlatRadioGetReceiveSensitivity#

int8_t otPlatRadioGetReceiveSensitivity (otInstance * aInstance)

Get the radio receive sensitivity value.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

Returns

  • The radio receive sensitivity value in dBm.


otPlatRadioGetIeeeEui64#

void otPlatRadioGetIeeeEui64 (otInstance * aInstance, uint8_t * aIeeeEui64)

Gets the factory-assigned IEEE EUI-64 for this interface.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

uint8_t *[out]aIeeeEui64

A pointer to the factory-assigned IEEE EUI-64.


otPlatRadioSetPanId#

void otPlatRadioSetPanId (otInstance * aInstance, otPanId aPanId)

Set the PAN ID for address filtering.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

otPanId[in]aPanId

The IEEE 802.15.4 PAN ID.


otPlatRadioSetExtendedAddress#

void otPlatRadioSetExtendedAddress (otInstance * aInstance, const otExtAddress * aExtAddress)

Set the Extended Address for address filtering.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

const otExtAddress *[in]aExtAddress

A pointer to the IEEE 802.15.4 Extended Address stored in little-endian byte order.


otPlatRadioSetShortAddress#

void otPlatRadioSetShortAddress (otInstance * aInstance, otShortAddress aShortAddress)

Set the Short Address for address filtering.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

otShortAddress[in]aShortAddress

The IEEE 802.15.4 Short Address.


otPlatRadioGetTransmitPower#

otError otPlatRadioGetTransmitPower (otInstance * aInstance, int8_t * aPower)

Get the radio's transmit power in dBm.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

int8_t *[out]aPower

The transmit power in dBm.

Note

  • The transmit power returned will be no larger than the power specified in the max power table for the current channel.


otPlatRadioSetTransmitPower#

otError otPlatRadioSetTransmitPower (otInstance * aInstance, int8_t aPower)

Set the radio's transmit power in dBm.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

int8_t[in]aPower

The transmit power in dBm.

Note

  • The real transmit power will be no larger than the power specified in the max power table for the current channel.


otPlatRadioGetCcaEnergyDetectThreshold#

otError otPlatRadioGetCcaEnergyDetectThreshold (otInstance * aInstance, int8_t * aThreshold)

Get the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

int8_t *[out]aThreshold

The CCA ED threshold in dBm.


otPlatRadioSetCcaEnergyDetectThreshold#

otError otPlatRadioSetCcaEnergyDetectThreshold (otInstance * aInstance, int8_t aThreshold)

Set the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

int8_t[in]aThreshold

The CCA ED threshold in dBm.


otPlatRadioGetFemLnaGain#

otError otPlatRadioGetFemLnaGain (otInstance * aInstance, int8_t * aGain)

Gets the external FEM's Rx LNA gain in dBm.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

int8_t *[out]aGain

The external FEM's Rx LNA gain in dBm.


otPlatRadioSetFemLnaGain#

otError otPlatRadioSetFemLnaGain (otInstance * aInstance, int8_t aGain)

Sets the external FEM's Rx LNA gain in dBm.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

int8_t[in]aGain

The external FEM's Rx LNA gain in dBm.


otPlatRadioGetPromiscuous#

bool otPlatRadioGetPromiscuous (otInstance * aInstance)

Get the status of promiscuous mode.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.


otPlatRadioSetPromiscuous#

void otPlatRadioSetPromiscuous (otInstance * aInstance, bool aEnable)

Enable or disable promiscuous mode.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

bool[in]aEnable

TRUE to enable or FALSE to disable promiscuous mode.


otPlatRadioSetRxOnWhenIdle#

void otPlatRadioSetRxOnWhenIdle (otInstance * aInstance, bool aEnable)

Sets the rx-on-when-idle state to the radio platform.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

bool[in]aEnable

TRUE to keep radio in Receive state, FALSE to put to Sleep state during idle periods.

There are a few situations that the radio can enter sleep state if the device is in rx-off-when-idle state but it's hard and costly for the SubMac to identify these situations and instruct the radio to enter sleep:

  • Finalization of a regular frame reception task, provided that:

    • The frame is received without errors and passes the filtering and it's not an spurious ACK.

    • ACK is not requested or transmission of ACK is not possible due to internal conditions.

  • Finalization of a frame transmission or transmission of an ACK frame, when ACK is not requested in the transmitted frame.

  • Finalization of the reception operation of a requested ACK due to:

    • ACK timeout expiration.

    • Reception of an invalid ACK or not an ACK frame.

    • Reception of the proper ACK, unless the transmitted frame was a Data Request Command and the frame pending bit on the received ACK is set to true. In this case the radio platform implementation SHOULD keep the receiver on until a determined timeout which triggers an idle period start.OPENTHREAD_CONFIG_MAC_DATA_POLL_TIMEOUT can be taken as a reference for this.

  • Finalization of a stand alone CCA task.

  • Finalization of a CCA operation with busy result during CSMA/CA procedure.

  • Finalization of an Energy Detection task.

  • Finalization of a radio reception window scheduled with otPlatRadioReceiveAt.

If a platform supports OT_RADIO_CAPS_RX_ON_WHEN_IDLE it must also support OT_RADIO_CAPS_CSMA_BACKOFF and handle idle periods after CCA as described above.


otPlatRadioSetMacKey#

void otPlatRadioSetMacKey (otInstance * aInstance, uint8_t aKeyIdMode, uint8_t aKeyId, const otMacKeyMaterial * aPrevKey, const otMacKeyMaterial * aCurrKey, const otMacKeyMaterial * aNextKey, otRadioKeyType aKeyType)

Update MAC keys and key index.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aKeyIdMode

The key ID mode.

uint8_t[in]aKeyId

Current MAC key index.

const otMacKeyMaterial *[in]aPrevKey

A pointer to the previous MAC key.

const otMacKeyMaterial *[in]aCurrKey

A pointer to the current MAC key.

const otMacKeyMaterial *[in]aNextKey

A pointer to the next MAC key.

otRadioKeyType[in]aKeyType

Key Type used.

Is used when radio provides OT_RADIO_CAPS_TRANSMIT_SEC capability.


otPlatRadioSetMacFrameCounter#

void otPlatRadioSetMacFrameCounter (otInstance * aInstance, uint32_t aMacFrameCounter)

Sets the current MAC frame counter value.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint32_t[in]aMacFrameCounter

The MAC frame counter value.

Is used when radio provides OT_RADIO_CAPS_TRANSMIT_SEC capability.


otPlatRadioSetMacFrameCounterIfLarger#

void otPlatRadioSetMacFrameCounterIfLarger (otInstance * aInstance, uint32_t aMacFrameCounter)

Sets the current MAC frame counter value only if the new given value is larger than the current value.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint32_t[in]aMacFrameCounter

The MAC frame counter value.

Is used when radio provides OT_RADIO_CAPS_TRANSMIT_SEC capability.


otPlatRadioGetNow#

uint64_t otPlatRadioGetNow (otInstance * aInstance)

Get the current time in microseconds referenced to a continuous monotonic local radio clock (64 bits width).

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

The radio clock SHALL NOT wrap during the device's uptime. Implementations SHALL therefore identify and compensate for internal counter overflows. The clock does not have a defined epoch and it SHALL NOT introduce any continuous or discontinuous adjustments (e.g. leap seconds). Implementations SHALL compensate for any sleep times of the device.

Implementations MAY choose to discipline the radio clock and compensate for sleep times by any means (e.g. by combining a high precision/low power RTC with a high resolution counter) as long as the exposed combined clock provides continuous monotonic microsecond resolution ticks within the accuracy limits announced by otPlatRadioGetCslAccuracy.

Returns

  • The current time in microseconds. UINT64_MAX when platform does not support or radio time is not ready.


otPlatRadioGetBusSpeed#

uint32_t otPlatRadioGetBusSpeed (otInstance * aInstance)

Get the bus speed in bits/second between the host and the radio chip.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The bus speed in bits/second between the host and the radio chip. Return 0 when the MAC and above layer and Radio layer resides on the same chip.