Contains the counters of DNS-SD server.
Public Attributes#
uint32_t
The number of successful responses.
uint32_t
The number of server failure responses.
uint32_t
The number of format error responses.
uint32_t
The number of name error responses.
uint32_t
The number of 'not implemented' responses.
uint32_t
The number of other responses.
uint32_t
The number of queries resolved by the local SRP server.
The number of queries, responses, failures handled by upstream DNS server.
Public Attribute Documentation#
mServerFailureResponse#
uint32_t otDnssdCounters::mServerFailureResponse
The number of server failure responses.
mFormatErrorResponse#
uint32_t otDnssdCounters::mFormatErrorResponse
The number of format error responses.
mNotImplementedResponse#
uint32_t otDnssdCounters::mNotImplementedResponse
The number of 'not implemented' responses.
mResolvedBySrp#
uint32_t otDnssdCounters::mResolvedBySrp
The number of queries resolved by the local SRP server.
mUpstreamDnsCounters#
otUpstreamDnsCounters otDnssdCounters::mUpstreamDnsCounters
The number of queries, responses, failures handled by upstream DNS server.