You are viewing documentation for version:
Represents an Active or Pending Operational Dataset. 
Components in Dataset are optional. mComponents structure specifies which components are present in the Dataset. 
Public Attributes#
Specifies which components are set in the Dataset. 
Public Attribute Documentation#
mActiveTimestamp#
otTimestamp otOperationalDataset::mActiveTimestamp
Active Timestamp. 
mPendingTimestamp#
otTimestamp otOperationalDataset::mPendingTimestamp
Pending Timestamp. 
mNetworkKey#
otNetworkKey otOperationalDataset::mNetworkKey
Network Key. 
mNetworkName#
otNetworkName otOperationalDataset::mNetworkName
Network Name. 
mExtendedPanId#
otExtendedPanId otOperationalDataset::mExtendedPanId
Extended PAN ID. 
mMeshLocalPrefix#
otMeshLocalPrefix otOperationalDataset::mMeshLocalPrefix
Mesh Local Prefix. 
mDelay#
uint32_t otOperationalDataset::mDelay
Delay Timer. 
mPanId#
otPanId otOperationalDataset::mPanId
PAN ID. 
mChannel#
uint16_t otOperationalDataset::mChannel
Channel. 
mWakeupChannel#
uint16_t otOperationalDataset::mWakeupChannel
Wake-up Channel. 
mPskc#
otPskc otOperationalDataset::mPskc
PSKc. 
mSecurityPolicy#
otSecurityPolicy otOperationalDataset::mSecurityPolicy
Security Policy. 
mChannelMask#
otChannelMask otOperationalDataset::mChannelMask
Channel Mask. 
mComponents#
otOperationalDatasetComponents otOperationalDataset::mComponents
Specifies which components are set in the Dataset.