Contains the statistics of radio.
Public Attributes#
uint64_t
The total time that radio is in disabled state, in unit of microseconds.
uint64_t
The total time that radio is in sleep state, in unit of microseconds.
uint64_t
uint64_t
The total time that radio is doing transmission, in unit of microseconds.
Public Attribute Documentation#
mDisabledTime#
uint64_t otRadioTimeStats::mDisabledTime
The total time that radio is in disabled state, in unit of microseconds.
mSleepTime#
uint64_t otRadioTimeStats::mSleepTime
The total time that radio is in sleep state, in unit of microseconds.
mRxTime#
uint64_t otRadioTimeStats::mRxTime
The total time that radio is doing transmission, in unit of microseconds.