Represents a DNS query configuration.
Any of the fields in this structure can be set to zero to indicate that it is not specified. How the unspecified fields are treated is determined by the function which uses the instance of otDnsQueryConfig. 
Public Attributes#
Server address (IPv6 addr/port). All zero or zero port for unspecified.
Wait time (in msec) to rx response. Zero indicates unspecified value.
Maximum tx attempts before reporting failure. Zero for unspecified value.
Indicates whether the server can resolve the query recursively or not.
Allow/Disallow NAT64 address translation during address resolution.
Determines which records to query during service resolution.
Select default transport protocol.
Public Attribute Documentation#
mServerSockAddr#
otSockAddr otDnsQueryConfig::mServerSockAddr
Server address (IPv6 addr/port). All zero or zero port for unspecified.
mResponseTimeout#
uint32_t otDnsQueryConfig::mResponseTimeout
Wait time (in msec) to rx response. Zero indicates unspecified value.
mMaxTxAttempts#
uint8_t otDnsQueryConfig::mMaxTxAttempts
Maximum tx attempts before reporting failure. Zero for unspecified value.
mRecursionFlag#
otDnsRecursionFlag otDnsQueryConfig::mRecursionFlag
Indicates whether the server can resolve the query recursively or not.
mNat64Mode#
otDnsNat64Mode otDnsQueryConfig::mNat64Mode
Allow/Disallow NAT64 address translation during address resolution.
mServiceMode#
otDnsServiceMode otDnsQueryConfig::mServiceMode
Determines which records to query during service resolution.
mTransportProto#
otDnsTransportProto otDnsQueryConfig::mTransportProto
Select default transport protocol.