Operational Dataset#
Includes functions for the Operational Dataset API.
For FTD builds only, Dataset Updater includes functions to manage dataset updates.
For FTD and MTD builds, the Operational Dataset API includes functions to manage Active and Pending datasets and dataset TLVs.
Modules#
otOperationalDatasetComponents
Enumerations#
Represents meshcop TLV types.
Typedefs#
Represents a Thread Network Key.
This datatype represents KeyRef to NetworkKey.
Represents a Network Name.
Represents an Extended PAN ID.
Represents a Mesh Local Prefix.
This datatype represents KeyRef to PSKc.
Represent Security Policy.
Represents a Channel Mask.
Represents presence of different components in Active or Pending Operational Dataset.
Represents a Thread Dataset timestamp component.
Represents an Active or Pending Operational Dataset.
Represents an Active or Pending Operational Dataset.
Represents meshcop TLV types.
Pointer is called when a response to a MGMT_SET request is received or times out.
This callback function pointer is called when a Dataset update request finishes, reporting success or failure status of the Dataset update request.
Variables#
Functions#
Indicates whether a valid network is present in the Active Operational Dataset or not.
Gets the Active Operational Dataset.
Gets the Active Operational Dataset.
Sets the Active Operational Dataset.
Sets the Active Operational Dataset.
Gets the Pending Operational Dataset.
Gets the Pending Operational Dataset.
Sets the Pending Operational Dataset.
Sets the Pending Operational Dataset.
Sends MGMT_ACTIVE_GET.
Sends MGMT_ACTIVE_SET.
Sends MGMT_PENDING_GET.
Sends MGMT_PENDING_SET.
Generates PSKc from a given pass-phrase, network name, and extended PAN ID.
Sets an otNetworkName instance from a given null terminated C string.
Parses an Operational Dataset from a given otOperationalDatasetTlvs.
Converts a given Operational Dataset to otOperationalDatasetTlvs.
Updates a given Operational Dataset.
For FTD only, creates a new Operational Dataset to use when forming a new network.
For FTD only, gets a minimal delay timer.
For FTD only, sets a minimal delay timer.
Requests an update to Operational Dataset.
Cancels an ongoing (if any) Operational Dataset update request.
Indicates whether there is an ongoing Operation Dataset update request.
Macros#
Size of the Thread Network Key (bytes)
Maximum size of the Thread Network Name field (bytes)
Size of a Thread PAN ID (bytes)
Size of the Mesh Local Prefix (bytes)
Maximum size of the PSKc (bytes)
Channel 1.
Channel 2.
Channel 3.
Channel 4.
Channel 5.
Channel 6.
Channel 7.
Channel 8.
Channel 9.
Channel 10.
Channel 11.
Channel 12.
Channel 13.
Channel 14.
Channel 15.
Channel 16.
Channel 17.
Channel 18.
Channel 19.
Channel 20.
Channel 21.
Channel 22.
Channel 23.
Channel 24.
Channel 25.
Channel 26.
Maximum length of Operational Dataset in bytes.
Enumeration Documentation#
otMeshcopTlvType#
otMeshcopTlvType
Represents meshcop TLV types.
| Enumerator | |
|---|---|
| OT_MESHCOP_TLV_CHANNEL | meshcop Channel TLV |
| OT_MESHCOP_TLV_PANID | meshcop Pan Id TLV |
| OT_MESHCOP_TLV_EXTPANID | meshcop Extended Pan Id TLV |
| OT_MESHCOP_TLV_NETWORKNAME | meshcop Network Name TLV |
| OT_MESHCOP_TLV_PSKC | meshcop PSKc TLV |
| OT_MESHCOP_TLV_NETWORKKEY | meshcop Network Key TLV |
| OT_MESHCOP_TLV_NETWORK_KEY_SEQUENCE | meshcop Network Key Sequence TLV |
| OT_MESHCOP_TLV_MESHLOCALPREFIX | meshcop Mesh Local Prefix TLV |
| OT_MESHCOP_TLV_STEERING_DATA | meshcop Steering Data TLV |
| OT_MESHCOP_TLV_BORDER_AGENT_RLOC | meshcop Border Agent Locator TLV |
| OT_MESHCOP_TLV_COMMISSIONER_ID | meshcop Commissioner ID TLV |
| OT_MESHCOP_TLV_COMM_SESSION_ID | meshcop Commissioner Session ID TLV |
| OT_MESHCOP_TLV_SECURITYPOLICY | meshcop Security Policy TLV |
| OT_MESHCOP_TLV_GET | meshcop Get TLV |
| OT_MESHCOP_TLV_ACTIVETIMESTAMP | meshcop Active Timestamp TLV |
| OT_MESHCOP_TLV_COMMISSIONER_UDP_PORT | meshcop Commissioner UDP Port TLV |
| OT_MESHCOP_TLV_STATE | meshcop State TLV |
| OT_MESHCOP_TLV_JOINER_DTLS | meshcop Joiner DTLS Encapsulation TLV |
| OT_MESHCOP_TLV_JOINER_UDP_PORT | meshcop Joiner UDP Port TLV |
| OT_MESHCOP_TLV_JOINER_IID | meshcop Joiner IID TLV |
| OT_MESHCOP_TLV_JOINER_RLOC | meshcop Joiner Router Locator TLV |
| OT_MESHCOP_TLV_JOINER_ROUTER_KEK | meshcop Joiner Router KEK TLV |
| OT_MESHCOP_TLV_PROVISIONING_URL | meshcop Provisioning URL TLV |
| OT_MESHCOP_TLV_VENDOR_NAME_TLV | meshcop Vendor Name TLV |
| OT_MESHCOP_TLV_VENDOR_MODEL_TLV | meshcop Vendor Model TLV |
| OT_MESHCOP_TLV_VENDOR_SW_VERSION_TLV | meshcop Vendor SW Version TLV |
| OT_MESHCOP_TLV_VENDOR_DATA_TLV | meshcop Vendor Data TLV |
| OT_MESHCOP_TLV_VENDOR_STACK_VERSION_TLV | meshcop Vendor Stack Version TLV |
| OT_MESHCOP_TLV_UDP_ENCAPSULATION_TLV | meshcop UDP encapsulation TLV |
| OT_MESHCOP_TLV_IPV6_ADDRESS_TLV | meshcop IPv6 address TLV |
| OT_MESHCOP_TLV_PENDINGTIMESTAMP | meshcop Pending Timestamp TLV |
| OT_MESHCOP_TLV_DELAYTIMER | meshcop Delay Timer TLV |
| OT_MESHCOP_TLV_CHANNELMASK | meshcop Channel Mask TLV |
| OT_MESHCOP_TLV_COUNT | meshcop Count TLV |
| OT_MESHCOP_TLV_PERIOD | meshcop Period TLV |
| OT_MESHCOP_TLV_SCAN_DURATION | meshcop Scan Duration TLV |
| OT_MESHCOP_TLV_ENERGY_LIST | meshcop Energy List TLV |
| OT_MESHCOP_TLV_THREAD_DOMAIN_NAME | meshcop Thread Domain Name TLV |
| OT_MESHCOP_TLV_WAKEUP_CHANNEL | meshcop Wake-up Channel TLV |
| OT_MESHCOP_TLV_DISCOVERYREQUEST | meshcop Discovery Request TLV |
| OT_MESHCOP_TLV_DISCOVERYRESPONSE | meshcop Discovery Response TLV |
| OT_MESHCOP_TLV_JOINERADVERTISEMENT | meshcop Joiner Advertisement TLV |
Typedef Documentation#
otNetworkKeyRef#
typedef otCryptoKeyRef otNetworkKeyRef
This datatype represents KeyRef to NetworkKey.
Reference to Key
otNetworkName#
typedef struct otNetworkName otNetworkName
Represents a Network Name.
The otNetworkName is a null terminated C string (i.e., m8 char array MUST end with null char \0).
otPskcRef#
typedef otCryptoKeyRef otPskcRef
This datatype represents KeyRef to PSKc.
Reference to Key
otChannelMask#
typedef uint32_t otChannelMask
Represents a Channel Mask.
The least significant bit (LSB), also referred to as bit 0, corresponds to channel number 0, and so on.
otOperationalDatasetComponents#
typedef struct otOperationalDatasetComponents otOperationalDatasetComponents
Represents presence of different components in Active or Pending Operational Dataset.
otOperationalDataset#
typedef struct otOperationalDataset otOperationalDataset
Represents an Active or Pending Operational Dataset.
Components in Dataset are optional. mComponents structure specifies which components are present in the Dataset.
otOperationalDatasetTlvs#
typedef struct otOperationalDatasetTlvs otOperationalDatasetTlvs
Represents an Active or Pending Operational Dataset.
The Operational Dataset is TLV encoded as specified by Thread.
otDatasetMgmtSetCallback#
typedef void(* otDatasetMgmtSetCallback) (otError aResult, void *aContext) )(otError aResult, void *aContext)
Pointer is called when a response to a MGMT_SET request is received or times out.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | aResult | A result of the operation. | |
| [in] | aContext | A pointer to application-specific context. |
otDatasetUpdaterCallback#
typedef void(* otDatasetUpdaterCallback) (otError aError, void *aContext) )(otError aError, void *aContext)
This callback function pointer is called when a Dataset update request finishes, reporting success or failure status of the Dataset update request.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | aError | The error status. OT_ERROR_NONE indicates successful Dataset update. OT_ERROR_INVALID_STATE indicates failure due invalid state (MLE being disabled). OT_ERROR_ALREADY indicates failure due to another device within network requesting a conflicting Dataset update. | |
| [in] | aContext | A pointer to the arbitrary context (provided by user in |
Available when OPENTHREAD_CONFIG_DATASET_UPDATER_ENABLE is enabled.
Function Documentation#
otDatasetIsCommissioned#
bool otDatasetIsCommissioned (otInstance * aInstance)
Indicates whether a valid network is present in the Active Operational Dataset or not.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Returns
TRUE if a valid network is present in the Active Operational Dataset, FALSE otherwise.
otDatasetGetActive#
otError otDatasetGetActive (otInstance * aInstance, otOperationalDataset * aDataset)
Gets the Active Operational Dataset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otOperationalDataset * | [out] | aDataset | A pointer to where the Active Operational Dataset will be placed. |
otDatasetGetActiveTlvs#
otError otDatasetGetActiveTlvs (otInstance * aInstance, otOperationalDatasetTlvs * aDataset)
Gets the Active Operational Dataset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otOperationalDatasetTlvs * | [out] | aDataset | A pointer to where the Active Operational Dataset will be placed. |
otDatasetSetActive#
otError otDatasetSetActive (otInstance * aInstance, const otOperationalDataset * aDataset)
Sets the Active Operational Dataset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const otOperationalDataset * | [in] | aDataset | A pointer to the Active Operational Dataset. |
If the dataset does not include an Active Timestamp, the dataset is only partially complete.
If Thread is enabled on a device that has a partially complete Active Dataset, the device will attempt to attach to an existing Thread network using any existing information in the dataset. Only the Thread Network Key is needed to attach to a network.
If channel is not included in the dataset, the device will send MLE Announce messages across different channels to find neighbors on other channels.
If the device successfully attaches to a Thread network, the device will then retrieve the full Active Dataset from its Parent. Note that a router-capable device will not transition to the Router or Leader roles until it has a complete Active Dataset.
This function consistently returns OT_ERROR_NONE and can effectively be treated as having a void return type. Previously, other errors (e.g., OT_ERROR_NOT_IMPLEMENTED) were allowed for legacy reasons. However, as non-volatile storage is now mandatory for Thread operation, any failure to save the dataset will trigger an assertion. The otError return type is retained for backward compatibility.
otDatasetSetActiveTlvs#
otError otDatasetSetActiveTlvs (otInstance * aInstance, const otOperationalDatasetTlvs * aDataset)
Sets the Active Operational Dataset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const otOperationalDatasetTlvs * | [in] | aDataset | A pointer to the Active Operational Dataset. |
If the dataset does not include an Active Timestamp, the dataset is only partially complete.
If Thread is enabled on a device that has a partially complete Active Dataset, the device will attempt to attach to an existing Thread network using any existing information in the dataset. Only the Thread Network Key is needed to attach to a network.
If channel is not included in the dataset, the device will send MLE Announce messages across different channels to find neighbors on other channels.
If the device successfully attaches to a Thread network, the device will then retrieve the full Active Dataset from its Parent. Note that a router-capable device will not transition to the Router or Leader roles until it has a complete Active Dataset.
otDatasetGetPending#
otError otDatasetGetPending (otInstance * aInstance, otOperationalDataset * aDataset)
Gets the Pending Operational Dataset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otOperationalDataset * | [out] | aDataset | A pointer to where the Pending Operational Dataset will be placed. |
otDatasetGetPendingTlvs#
otError otDatasetGetPendingTlvs (otInstance * aInstance, otOperationalDatasetTlvs * aDataset)
Gets the Pending Operational Dataset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otOperationalDatasetTlvs * | [out] | aDataset | A pointer to where the Pending Operational Dataset will be placed. |
otDatasetSetPending#
otError otDatasetSetPending (otInstance * aInstance, const otOperationalDataset * aDataset)
Sets the Pending Operational Dataset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const otOperationalDataset * | [in] | aDataset | A pointer to the Pending Operational Dataset. |
This function consistently returns OT_ERROR_NONE and can effectively be treated as having a void return type. Previously, other errors (e.g., OT_ERROR_NOT_IMPLEMENTED) were allowed for legacy reasons. However, as non-volatile storage is now mandatory for Thread operation, any failure to save the dataset will trigger an assertion. The otError return type is retained for backward compatibility.
otDatasetSetPendingTlvs#
otError otDatasetSetPendingTlvs (otInstance * aInstance, const otOperationalDatasetTlvs * aDataset)
Sets the Pending Operational Dataset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const otOperationalDatasetTlvs * | [in] | aDataset | A pointer to the Pending Operational Dataset. |
otDatasetSendMgmtActiveGet#
otError otDatasetSendMgmtActiveGet (otInstance * aInstance, const otOperationalDatasetComponents * aDatasetComponents, const uint8_t * aTlvTypes, uint8_t aLength, const otIp6Address * aAddress)
Sends MGMT_ACTIVE_GET.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const otOperationalDatasetComponents * | [in] | aDatasetComponents | A pointer to a Dataset Components structure specifying which components to request. |
| const uint8_t * | [in] | aTlvTypes | A pointer to array containing additional raw TLV types to be requested. |
| uint8_t | [in] | aLength | The length of |
| const otIp6Address * | [in] | aAddress | A pointer to the IPv6 destination, if it is NULL, will use Leader ALOC as default. |
otDatasetSendMgmtActiveSet#
otError otDatasetSendMgmtActiveSet (otInstance * aInstance, const otOperationalDataset * aDataset, const uint8_t * aTlvs, uint8_t aLength, otDatasetMgmtSetCallback aCallback, void * aContext)
Sends MGMT_ACTIVE_SET.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const otOperationalDataset * | [in] | aDataset | A pointer to operational dataset. |
| const uint8_t * | [in] | aTlvs | A pointer to TLVs. |
| uint8_t | [in] | aLength | The length of TLVs. |
| otDatasetMgmtSetCallback | [in] | aCallback | A pointer to a function that is called on response reception or timeout. |
| void * | [in] | aContext | A pointer to application-specific context for |
otDatasetSendMgmtPendingGet#
otError otDatasetSendMgmtPendingGet (otInstance * aInstance, const otOperationalDatasetComponents * aDatasetComponents, const uint8_t * aTlvTypes, uint8_t aLength, const otIp6Address * aAddress)
Sends MGMT_PENDING_GET.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const otOperationalDatasetComponents * | [in] | aDatasetComponents | A pointer to a Dataset Components structure specifying which components to request. |
| const uint8_t * | [in] | aTlvTypes | A pointer to array containing additional raw TLV types to be requested. |
| uint8_t | [in] | aLength | The length of |
| const otIp6Address * | [in] | aAddress | A pointer to the IPv6 destination, if it is NULL, will use Leader ALOC as default. |
otDatasetSendMgmtPendingSet#
otError otDatasetSendMgmtPendingSet (otInstance * aInstance, const otOperationalDataset * aDataset, const uint8_t * aTlvs, uint8_t aLength, otDatasetMgmtSetCallback aCallback, void * aContext)
Sends MGMT_PENDING_SET.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const otOperationalDataset * | [in] | aDataset | A pointer to operational dataset. |
| const uint8_t * | [in] | aTlvs | A pointer to TLVs. |
| uint8_t | [in] | aLength | The length of TLVs. |
| otDatasetMgmtSetCallback | [in] | aCallback | A pointer to a function that is called on response reception or timeout. |
| void * | [in] | aContext | A pointer to application-specific context for |
otDatasetGeneratePskc#
otError otDatasetGeneratePskc (const char * aPassPhrase, const otNetworkName * aNetworkName, const otExtendedPanId * aExtPanId, otPskc * aPskc)
Generates PSKc from a given pass-phrase, network name, and extended PAN ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const char * | [in] | aPassPhrase | The commissioning pass-phrase. |
| const otNetworkName * | [in] | aNetworkName | The network name for PSKc computation. |
| const otExtendedPanId * | [in] | aExtPanId | The extended PAN ID for PSKc computation. |
| otPskc * | [out] | aPskc | A pointer to variable to output the generated PSKc. |
PSKc is used to establish the Commissioner Session.
otNetworkNameFromString#
otError otNetworkNameFromString (otNetworkName * aNetworkName, const char * aNameString)
Sets an otNetworkName instance from a given null terminated C string.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otNetworkName * | [out] | aNetworkName | A pointer to the |
| const char * | [in] | aNameString | A name C string. |
aNameString must follow UTF-8 encoding and the Network Name length must not be longer than OT_NETWORK_NAME_MAX_SIZE.
otDatasetParseTlvs#
otError otDatasetParseTlvs (const otOperationalDatasetTlvs * aDatasetTlvs, otOperationalDataset * aDataset)
Parses an Operational Dataset from a given otOperationalDatasetTlvs.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const otOperationalDatasetTlvs * | [in] | aDatasetTlvs | A pointer to dataset TLVs. |
| otOperationalDataset * | [out] | aDataset | A pointer to where the dataset will be placed. |
otDatasetConvertToTlvs#
void otDatasetConvertToTlvs (const otOperationalDataset * aDataset, otOperationalDatasetTlvs * aDatasetTlvs)
Converts a given Operational Dataset to otOperationalDatasetTlvs.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const otOperationalDataset * | [in] | aDataset | An Operational dataset to convert to TLVs. |
| otOperationalDatasetTlvs * | [out] | aDatasetTlvs | A pointer to dataset TLVs to return the result. |
otDatasetUpdateTlvs#
otError otDatasetUpdateTlvs (const otOperationalDataset * aDataset, otOperationalDatasetTlvs * aDatasetTlvs)
Updates a given Operational Dataset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const otOperationalDataset * | [in] | aDataset | Specifies the set of types and values to update. |
| otOperationalDatasetTlvs * | [inout] | aDatasetTlvs | A pointer to dataset TLVs to update. |
aDataset contains the fields to be updated and their new value.
otDatasetCreateNewNetwork#
otError otDatasetCreateNewNetwork (otInstance * aInstance, otOperationalDataset * aDataset)
For FTD only, creates a new Operational Dataset to use when forming a new network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otOperationalDataset * | [out] | aDataset | The Operational Dataset. |
otDatasetGetDelayTimerMinimal#
uint32_t otDatasetGetDelayTimerMinimal (otInstance * aInstance)
For FTD only, gets a minimal delay timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
otDatasetSetDelayTimerMinimal#
otError otDatasetSetDelayTimerMinimal (otInstance * aInstance, uint32_t aDelayTimerMinimal)
For FTD only, sets a minimal delay timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| uint32_t | [in] | aDelayTimerMinimal | The value of minimal delay timer (in ms). |
Note
This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
otDatasetUpdaterRequestUpdate#
otError otDatasetUpdaterRequestUpdate (otInstance * aInstance, const otOperationalDataset * aDataset, otDatasetUpdaterCallback aCallback, void * aContext)
Requests an update to Operational Dataset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const otOperationalDataset * | [in] | aDataset | A pointer to the Dataset containing the fields to change. |
| otDatasetUpdaterCallback | [in] | aCallback | A callback to indicate when Dataset update request finishes. |
| void * | [in] | aContext | An arbitrary context passed to callback. |
Available when OPENTHREAD_CONFIG_DATASET_UPDATER_ENABLE is enabled.
aDataset should contain the fields to be updated and their new value. It must not contain Active or Pending Timestamp fields. The Delay field is optional, if not provided a default value (1000 ms) would be used.
otDatasetUpdaterCancelUpdate#
void otDatasetUpdaterCancelUpdate (otInstance * aInstance)
Cancels an ongoing (if any) Operational Dataset update request.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Available when OPENTHREAD_CONFIG_DATASET_UPDATER_ENABLE is enabled.
otDatasetUpdaterIsUpdateOngoing#
bool otDatasetUpdaterIsUpdateOngoing (otInstance * aInstance)
Indicates whether there is an ongoing Operation Dataset update request.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Available when OPENTHREAD_CONFIG_DATASET_UPDATER_ENABLE is enabled.