Represents a TXT resolver result.
Public Attributes#
const char *
The service instance name label.
const char *
The service type.
const uint8_t *
Encoded TXT data bytes. Can be NULL when mTtl is zero.
uint16_t
Length of TXT data.
uint32_t
The TXT data TTL in seconds. Zero TTL indicates record is removed.
uint32_t
The infrastructure network interface index.
Public Attribute Documentation#
mTxtData#
const uint8_t* otPlatDnssdTxtResult::mTxtData
Encoded TXT data bytes. Can be NULL when mTtl is zero.
mTtl#
uint32_t otPlatDnssdTxtResult::mTtl
The TXT data TTL in seconds. Zero TTL indicates record is removed.
mInfraIfIndex#
uint32_t otPlatDnssdTxtResult::mInfraIfIndex
The infrastructure network interface index.