OpenThread Version 2.7.2 (September 24, 2025) - Release Notes#

Simplicity SDK Version 2025.6.2

The OpenThread SDK is an enhanced version of the open-source OpenThread implementation released by Google that has been tailored to work with Silicon Labs hardware.

Click here for earlier releases.

Release Summary#

Release Item Version Release Date Release Notes Key Features API Changes Bug Fixes Chip Enablement

OpenThread SDK

2.7.2

September 24, 2025

Release Notes

None None Targeted quality improvements and bug fixes None

802.15.4 Mesh + BLE Multiprotocol

2.7.2

September 24, 2025

Release Notes

None None Targeted quality improvements and bug fixes None

Impact of Release Changes#

Impact Statements | Migration Guide

Impact Statements#

None.

Migration Guide#

None.

Using This Release#

What's in the Release? | Compatible Software | Installation and Use | Help and Feedback

What's in the Release?#

This release contains the following

  • Silicon Labs OpenThread stack

  • Silicon Labs OpenThread sample applications

  • Silicon Labs OpenThread border router

Compatible Software#

Software Compatible Version or Variant
Simplicity SDK 2025.6.2
GCC (The GNU Compiler Collection) 12.2.1 (provided with Simplicity Studio)

Installation and Use#

The OpenThread SDK is part of the Simplicity SDK, the suite of Silicon Labs SDKs. To quickly get started with OpenThread and the Simplicity SDK, start by installing Simplicity Studio 5, which will set up your development environment and walk you through Simplicity SDK installation. Simplicity Studio 5 includes everything needed for IoT product development with Silicon Labs devices, including a resource and project launcher, software configuration tools, full IDE with GNU toolchain, and analysis tools. Installation instructions are provided in the online Simplicity Studio 5 User’s Guide.

Alternatively, Simplicity SDK may be installed manually by downloading or cloning the latest from GitHub. See https://github.com/SiliconLabs/simplicity_sdk for more information.

The GSDK default installation location has changed beginning with Simplicity Studio 5.3.

  • Windows: C:\Users\<NAME>\SimplicityStudio\SDKs\simplicity_sdk

  • MacOS: /Users/<NAME>/SimplicityStudio/SDKs/simplicity_sdk

Documentation specific to the SDK version is installed with the SDK. API references and other information about this release are available on https://docs.silabs.com/openthread/latest/. Select your SDK version in the upper right.

For more information about the OpenThread SDK see QSG170: Silicon Labs OpenThread QuickStart Guide.

If you are new to Thread see Thread Fundamentals.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

To learn more about the software in this release, dive into our online documentation.

Additional Information#

  • OpenThread GitHub Repository

    The Silicon Labs OpenThread SDK includes all changes from the OpenThread GitHub repo https://github.com/openthread/openthread up to and including commit fb0446f53. An enhanced version of the OpenThread repo can be found in the following Simplicity Studio 5 GSDK location: <GSDK Installation Location>\util\third_party\openthread

  • OpenThread Border Router GitHub Repository

    The Silicon Labs OpenThread SDK includes all changes from the OpenThread border router GitHub repo https://github.com/openthread/ot-br-posix up to and including commit 622f5ecfc. An enhanced version of the OpenThread border router repo can be found in the following Simplicity Studio 5 GSDK location: <GSDK Installation Location>\util\third_party\ot-br-posix

  • Using the Border Router

    For ease of use, Silicon Labs recommends the use of a Docker container for your OpenThread border router. Refer to Using the Silicon Labs RCP with the OpenThread Border Router for details on how to set up the correct version of OpenThread border router Docker container. It is available at https://hub.docker.com/r/siliconlabsinc/openthread-border-router. If you are manually installing a border router, using the copies provided with the Silicon Labs OpenThread SDK, refer to Using the Silicon Labs RCP with the OpenThread Border Router for more details. Although updating the border router environment to a later GitHub version is supported on the OpenThread website, it may make the border router incompatible with the OpenThread RCP stack in the SDK.

  • Secure Vault Integration

    When deployed to Secure Vault High devices, sensitive keys are protected using the Secure Vault Key Management functionality. The following table shows the protected keys and their storage protection characteristics.

    Wrapped keys that are marked as “Non-Exportable” can be used but cannot be viewed or shared at runtime.

    Wrapped keys that are marked as “Exportable” can be used or shared at runtime but remain encrypted while stored in flash.

    For more information on Secure Vault Key Management functionality, see Secure Key Storage.

Wrapped Key Exportable / Non-Exportable Notes
Thread Master Key Exportable Must be exportable to form the TLVs
PSKc Exportable Must be exportable to form the TLVs
Key Encryption Key Exportable Must be exportable to form the TLVs
MLE Key Non-Exportable
Temporary MLE Key Non-Exportable
MAC Previous Key Non-Exportable
MAC Current Key Non-Exportable
MAC Next Key Non-Exportable
  • Thread Certification

    This release has been qualified for Thread 1.4 compliance for the SoC and Border Router using the Thread Test Harness v63.0 (latest available Member Release). For this release Silicon Labs recommends using the above TH version for qualification. Also included with this release is a set of OpenThread stack libraries that may be used for Thread certification by inheritance.

Help and Feedback#

Feature Matrix#

Supported Features | Unsupported Features

Supported Features#

Feature Name Description Quality Related API Names Supported Software Variants, Hardware, Modes, Host Interfaces Related Example Names
Thread 1.4 All features as defined by the Thread Specification up to and including version 1.4. Production OpenThread API None None

Unsupported Features#

This release includes support for running the OpenThread Border Router in a HOST / NCP architecture. However, at the time of the release, the following features were not complete when using this architecture: TREL, NAT64, DHCPv6.

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.