BLE Secure#
This module includes functions that control BLE Secure (TLS over BLE) communication.
This module includes functions that implement TCAT communication.
The functions in this module are available when BLE Secure API feature (OPENTHREAD_CONFIG_BLE_TCAT_ENABLE) is enabled.
The functions in this module are available when TCAT feature (OPENTHREAD_CONFIG_BLE_TCAT_ENABLE) is enabled.
Modules#
Enumerations#
Represents TCAT status code.
Represents TCAT application protocol options.
Represents a TCAT command class.
Represents Advertised Device ID type.
Typedefs#
Pointer to call when ble secure connection state changes.
Pointer to call when data was received over a BLE Secure TLS connection.
Represents TCAT status code.
Represents TCAT application protocol options.
Represents a TCAT command class.
Represents Advertised Device ID type.
Represents General Device ID type.
This structure represents a TCAT vendor information.
Pointer to call when application data or vendor-specific data was received over a TCAT TLS connection.
Pointer to call to notify the completion of a network join/leave operation performed under guidance of a TCAT Commissioner.
Functions#
Starts the BLE Secure service.
Sets TCAT vendor info.
Enables the TCAT protocol over BLE Secure.
Stops the BLE Secure server.
Sets the TCAT agent over BLE Secure into active or standby state.
Sets the Pre-Shared Key (PSK) and cipher suite TLS_PSK_WITH_AES_128_CCM_8.
Returns the peer x509 certificate base64 encoded.
Returns the DER encoded peer x509 certificate.
Returns an attribute value identified by its OID from the subject of the peer x509 certificate.
Returns an attribute value for the OID 1.3.6.1.4.1.44970.x from the v3 extensions of the peer x509 certificate, where the last digit x is set to aThreadOidDescriptor.
Returns an attribute value for the OID 1.3.6.1.4.1.44970.x from the v3 extensions of the own x509 certificate, where the last digit x is set to aThreadOidDescriptor.
Sets the authentication mode for the BLE secure connection.
Sets the local device's X509 certificate and corresponding private key.
Sets the trusted top level CAs.
Initializes TLS session with a peer using an already open BLE connection.
Stops the BLE and TLS connections.
Indicates whether or not the TLS session is active (connected or connecting).
Indicates whether or not the TLS session is connected.
Indicates whether or not the TCAT agent is started over BLE secure.
Indicates whether or not a TCAT command class is authorized for the current TCAT Commissioner.
Sends a secure BLE message.
Sends a secure BLE data packet.
Sends a secure BLE data packet containing application data directed to the application layer aApplicationProtocol or a response to the latest received application data packet.
Flushes the send buffer.
Gets the Install Code Verify Status during the current session.
Macros#
Maximum string length of a UDP or TCP service name (does not include null char).
Maximum number of application layer service names supported.
Maximum length of TCAT advertisement.
TCAT Advertisement Operation Code.
TCAT max size of any type of advertised Device ID.
TCAT max size of device ID.
TCAT_ENABLE_MAX, default max TMF TCAT enable time, in seconds.
Enumeration Documentation#
otTcatStatusCode#
otTcatStatusCode
Represents TCAT status code.
| Enumerator | |
|---|---|
| OT_TCAT_STATUS_SUCCESS | Command or request was successfully processed. |
| OT_TCAT_STATUS_UNSUPPORTED | Requested command or received TLV is not supported. |
| OT_TCAT_STATUS_PARSE_ERROR | Request / command could not be parsed correctly. |
| OT_TCAT_STATUS_VALUE_ERROR | The value of the transmitted TLV has an error. |
| OT_TCAT_STATUS_GENERAL_ERROR | An error not matching any other category occurred. |
| OT_TCAT_STATUS_BUSY | Command cannot be executed because the resource is busy. |
| OT_TCAT_STATUS_UNDEFINED | The requested value, data or service is not defined (currently) or not present. |
| OT_TCAT_STATUS_HASH_ERROR | The hash value presented by the commissioner was incorrect. |
| OT_TCAT_STATUS_INVALID_STATE | The TCAT device is not in a correct state for the given command. |
| OT_TCAT_STATUS_UNAUTHORIZED | Sender does not have sufficient authorization for the given command. |
otTcatApplicationProtocol#
otTcatApplicationProtocol
Represents TCAT application protocol options.
| Enumerator | |
|---|---|
| OT_TCAT_APPLICATION_PROTOCOL_NONE | Message which has been sent without activating the TCAT agent. |
| OT_TCAT_APPLICATION_PROTOCOL_STATUS | |
| OT_TCAT_APPLICATION_PROTOCOL_RESPONSE | Message directed to any application protocol indicating a response with status value (one byte otTcatStatusCode) |
| OT_TCAT_APPLICATION_PROTOCOL_1 | Message directed to application protocol 1. |
| OT_TCAT_APPLICATION_PROTOCOL_2 | Message directed to application protocol 2. |
| OT_TCAT_APPLICATION_PROTOCOL_3 | Message directed to application protocol 3. |
| OT_TCAT_APPLICATION_PROTOCOL_4 | Message directed to application protocol 4. |
| OT_TCAT_APPLICATION_PROTOCOL_VENDOR | Message directed to a vendor specific application protocol. |
otTcatCommandClass#
otTcatCommandClass
Represents a TCAT command class.
| Enumerator | |
|---|---|
| OT_TCAT_COMMAND_CLASS_GENERAL | TCAT commands related to general operations. |
| OT_TCAT_COMMAND_CLASS_COMMISSIONING | TCAT commands related to commissioning. |
| OT_TCAT_COMMAND_CLASS_EXTRACTION | TCAT commands related to key extraction. |
| OT_TCAT_COMMAND_CLASS_DECOMMISSIONING | TCAT commands related to de-commissioning. |
| OT_TCAT_COMMAND_CLASS_APPLICATION | TCAT commands related to application layer. |
otTcatAdvertisedDeviceIdType#
otTcatAdvertisedDeviceIdType
Represents Advertised Device ID type.
Used during TCAT advertisement.
| Enumerator | |
|---|---|
| OT_TCAT_DEVICE_ID_EMPTY | Advertised device ID type not set. |
| OT_TCAT_DEVICE_ID_OUI24 | Advertised device ID type IEEE OUI-24. |
| OT_TCAT_DEVICE_ID_OUI36 | Advertised device ID type IEEE OUI-36. |
| OT_TCAT_DEVICE_ID_DISCRIMINATOR | Advertised device ID type Device Discriminator. |
| OT_TCAT_DEVICE_ID_IANAPEN | Advertised device ID type IANA PEN. |
| OT_TCAT_DEVICE_ID_MAX | Advertised device ID max number of types. |
Typedef Documentation#
otHandleBleSecureConnect#
typedef void(* otHandleBleSecureConnect) (otInstance *aInstance, bool aConnected, bool aBleConnectionOpen, void *aContext) )(otInstance *aInstance, bool aConnected, bool aBleConnectionOpen, void *aContext)
Pointer to call when ble secure connection state changes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | aInstance | A pointer to an OpenThread instance. | |
| [in] | aConnected | TRUE, if a secure connection was established, FALSE otherwise. | |
| [in] | aBleConnectionOpen | TRUE if a BLE connection was established to carry a TLS data stream, FALSE otherwise. | |
| [in] | aContext | A pointer to arbitrary context information. |
otHandleBleSecureReceive#
typedef otHandleTcatApplicationDataReceive otHandleBleSecureReceive
Pointer to call when data was received over a BLE Secure TLS connection.
When TCAT has been started, the TCAT agent automatically responds with status OT_TCAT_STATUS_UNSUPPORTED if no response has been generated or no handler is defined. The application may generate a response to incoming TCAT application data or vendor-specific data by calling otBleSecureSendApplicationTlv.
otTcatApplicationProtocol#
typedef enum otTcatApplicationProtocol otTcatApplicationProtocol
Represents TCAT application protocol options.
otTcatCommandClass#
typedef enum otTcatCommandClass otTcatCommandClass
Represents a TCAT command class.
otTcatAdvertisedDeviceIdType#
typedef enum otTcatAdvertisedDeviceIdType otTcatAdvertisedDeviceIdType
Represents Advertised Device ID type.
Used during TCAT advertisement.
otTcatGeneralDeviceId#
typedef struct otTcatGeneralDeviceId otTcatGeneralDeviceId
Represents General Device ID type.
otTcatVendorInfo#
typedef struct otTcatVendorInfo otTcatVendorInfo
This structure represents a TCAT vendor information.
The content of this structure MUST persist and remain unchanged while a TCAT session is running.
otHandleTcatApplicationDataReceive#
typedef void(* otHandleTcatApplicationDataReceive) (otInstance *aInstance, const otMessage *aMessage, int32_t aOffset, otTcatApplicationProtocol aTcatApplicationProtocol, void *aContext) )(otInstance *aInstance, const otMessage *aMessage, int32_t aOffset, otTcatApplicationProtocol aTcatApplicationProtocol, void *aContext)
Pointer to call when application data or vendor-specific data was received over a TCAT TLS connection.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | aInstance | A pointer to an OpenThread instance. | |
| [in] | aMessage | A pointer to the message. | |
| [in] | aOffset | The offset where the application data begins. | |
| [in] | aTcatApplicationProtocol | The application protocol the message is targeted to. | |
| [in] | aContext | A pointer to arbitrary context information. |
The application may generate a response to an incoming TCAT application data packet. The TCAT agent automatically responds with status OT_TCAT_STATUS_UNSUPPORTED if no response has been generated or no handler is defined.
otHandleTcatJoin#
typedef void(* otHandleTcatJoin) (otError aError, void *aContext) )(otError aError, void *aContext)
Pointer to call to notify the completion of a network join/leave operation performed under guidance of a TCAT Commissioner.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | aError | OT_ERROR_NONE if the network join/leave operation was successfully started. OT_ERROR_INVALID_STATE if network join was requested but network credentials were missing or incomplete. OT_ERROR_REJECTED if a network join/leave operation was requested, but the TCAT Commissioner is not authorized to make such a request. OT_ERROR_SECURITY is reserved for future use for a failed join due to credential mismatch. | |
| [in] | aContext | A pointer to arbitrary context information. |
Function Documentation#
otBleSecureStart#
otError otBleSecureStart (otInstance * aInstance, otHandleBleSecureConnect aConnectHandler, otHandleBleSecureReceive aReceiveHandler, bool aTlvMode, void * aContext)
Starts the BLE Secure service.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otHandleBleSecureConnect | [in] | aConnectHandler | A pointer to a function that will be called when the connection state changes. |
| otHandleBleSecureReceive | [in] | aReceiveHandler | A pointer to a function that will be called once data has been received over the TLS connection. |
| bool | [in] | aTlvMode | A boolean value indicating if TLV mode (TRUE) shall be activated, or line mode (FALSE). |
| void * | [in] | aContext | A pointer to arbitrary context information. May be NULL if not used. |
When TLV mode is active, the function aReceiveHandler will be called once a complete TLV or line was received and the message offset points to the TLV value.
otBleSecureSetTcatVendorInfo#
otError otBleSecureSetTcatVendorInfo (otInstance * aInstance, const otTcatVendorInfo * aVendorInfo)
Sets TCAT vendor info.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const otTcatVendorInfo * | [in] | aVendorInfo | A pointer to the Vendor Information (MUST remain valid after the method call). |
The vendor info is used for advertising in TCAT Advertisements, as well as for responding to particular TCAT commands that supply vendor info to the TCAT Commissioner.
otBleSecureTcatStart#
otError otBleSecureTcatStart (otInstance * aInstance, otHandleTcatJoin aJoinHandler)
Enables the TCAT protocol over BLE Secure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otHandleTcatJoin | [in] | aJoinHandler | A pointer to a function that is called when a network join or leave operation is requested under guidance of the TCAT Commissioner. |
otBleSecureStop#
void otBleSecureStop (otInstance * aInstance)
Stops the BLE Secure server.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
If the TCAT agent is active, it is also stopped and any ongoing connection is forcibly ended.
otBleSecureSetTcatAgentState#
otError otBleSecureSetTcatAgentState (otInstance * aInstance, bool aActive, uint32_t aDelayMs, uint32_t aDurationMs)
Sets the TCAT agent over BLE Secure into active or standby state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| bool | [in] | aActive | If TRUE, attempts to set TCAT agent to active state. If FALSE, attempts to set TCAT agent to standby (inactive) state. |
| uint32_t | [in] | aDelayMs | Delay in ms before activating TCAT agent. If 0, activate immediately. |
| uint32_t | [in] | aDurationMs | Duration in ms of the activation of the TCAT agent. If 0, activate indefinitely. |
In standby state, no BLE advertisements are sent and TCAT Commissioners can't connect. TCAT can be automatically enabled via a TMF message while in standby.
otBleSecureSetPsk#
void otBleSecureSetPsk (otInstance * aInstance, const uint8_t * aPsk, uint16_t aPskLength, const uint8_t * aPskIdentity, uint16_t aPskIdLength)
Sets the Pre-Shared Key (PSK) and cipher suite TLS_PSK_WITH_AES_128_CCM_8.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const uint8_t * | [in] | aPsk | A pointer to the PSK. |
| uint16_t | [in] | aPskLength | The PSK length. |
| const uint8_t * | [in] | aPskIdentity | The Identity Name for the PSK. |
| uint16_t | [in] | aPskIdLength | The PSK Identity Length. |
Note
Requires the build-time feature
MBEDTLS_KEY_EXCHANGE_PSK_ENABLEDto be enabled.
otBleSecureGetPeerCertificateBase64#
otError otBleSecureGetPeerCertificateBase64 (otInstance * aInstance, unsigned char * aPeerCert, size_t * aCertLength)
Returns the peer x509 certificate base64 encoded.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| unsigned char * | [out] | aPeerCert | A pointer to the base64 encoded certificate buffer. |
| size_t * | [inout] | aCertLength | On input, the size the max size of |
Note
Requires the build-time features
MBEDTLS_BASE64_CandMBEDTLS_SSL_KEEP_PEER_CERTIFICATEto be enabled.
otBleSecureGetPeerCertificateDer#
otError otBleSecureGetPeerCertificateDer (otInstance * aInstance, unsigned char * aPeerCert, size_t * aCertLength)
Returns the DER encoded peer x509 certificate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| unsigned char * | [out] | aPeerCert | A pointer to the DER encoded certificate buffer. |
| size_t * | [inout] | aCertLength | On input, the size the max size of |
Note
Requires the build-time feature
MBEDTLS_SSL_KEEP_PEER_CERTIFICATEto be enabled.
otBleSecureGetPeerSubjectAttributeByOid#
otError otBleSecureGetPeerSubjectAttributeByOid (otInstance * aInstance, const char * aOid, size_t aOidLength, uint8_t * aAttributeBuffer, size_t * aAttributeLength, int * aAsn1Type)
Returns an attribute value identified by its OID from the subject of the peer x509 certificate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const char * | [in] | aOid | A pointer to the OID to be found. |
| size_t | [in] | aOidLength | The length of the OID. |
| uint8_t * | [out] | aAttributeBuffer | A pointer to the attribute buffer. |
| size_t * | [inout] | aAttributeLength | On input, the size the max size of |
| int * | [out] | aAsn1Type | A pointer to the ASN.1 type of the attribute written to the buffer. |
The peer OID is provided in binary format. The attribute length is set if the attribute was successfully read or zero if unsuccessful. The ASN.1 type as is set as defineded in the ITU-T X.690 standard if the attribute was successfully read.
Note
Requires the build-time feature
MBEDTLS_SSL_KEEP_PEER_CERTIFICATEto be enabled.
otBleSecureGetThreadAttributeFromPeerCertificate#
otError otBleSecureGetThreadAttributeFromPeerCertificate (otInstance * aInstance, int aThreadOidDescriptor, uint8_t * aAttributeBuffer, size_t * aAttributeLength)
Returns an attribute value for the OID 1.3.6.1.4.1.44970.x from the v3 extensions of the peer x509 certificate, where the last digit x is set to aThreadOidDescriptor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| int | [in] | aThreadOidDescriptor | The last digit of the Thread attribute OID. |
| uint8_t * | [out] | aAttributeBuffer | A pointer to the attribute buffer. |
| size_t * | [inout] | aAttributeLength | On input, the size the max size of |
The attribute length is set if the attribute was successfully read or zero if unsuccessful. Requires a connection to be active.
Note
Requires the build-time feature
MBEDTLS_SSL_KEEP_PEER_CERTIFICATEto be enabled.
otBleSecureGetThreadAttributeFromOwnCertificate#
otError otBleSecureGetThreadAttributeFromOwnCertificate (otInstance * aInstance, int aThreadOidDescriptor, uint8_t * aAttributeBuffer, size_t * aAttributeLength)
Returns an attribute value for the OID 1.3.6.1.4.1.44970.x from the v3 extensions of the own x509 certificate, where the last digit x is set to aThreadOidDescriptor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| int | [in] | aThreadOidDescriptor | The last digit of the Thread attribute OID. |
| uint8_t * | [out] | aAttributeBuffer | A pointer to the attribute buffer. |
| size_t * | [inout] | aAttributeLength | On input, the size the max size of |
The attribute length is set if the attribute was successfully read or zero if unsuccessful. Requires a connection to be active.
otBleSecureSetSslAuthMode#
void otBleSecureSetSslAuthMode (otInstance * aInstance, bool aVerifyPeerCertificate)
Sets the authentication mode for the BLE secure connection.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| bool | [in] | aVerifyPeerCertificate | true, to verify the peer certificate. |
Disable or enable the verification of peer certificate. Must be called before start.
otBleSecureSetCertificate#
void otBleSecureSetCertificate (otInstance * aInstance, const uint8_t * aX509Cert, uint32_t aX509Length, const uint8_t * aPrivateKey, uint32_t aPrivateKeyLength)
Sets the local device's X509 certificate and corresponding private key.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const uint8_t * | [in] | aX509Cert | A pointer to the PEM formatted X509 certificate. |
| uint32_t | [in] | aX509Length | The length of certificate. |
| const uint8_t * | [in] | aPrivateKey | A pointer to the PEM formatted private key. |
| uint32_t | [in] | aPrivateKeyLength | The length of the private key. |
Used for TLS sessions with cipher suite TLS_ECDHE_ECDSA_WITH_AES_128_GCM_SHA256.
Note
Requires
MBEDTLS_KEY_EXCHANGE_ECDHE_ECDSA_ENABLED=1.
otBleSecureSetCaCertificateChain#
void otBleSecureSetCaCertificateChain (otInstance * aInstance, const uint8_t * aX509CaCertificateChain, uint32_t aX509CaCertChainLength)
Sets the trusted top level CAs.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const uint8_t * | [in] | aX509CaCertificateChain | A pointer to the PEM formatted X509 CA chain. |
| uint32_t | [in] | aX509CaCertChainLength | The length of chain. |
It is needed for validating the certificate of the peer via TLS.
Used for TLS sessions with cipher suite TLS_ECDHE_ECDSA_WITH_AES_128_GCM_SHA256.
Note
Requires
MBEDTLS_KEY_EXCHANGE_ECDHE_ECDSA_ENABLED=1.
otBleSecureConnect#
otError otBleSecureConnect (otInstance * aInstance)
Initializes TLS session with a peer using an already open BLE connection.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
otBleSecureDisconnect#
void otBleSecureDisconnect (otInstance * aInstance)
Stops the BLE and TLS connections.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
otBleSecureIsConnectionActive#
bool otBleSecureIsConnectionActive (otInstance * aInstance)
Indicates whether or not the TLS session is active (connected or connecting).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
otBleSecureIsConnected#
bool otBleSecureIsConnected (otInstance * aInstance)
Indicates whether or not the TLS session is connected.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
otBleSecureIsTcatAgentStarted#
bool otBleSecureIsTcatAgentStarted (otInstance * aInstance)
Indicates whether or not the TCAT agent is started over BLE secure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | N/A | aInstance |
otBleSecureIsCommandClassAuthorized
bool otBleSecureIsCommandClassAuthorized (otInstance * aInstance, otTcatCommandClass aCommandClass)
Indicates whether or not a TCAT command class is authorized for the current TCAT Commissioner.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otTcatCommandClass | [in] | aCommandClass | A command class to check. |
otBleSecureSendMessage#
otError otBleSecureSendMessage (otInstance * aInstance, otMessage * aMessage)
Sends a secure BLE message.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otMessage * | [in] | aMessage | A pointer to the message to send. |
If the return value is OT_ERROR_NONE, OpenThread takes ownership of aMessage, and the caller should no longer reference aMessage. If the return value is not OT_ERROR_NONE, the caller retains ownership of aMessage, including freeing aMessage if the message buffer is no longer needed.
otBleSecureSend#
otError otBleSecureSend (otInstance * aInstance, uint8_t * aBuf, uint16_t aLength)
Sends a secure BLE data packet.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| uint8_t * | [in] | aBuf | A pointer to the data to send as the Value of the TCAT Send Application Data TLV. |
| uint16_t | [in] | aLength | A number indicating the length of the data buffer. |
otBleSecureSendApplicationTlv#
otError otBleSecureSendApplicationTlv (otInstance * aInstance, otTcatApplicationProtocol aApplicationProtocol, uint8_t * aBuf, uint16_t aLength)
Sends a secure BLE data packet containing application data directed to the application layer aApplicationProtocol or a response to the latest received application data packet.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otTcatApplicationProtocol | [in] | aApplicationProtocol | An application protocol the data is directed to. |
| uint8_t * | [in] | aBuf | A pointer to the data to send as the Value of the TCAT Send Application Data TLV. |
| uint16_t | [in] | aLength | A number indicating the length of the data buffer. |
Only a single response can be sent while executing the otHandleBleSecureReceive handler. If no (further) response is expected OT_ERROR_REJECTED is returned.
For responses with a payload aApplicationProtocol shall be set to OT_TCAT_APPLICATION_PROTOCOL_PAYLOAD. For responses with a status aApplicationProtocol shall be OT_TCAT_APPLICATION_PROTOCOL_STATUS and @ aBuf shall contain a single byte otTcatStatusCode value.
otBleSecureFlush#
otError otBleSecureFlush (otInstance * aInstance)
Flushes the send buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
otBleSecureGetInstallCodeVerifyStatus#
bool otBleSecureGetInstallCodeVerifyStatus (otInstance * aInstance)
Gets the Install Code Verify Status during the current session.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Macro Definition Documentation#
OT_TCAT_SERVICE_NAME_MAX_LENGTH#
#define OT_TCAT_SERVICE_NAME_MAX_LENGTHValue:
15
Maximum string length of a UDP or TCP service name (does not include null char).
OT_TCAT_APPLICATION_LAYER_MAX_COUNT#
#define OT_TCAT_APPLICATION_LAYER_MAX_COUNTValue:
4
Maximum number of application layer service names supported.
OT_TCAT_ADVERTISEMENT_MAX_LEN#
#define OT_TCAT_ADVERTISEMENT_MAX_LENValue:
29
Maximum length of TCAT advertisement.
OT_TCAT_MAX_ADVERTISED_DEVICEID_SIZE#
#define OT_TCAT_MAX_ADVERTISED_DEVICEID_SIZEValue:
5
TCAT max size of any type of advertised Device ID.
OT_TCAT_ENABLE_MAX#
#define OT_TCAT_ENABLE_MAXValue:
600
TCAT_ENABLE_MAX, default max TMF TCAT enable time, in seconds.