BLE#

This module includes the platform abstraction for BLE Host communication.

The platform needs to implement Bluetooth LE 4.2 or higher.

Modules#

otBleLinkCapabilities

otBleRadioPacket

Typedefs#

typedef struct otBleLinkCapabilities

Represent BLE link capabilities.

typedef struct otBleRadioPacket

Represents a BLE packet.

Functions#

otPlatBleEnable(otInstance *aInstance)

Enable the Bluetooth Low Energy radio.

otPlatBleDisable(otInstance *aInstance)

Disable the Bluetooth Low Energy radio.

otPlatBleGetAdvertisementBuffer(otInstance *aInstance, uint8_t **aAdvertisementBuffer)

Gets BLE Advertising buffer.

otPlatBleGapAdvSetData(otInstance *aInstance, uint8_t *aAdvertisementData, uint16_t aAdvertisementLen)

Sets BLE Advertising data.

otPlatBleGapAdvUpdateData(otInstance *aInstance, uint8_t *aAdvertisementData, uint16_t aAdvertisementLen)

Updates BLE Advertising data.

otPlatBleGapAdvStart(otInstance *aInstance, uint16_t aInterval)

Starts BLE Advertising procedure.

otPlatBleGapAdvStop(otInstance *aInstance)

Stops BLE Advertising procedure.

void
otPlatBleGapOnConnected(otInstance *aInstance, uint16_t aConnectionId)

The BLE driver calls this method to notify OpenThread that a BLE Central Device has been connected.

void
otPlatBleGapOnDisconnected(otInstance *aInstance, uint16_t aConnectionId)

The BLE driver calls this method to notify OpenThread that the BLE Central Device has been disconnected.

otPlatBleGapDisconnect(otInstance *aInstance)

Disconnects BLE connection.

otPlatBleGattMtuGet(otInstance *aInstance, uint16_t *aMtu)

Reads currently use value of ATT_MTU.

void
otPlatBleGattOnMtuUpdate(otInstance *aInstance, uint16_t aMtu)

The BLE driver calls this method to notify OpenThread that ATT_MTU has been updated.

otPlatBleGattServerIndicate(otInstance *aInstance, uint16_t aHandle, const otBleRadioPacket *aPacket)

Sends ATT Handle Value Indication.

void
otPlatBleGattServerOnWriteRequest(otInstance *aInstance, uint16_t aHandle, const otBleRadioPacket *aPacket)

The BLE driver calls this method to notify OpenThread that an ATT Write Request packet has been received.

void
otPlatBleGetLinkCapabilities(otInstance *aInstance, otBleLinkCapabilities *aBleLinkCapabilities)

Function to retrieve from platform BLE link capabilities.

bool
otPlatBleSupportsMultiRadio(otInstance *aInstance)

Function to retrieve from platform multiradio support of BLE and IEEE.

Macros#

#define

Time slot duration on PHY layer in microseconds (0.625ms).

#define

Minimum allowed interval for advertising packet in OT_BLE_ADV_INTERVAL_UNIT units (20ms).

#define

Maximum allowed interval for advertising packet in OT_BLE_ADV_INTERVAL_UNIT units (10.24s).

#define

Default interval for advertising packet (ms).

#define
OT_BLE_ADV_INTERVAL_UNIT OT_BLE_TIMESLOT_UNIT

Unit used to calculate interval duration (0.625ms).

#define

Maximum allowed ATT MTU size (must be >= 23).

#define

Default power value for BLE.

#define

TOBLE service UUID.

Typedef Documentation#

otBleLinkCapabilities#

typedef struct otBleLinkCapabilities otBleLinkCapabilities

Represent BLE link capabilities.


otBleRadioPacket#

typedef struct otBleRadioPacket otBleRadioPacket

Represents a BLE packet.


Function Documentation#

otPlatBleEnable#

otError otPlatBleEnable (otInstance * aInstance)

Enable the Bluetooth Low Energy radio.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

Note

  • BLE Device should use the highest ATT_MTU supported that does not exceed OT_BLE_ATT_MTU_MAX octets.


otPlatBleDisable#

otError otPlatBleDisable (otInstance * aInstance)

Disable the Bluetooth Low Energy radio.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

When disabled, the BLE stack will flush event queues and not generate new events. The BLE peripheral is turned off or put into a low power sleep state. Any dynamic memory used by the stack should be released, but static memory may remain reserved.


otPlatBleGetAdvertisementBuffer#

otError otPlatBleGetAdvertisementBuffer (otInstance * aInstance, uint8_t ** aAdvertisementBuffer, aAdvertisementLen)

Gets BLE Advertising buffer.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

uint8_t **[in]aAdvertisementBuffer

The formatted TCAT advertisement frame.

[in]aAdvertisementLen

The TCAT advertisement frame length.

Note

  • This function shall be used only for BLE Peripheral role. Returned buffer should have enough space to fit max advertisement defined by specification.


otPlatBleGapAdvSetData#

otError otPlatBleGapAdvSetData (otInstance * aInstance, uint8_t * aAdvertisementData, uint16_t aAdvertisementLen)

Sets BLE Advertising data.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

uint8_t *[in]aAdvertisementData

The formatted TCAT advertisement frame.

uint16_t[in]aAdvertisementLen

The TCAT advertisement frame length.

Note

  • This function shall be used only for BLE Peripheral role.


otPlatBleGapAdvUpdateData#

otError otPlatBleGapAdvUpdateData (otInstance * aInstance, uint8_t * aAdvertisementData, uint16_t aAdvertisementLen)

Updates BLE Advertising data.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

uint8_t *[in]aAdvertisementData

The formatted TCAT advertisement frame.

uint16_t[in]aAdvertisementLen

The TCAT advertisement frame length.

Note

  • This function shall be used only for BLE Peripheral role.


otPlatBleGapAdvStart#

otError otPlatBleGapAdvStart (otInstance * aInstance, uint16_t aInterval)

Starts BLE Advertising procedure.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

uint16_t[in]aInterval

The interval between subsequent advertising packets in OT_BLE_ADV_INTERVAL_UNIT units. Shall be within OT_BLE_ADV_INTERVAL_MIN and OT_BLE_ADV_INTERVAL_MAX range or OT_BLE_ADV_INTERVAL_DEFAULT for a default value set at compile time.

The BLE device shall use undirected advertising with no filter applied. A single BLE Advertising packet must be sent on all advertising channels (37, 38 and 39).

Note

  • This function shall be used only for BLE Peripheral role.


otPlatBleGapAdvStop#

otError otPlatBleGapAdvStop (otInstance * aInstance)

Stops BLE Advertising procedure.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

Note

  • This function shall be used only for BLE Peripheral role.


otPlatBleGapOnConnected#

void otPlatBleGapOnConnected (otInstance * aInstance, uint16_t aConnectionId)

The BLE driver calls this method to notify OpenThread that a BLE Central Device has been connected.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

uint16_t[in]aConnectionId

The identifier of the open connection.


otPlatBleGapOnDisconnected#

void otPlatBleGapOnDisconnected (otInstance * aInstance, uint16_t aConnectionId)

The BLE driver calls this method to notify OpenThread that the BLE Central Device has been disconnected.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

uint16_t[in]aConnectionId

The identifier of the closed connection.


otPlatBleGapDisconnect#

otError otPlatBleGapDisconnect (otInstance * aInstance)

Disconnects BLE connection.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

The BLE device shall use the Remote User Terminated Connection (0x13) reason code when disconnecting from the peer BLE device..


otPlatBleGattMtuGet#

otError otPlatBleGattMtuGet (otInstance * aInstance, uint16_t * aMtu)

Reads currently use value of ATT_MTU.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

uint16_t *[out]aMtu

A pointer to output the current ATT_MTU value.


otPlatBleGattOnMtuUpdate#

void otPlatBleGattOnMtuUpdate (otInstance * aInstance, uint16_t aMtu)

The BLE driver calls this method to notify OpenThread that ATT_MTU has been updated.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

uint16_t[in]aMtu

The updated ATT_MTU value.


otPlatBleGattServerIndicate#

otError otPlatBleGattServerIndicate (otInstance * aInstance, uint16_t aHandle, const otBleRadioPacket * aPacket)

Sends ATT Handle Value Indication.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

uint16_t[in]aHandle

The handle of the attribute to be indicated.

const otBleRadioPacket *[in]aPacket

A pointer to the packet contains value to be indicated.

Note

  • This function shall be used only for GATT Server.


otPlatBleGattServerOnWriteRequest#

void otPlatBleGattServerOnWriteRequest (otInstance * aInstance, uint16_t aHandle, const otBleRadioPacket * aPacket)

The BLE driver calls this method to notify OpenThread that an ATT Write Request packet has been received.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

uint16_t[in]aHandle

The handle of the attribute to be written.

const otBleRadioPacket *[in]aPacket

A pointer to the packet contains value to be written to the attribute.

Note

  • This function shall be used only for GATT Server.


otPlatBleGetLinkCapabilities#

void otPlatBleGetLinkCapabilities (otInstance * aInstance, otBleLinkCapabilities * aBleLinkCapabilities)

Function to retrieve from platform BLE link capabilities.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

otBleLinkCapabilities *[out]aBleLinkCapabilities

The pointer to retrieve the BLE ling capabilities.


otPlatBleSupportsMultiRadio#

bool otPlatBleSupportsMultiRadio (otInstance * aInstance)

Function to retrieve from platform multiradio support of BLE and IEEE.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.


Macro Definition Documentation#

OT_BLE_TIMESLOT_UNIT#

#define OT_BLE_TIMESLOT_UNIT
Value:
625

Time slot duration on PHY layer in microseconds (0.625ms).


OT_BLE_ADV_INTERVAL_MIN#

#define OT_BLE_ADV_INTERVAL_MIN
Value:
0x0020

Minimum allowed interval for advertising packet in OT_BLE_ADV_INTERVAL_UNIT units (20ms).


OT_BLE_ADV_INTERVAL_MAX#

#define OT_BLE_ADV_INTERVAL_MAX
Value:
0x4000

Maximum allowed interval for advertising packet in OT_BLE_ADV_INTERVAL_UNIT units (10.24s).


OT_BLE_ADV_INTERVAL_DEFAULT#

#define OT_BLE_ADV_INTERVAL_DEFAULT
Value:
100

Default interval for advertising packet (ms).


OT_BLE_ADV_INTERVAL_UNIT#

#define OT_BLE_ADV_INTERVAL_UNIT
Value:
OT_BLE_TIMESLOT_UNIT

Unit used to calculate interval duration (0.625ms).


OT_BLE_ATT_MTU_MAX#

#define OT_BLE_ATT_MTU_MAX
Value:
67

Maximum allowed ATT MTU size (must be >= 23).


OT_BLE_DEFAULT_POWER#

#define OT_BLE_DEFAULT_POWER
Value:
0

Default power value for BLE.


OT_TOBLE_SERVICE_UUID#

#define OT_TOBLE_SERVICE_UUID
Value:
0xfffb

TOBLE service UUID.