Silicon Labs
openthread/latest/structotLinkMetrics
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
Results 1-5 of 5 for openthread/latest/structotLinkMetrics in 0.17 seconds
Sleep Timer | API Documentation | Gecko Platform | v4.4.1 | Silicon Labs
https://docs.silabs.com/.../sleepti...
// Gecko Platform//Version 4.4.1 //Services ... .h source files for the SLEEPTIMER device driver library are in the service/ ... All API functions can be called from within interrupt handlers.
SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
https://docs.silabs.com/.../sl-se-mana...
Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Device configuration and utilities (Utilities) ... Reset The device is reset. 7
I/O Stream RTT - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-iostream-...
You can configure the number and size of the ring buffers at compile-time in SEGGER_RTT_Conf.h configuration file. Please refer to Segger's documentation for further information on RTT.
ProductMicrocontrollers Resource TypeSoftware API documentation
UARTDRV - UART Driver - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-uart...
Configuration Options The API Flow Control Support ... [in] type Abort type – whether to abort only Tx, only Rx, or both. ... The UARTDRV device handle used to start the transfer.
ProductMicrocontrollers Resource TypeSoftware API documentation
Project Configurator and Gecko Platform
https://www.silabs.com/.../project-configuration-gecko-platform-training....
P L AT F O R M A N D M C U A P P S | N O V E M B E R 2 0 2 0 ... Gecko Platform –EMLIB Peripheral Library ... Device Init component adds autogen files and function calls to project:
    Results 1-5 of 5 for openthread/latest/structotLinkMetrics