USB DEVICE MICROSOFT XTENDED PROPERTIES DATA TYPE.
USB SETUP REQUEST
Public Attributes#
uint8_t
Characteristics of request.
uint8_t
Specific request.
uint16_t
Varies according to request.
uint16_t
Varies according to request; typically used as index.
uint16_t
Transfer length if data stage present.
Public Attribute Documentation#
bmRequestType#
uint8_t sl_usbd_setup_req_t::bmRequestType
Characteristics of request.
Definition at line
513
of file protocol/usb/inc/sl_usbd_core.h
bRequest#
uint8_t sl_usbd_setup_req_t::bRequest
Specific request.
Definition at line
514
of file protocol/usb/inc/sl_usbd_core.h
wValue#
uint16_t sl_usbd_setup_req_t::wValue
Varies according to request.
Definition at line
515
of file protocol/usb/inc/sl_usbd_core.h
wIndex#
uint16_t sl_usbd_setup_req_t::wIndex
Varies according to request; typically used as index.
Definition at line
516
of file protocol/usb/inc/sl_usbd_core.h
wLength#
uint16_t sl_usbd_setup_req_t::wLength
Transfer length if data stage present.
Definition at line
517
of file protocol/usb/inc/sl_usbd_core.h