MODULE.
INCLUDE FILES DATA TYPES Vendor callbacks
Public Attributes#
void(*
Callback for enable event.
void(*
Callback for disable event.
void(*
Callback for setup req event.
Public Attribute Documentation#
enable#
void(* sl_usbd_vendor_callbacks_t::enable) (uint8_t class_nbr)
Callback for enable event.
Definition at line
54
of file protocol/usb/inc/sl_usbd_class_vendor.h
disable#
void(* sl_usbd_vendor_callbacks_t::disable) (uint8_t class_nbr)
Callback for disable event.
Definition at line
56
of file protocol/usb/inc/sl_usbd_class_vendor.h
setup_req#
void(* sl_usbd_vendor_callbacks_t::setup_req) (uint8_t class_nbr, const sl_usbd_setup_req_t *p_setup_req)
Callback for setup req event.
Definition at line
58
of file protocol/usb/inc/sl_usbd_class_vendor.h