USB Device HID API#

USB Device HID API.

Modules#

sl_usbd_hid_callbacks_t

Enumerations#

enum
SL_USBD_HID_COUNTRY_CODE_NOT_SUPPORTED = 0u
SL_USBD_HID_COUNTRY_CODE_ARABIC = 1u
SL_USBD_HID_COUNTRY_CODE_BELGIAN = 2u
SL_USBD_HID_COUNTRY_CODE_CANADIAN_BILINGUAL = 3u
SL_USBD_HID_COUNTRY_CODE_CANADIAN_FRENCH = 4u
SL_USBD_HID_COUNTRY_CODE_CZECH_REPUBLIC = 5u
SL_USBD_HID_COUNTRY_CODE_DANISH = 6u
SL_USBD_HID_COUNTRY_CODE_FINNISH = 7u
SL_USBD_HID_COUNTRY_CODE_FRENCH = 8u
SL_USBD_HID_COUNTRY_CODE_GERMAN = 9u
SL_USBD_HID_COUNTRY_CODE_GREEK = 10u
SL_USBD_HID_COUNTRY_CODE_HEBREW = 11u
SL_USBD_HID_COUNTRY_CODE_HUNGARY = 12u
SL_USBD_HID_COUNTRY_CODE_INTERNATIONAL = 13u
SL_USBD_HID_COUNTRY_CODE_ITALIAN = 14u
SL_USBD_HID_COUNTRY_CODE_JAPAN_KATAKANA = 15u
SL_USBD_HID_COUNTRY_CODE_KOREAN = 16u
SL_USBD_HID_COUNTRY_CODE_LATIN_AMERICAN = 17u
SL_USBD_HID_COUNTRY_CODE_NETHERLANDS_DUTCH = 18u
SL_USBD_HID_COUNTRY_CODE_NORWEGIAN = 19u
SL_USBD_HID_COUNTRY_CODE_PERSIAN_FARSI = 20u
SL_USBD_HID_COUNTRY_CODE_POLAND = 21u
SL_USBD_HID_COUNTRY_CODE_PORTUGUESE = 22u
SL_USBD_HID_COUNTRY_CODE_RUSSIA = 23u
SL_USBD_HID_COUNTRY_CODE_SLOVAKIA = 24u
SL_USBD_HID_COUNTRY_CODE_SPANISH = 25u
SL_USBD_HID_COUNTRY_CODE_SWEDISH = 26u
SL_USBD_HID_COUNTRY_CODE_SWISS_FRENCH = 27u
SL_USBD_HID_COUNTRY_CODE_SWISS_GERMAN = 28u
SL_USBD_HID_COUNTRY_CODE_SWITZERLAND = 29u
SL_USBD_HID_COUNTRY_CODE_TAIWAN = 30u
SL_USBD_HID_COUNTRY_CODE_TURKISH_Q = 31u
SL_USBD_HID_COUNTRY_CODE_UK = 32u
SL_USBD_HID_COUNTRY_CODE_US = 33u
SL_USBD_HID_COUNTRY_CODE_YUGOSLAVIA = 34u
SL_USBD_HID_COUNTRY_CODE_TURKISH_F = 35u
}

DEFINES.

Typedefs#

typedef void(*
sl_usbd_hid_async_function_t)(uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint32_t xfer_len, void *p_callback_arg, sl_status_t status)

GLOBAL CONSTANTS.

Functions#

sl_status_t

GLOBAL CONSTANTS.

sl_status_t
sl_usbd_hid_create_instance(uint8_t subclass, uint8_t protocol, sl_usbd_hid_country_code_t country_code, uint16_t interval_in, uint16_t interval_out, bool ctrl_rd_en, sl_usbd_hid_callbacks_t *p_hid_callbacks, uint8_t *p_class_nbr)

Add a new instance of the HID class.

sl_status_t
sl_usbd_hid_add_to_configuration(uint8_t class_nbr, uint8_t config_nbr)

Add the HID class instance to the USB device configuration (see Note #1).

sl_status_t
sl_usbd_hid_is_enabled(uint8_t class_nbr, bool *p_enabled)

Get the HID class enable state.

sl_status_t
sl_usbd_hid_write_sync(uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint16_t timeout, uint32_t *p_xfer_len)

Send data to the host through the Interrupt IN endpoint.

sl_status_t
sl_usbd_hid_read_sync(uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint16_t timeout, uint32_t *p_xfer_len)

Receive data from the host through the Interrupt OUT endpoint.

sl_status_t
sl_usbd_hid_read_async(uint8_t class_nbr, void *p_buf, uint32_t buf_len, sl_usbd_hid_async_function_t async_fnct, void *p_async_arg)

Receive data from the host through the Interrupt OUT endpoint.

sl_status_t
sl_usbd_hid_write_async(uint8_t class_nbr, void *p_buf, uint32_t buf_len, sl_usbd_hid_async_function_t async_fnct, void *p_async_arg)

Send data to the host through the Interrupt IN endpoint.

Macros#

#define
SLI_USBD_HID_EXTERN extern

MODULE.

#define
SL_USBD_HID_SUBCLASS_NONE 0x00u

HUMAN INTERFACE DEVICE CLASS SUBCLASS CODES DEFINES.

#define
SL_USBD_HID_SUBCLASS_BOOT 0x01u
#define
SL_USBD_HID_PROTOCOL_NONE 0x00u

HUMAN INTERFACE DEVICE CLASS PROTOCOL CODES DEFINES.

#define
SL_USBD_HID_PROTOCOL_KBD 0x01u
#define
SL_USBD_HID_PROTOCOL_MOUSE 0x02u
#define
SL_USBD_HID_ITEM_LONG 0xFE

ITEM TYPES.

#define
SL_USBD_HID_ITEM_TYPE_MAIN 0x00
#define
SL_USBD_HID_ITEM_TYPE_GLOBAL 0x04
#define
SL_USBD_HID_ITEM_TYPE_LOCAL 0x08
#define
SL_USBD_HID_ITEM_TYPE_RESERVED 0x0C
#define
SL_USBD_HID_MAIN_INPUT 0x80
#define
SL_USBD_HID_MAIN_OUTPUT 0x90
#define
SL_USBD_HID_MAIN_COLLECTION 0xA0
#define
SL_USBD_HID_MAIN_FEATURE 0xB0
#define
SL_USBD_HID_MAIN_ENDCOLLECTION 0xC0
#define
SL_USBD_HID_MAIN_CONSTANT 0x01
#define
SL_USBD_HID_MAIN_DATA 0x00
#define
SL_USBD_HID_MAIN_VARIABLE 0x02
#define
SL_USBD_HID_MAIN_ARRAY 0x00
#define
SL_USBD_HID_MAIN_RELATIVE 0x04
#define
SL_USBD_HID_MAIN_ABSOLUTE 0x00
#define
SL_USBD_HID_MAIN_WRAP 0x08
#define
SL_USBD_HID_MAIN_NOWRAP 0x00
#define
SL_USBD_HID_MAIN_NONLINEAR 0x10
#define
SL_USBD_HID_MAIN_LINEAR 0x00
#define
SL_USBD_HID_MAIN_NOPREFERRED 0x20
#define
SL_USBD_HID_MAIN_PREFERREDSTATE 0x00
#define
SL_USBD_HID_MAIN_NULLSTATE 0x40
#define
SL_USBD_HID_MAIN_NONULLPOSITION 0x00
#define
SL_USBD_HID_MAIN_VOLATILE 0x80
#define
SL_USBD_HID_MAIN_NONVOLATILE 0x00
#define
SL_USBD_HID_MAIN_BUFFEREDBYTES 0x0100
#define
SL_USBD_HID_MAIN_BITFIELD 0x0000
#define
SL_USBD_HID_COLLECTION_PHYSICAL 0x00
#define
SL_USBD_HID_COLLECTION_APPLICATION 0x01
#define
SL_USBD_HID_COLLECTION_LOGICAL 0x02
#define
SL_USBD_HID_COLLECTION_REPORT 0x03
#define
SL_USBD_HID_COLLECTION_NAMEDARRAY 0x04
#define
SL_USBD_HID_COLLECTION_USAGESWITCH 0x05
#define
SL_USBD_HID_COLLECTION_USAGEMODIFIER 0x06
#define
SL_USBD_HID_GLOBAL_USAGE_PAGE 0x04
#define
SL_USBD_HID_GLOBAL_LOG_MIN 0x14
#define
SL_USBD_HID_GLOBAL_LOG_MAX 0x24
#define
SL_USBD_HID_GLOBAL_PHY_MIN 0x34
#define
SL_USBD_HID_GLOBAL_PHY_MAX 0x44
#define
SL_USBD_HID_GLOBAL_UNIT_EXPONENT 0x54
#define
SL_USBD_HID_GLOBAL_UNIT 0x64
#define
SL_USBD_HID_GLOBAL_REPORT_SIZE 0x74
#define
SL_USBD_HID_GLOBAL_REPORT_ID 0x84
#define
SL_USBD_HID_GLOBAL_REPORT_COUNT 0x94
#define
SL_USBD_HID_GLOBAL_PUSH 0xA4
#define
SL_USBD_HID_GLOBAL_POP 0xB4
#define
SL_USBD_HID_LOCAL_USAGE 0x08
#define
SL_USBD_HID_LOCAL_USAGE_MIN 0x18
#define
SL_USBD_HID_LOCAL_USAGE_MAX 0x28
#define
SL_USBD_HID_LOCAL_DESIGNATOR_INDEX 0x38
#define
SL_USBD_HID_LOCAL_DESIGNATOR_MIN 0x48
#define
SL_USBD_HID_LOCAL_DESIGNATOR_MAX 0x58
#define
SL_USBD_HID_LOCAL_STRING_INDEX 0x78
#define
SL_USBD_HID_LOCAL_STRING_MIN 0x88
#define
SL_USBD_HID_LOCAL_STRING_MAX 0x98
#define
SL_USBD_HID_LOCAL_DELIMITER 0xA8
#define
SL_USBD_HID_BIAS_NOT_APPLICABLE 0
                              HID PHYSICAL DESCRIPTOR DEFINES

Note(s) : (1) See 'Device Class Definition for Human Interface Devices Version 1.11', Section 6.2.3.

#define
SL_USBD_HID_BIAS_RIGHT_HAND 1
#define
SL_USBD_HID_BIAS_LEFT_HAND 2
#define
SL_USBD_HID_BIAS_BOTH_HANDS 3
#define
SL_USBD_HID_BIAS_EITHER_HAND 4
#define
SL_USBD_HID_DESIGNATOR_NONE 0x00
#define
SL_USBD_HID_DESIGNATOR_HAND 0x01
#define
SL_USBD_HID_DESIGNATOR_EYEBALL 0x02
#define
SL_USBD_HID_DESIGNATOR_EYEBROW 0x03
#define
SL_USBD_HID_DESIGNATOR_EYELID 0x04
#define
SL_USBD_HID_DESIGNATOR_EAR 0x05
#define
SL_USBD_HID_DESIGNATOR_NOSE 0x06
#define
SL_USBD_HID_DESIGNATOR_MOUTH 0x07
#define
SL_USBD_HID_DESIGNATOR_UPPER_LIP 0x08
#define
SL_USBD_HID_DESIGNATOR_LOWER_LIP 0x09
#define
SL_USBD_HID_DESIGNATOR_JAW 0x0A
#define
SL_USBD_HID_DESIGNATOR_NECK 0x0B
#define
SL_USBD_HID_DESIGNATOR_UPPER_ARM 0x0C
#define
SL_USBD_HID_DESIGNATOR_ELBOW 0x0D
#define
SL_USBD_HID_DESIGNATOR_FOREARM 0x0E
#define
SL_USBD_HID_DESIGNATOR_WRIST 0x0F
#define
SL_USBD_HID_DESIGNATOR_PALM 0x10
#define
SL_USBD_HID_DESIGNATOR_THUMB 0x11
#define
SL_USBD_HID_DESIGNATOR_INDEX_FINGER 0x12
#define
SL_USBD_HID_DESIGNATOR_MIDDLE_FINGER 0x13
#define
SL_USBD_HID_DESIGNATOR_RING_FINGER 0x14
#define
SL_USBD_HID_DESIGNATOR_LITTLE_FINGER 0x15
#define
SL_USBD_HID_DESIGNATOR_HEAD 0x16
#define
SL_USBD_HID_DESIGNATOR_SHOULDER 0x17
#define
SL_USBD_HID_DESIGNATOR_HIP 0x18
#define
SL_USBD_HID_DESIGNATOR_WAIST 0x19
#define
SL_USBD_HID_DESIGNATOR_THIGH 0x1A
#define
SL_USBD_HID_DESIGNATOR_KNEE 0x1B
#define
SL_USBD_HID_DESIGNATOR_CALF 0x1C
#define
SL_USBD_HID_DESIGNATOR_ANKLE 0x1D
#define
SL_USBD_HID_DESIGNATOR_FOOT 0x1E
#define
SL_USBD_HID_DESIGNATOR_HEEL 0x1F
#define
SL_USBD_HID_DESIGNATOR_BALL_OF_FOOT 0x20
#define
SL_USBD_HID_DESIGNATOR_BIG_TOE 0x21
#define
SL_USBD_HID_DESIGNATOR_SECOND_TOE 0x22
#define
SL_USBD_HID_DESIGNATOR_THIRD_TOE 0x23
#define
SL_USBD_HID_DESIGNATOR_FOURTH_TOE 0x24
#define
SL_USBD_HID_DESIGNATOR_LITTLE_TOE 0x25
#define
SL_USBD_HID_DESIGNATOR_BROW 0x26
#define
SL_USBD_HID_DESIGNATOR_CHEEK 0x27
#define
SL_USBD_HID_QUALIFIER_NOT_APPLICABLE 0
#define
SL_USBD_HID_QUALIFIER_RIGHT 1
#define
SL_USBD_HID_QUALIFIER_LEFT 2
#define
SL_USBD_HID_QUALIFIER_BOTH 3
#define
SL_USBD_HID_QUALIFIER_EITHER 4
#define
SL_USBD_HID_QUALIFIER_CENTER 5
#define
SL_USBD_HID_USAGE_PAGE_UNDEFINED 0x00
                                      HID USAGE PAGES

Note(s) : (1) See 'Universal Serial Bus HID Usage Tables', Version 1.12, Section 3 for more details about Usage Pages.

(2) See 'Universal Serial Bus HID Usage Tables', Version 1.12, Section 4 for more details about Generic Desktop Page usages and controls.

#define
SL_USBD_HID_USAGE_PAGE_GENERIC_DESKTOP_CONTROLS 0x01
#define
SL_USBD_HID_USAGE_PAGE_SIMULATION_CONTROLS 0x02
#define
SL_USBD_HID_USAGE_PAGE_VR_CONTROLS 0x03
#define
SL_USBD_HID_USAGE_PAGE_SPORT_CONTROLS 0x04
#define
SL_USBD_HID_USAGE_PAGE_GAME_CONTROLS 0x05
#define
SL_USBD_HID_USAGE_PAGE_GENERIC_DEVICE_CONTROLS 0x06
#define
SL_USBD_HID_USAGE_PAGE_KEYBOARD 0x07
#define
SL_USBD_HID_USAGE_PAGE_LEDS 0x08
#define
SL_USBD_HID_USAGE_PAGE_BUTTON 0x09
#define
SL_USBD_HID_USAGE_PAGE_ORDINAL 0x0A
#define
SL_USBD_HID_USAGE_PAGE_TELEPHONY 0x0B
#define
SL_USBD_HID_USAGE_PAGE_CONSUMER 0x0C
#define
SL_USBD_HID_USAGE_PAGE_DIGITIZER 0x0D
#define
SL_USBD_HID_USAGE_PAGE_PID_PAGE 0x0F
#define
SL_USBD_HID_USAGE_PAGE_UNICODE 0x10
#define
SL_USBD_HID_USAGE_PAGE_ALPHANUMERIC_DISPLAY 0x14
#define
SL_USBD_HID_USAGE_PAGE_MEDICAL_INSTRUMENTS 0x40
#define
SL_USBD_HID_USAGE_PAGE_MONITOR_0 0x80
#define
SL_USBD_HID_USAGE_PAGE_MONITOR_1 0x81
#define
SL_USBD_HID_USAGE_PAGE_MONITOR_2 0x82
#define
SL_USBD_HID_USAGE_PAGE_MONITOR_3 0x83
#define
SL_USBD_HID_USAGE_PAGE_POWER_0 0x84
#define
SL_USBD_HID_USAGE_PAGE_POWER_1 0x85
#define
SL_USBD_HID_USAGE_PAGE_POWER_2 0x86
#define
SL_USBD_HID_USAGE_PAGE_POWER_3 0x87
#define
SL_USBD_HID_USAGE_PAGE_BAR_CODE_SCANNER_PAGE 0x8C
#define
SL_USBD_HID_USAGE_PAGE_SCALE_PAGE 0x8D
#define
SL_USBD_HID_USAGE_PAGE_MSR_DEVICES 0x8E
#define
SL_USBD_HID_USAGE_PAGE_POINT_OF_SALE_PAGES 0x8F
#define
SL_USBD_HID_USAGE_PAGE_CAMERA_CONTROL_PAGE 0x90
#define
SL_USBD_HID_USAGE_PAGE_ARCADE_PAGE 0x91
#define
SL_USBD_HID_CP_POINTER 0x01
#define
SL_USBD_HID_CA_MOUSE 0x02
#define
SL_USBD_HID_CA_JOYSTICK 0x04
#define
SL_USBD_HID_CA_GAME_PAD 0x05
#define
SL_USBD_HID_CA_KEYBOARD 0x06
#define
SL_USBD_HID_CA_KEYPAD 0x07
#define
SL_USBD_HID_CA_MULTI_AXIS_CONTROLLER 0x08
#define
SL_USBD_HID_DV_X 0x30
#define
SL_USBD_HID_DV_Y 0x31
#define
SL_USBD_HID_DV_Z 0x32
#define
SL_USBD_HID_DV_WHEEL 0x38
#define
SL_USBD_HID_CA_SYSTEM_CONTROL 0x80

Enumeration Documentation#

sl_usbd_hid_country_code_t#

sl_usbd_hid_country_code_t

DEFINES.

                     HUMAN INTERFACE DEVICE COUNTRY CODES DEFINES

Note(s) : (1) See 'Device Class Definition for Human Interface Devices (HID), 6/27/01, Version 1.11', section 6.2.1 for more details about HID descriptor country code.

(a) The country code identifies which country the hardware is localized for. Most hardware is not localized and thus this value would be zero (0). However, keyboards may use the field to indicate the language of the key caps.

Enumerator
SL_USBD_HID_COUNTRY_CODE_NOT_SUPPORTED
SL_USBD_HID_COUNTRY_CODE_ARABIC
SL_USBD_HID_COUNTRY_CODE_BELGIAN
SL_USBD_HID_COUNTRY_CODE_CANADIAN_BILINGUAL
SL_USBD_HID_COUNTRY_CODE_CANADIAN_FRENCH
SL_USBD_HID_COUNTRY_CODE_CZECH_REPUBLIC
SL_USBD_HID_COUNTRY_CODE_DANISH
SL_USBD_HID_COUNTRY_CODE_FINNISH
SL_USBD_HID_COUNTRY_CODE_FRENCH
SL_USBD_HID_COUNTRY_CODE_GERMAN
SL_USBD_HID_COUNTRY_CODE_GREEK
SL_USBD_HID_COUNTRY_CODE_HEBREW
SL_USBD_HID_COUNTRY_CODE_HUNGARY
SL_USBD_HID_COUNTRY_CODE_INTERNATIONAL
SL_USBD_HID_COUNTRY_CODE_ITALIAN
SL_USBD_HID_COUNTRY_CODE_JAPAN_KATAKANA
SL_USBD_HID_COUNTRY_CODE_KOREAN
SL_USBD_HID_COUNTRY_CODE_LATIN_AMERICAN
SL_USBD_HID_COUNTRY_CODE_NETHERLANDS_DUTCH
SL_USBD_HID_COUNTRY_CODE_NORWEGIAN
SL_USBD_HID_COUNTRY_CODE_PERSIAN_FARSI
SL_USBD_HID_COUNTRY_CODE_POLAND
SL_USBD_HID_COUNTRY_CODE_PORTUGUESE
SL_USBD_HID_COUNTRY_CODE_RUSSIA
SL_USBD_HID_COUNTRY_CODE_SLOVAKIA
SL_USBD_HID_COUNTRY_CODE_SPANISH
SL_USBD_HID_COUNTRY_CODE_SWEDISH
SL_USBD_HID_COUNTRY_CODE_SWISS_FRENCH
SL_USBD_HID_COUNTRY_CODE_SWISS_GERMAN
SL_USBD_HID_COUNTRY_CODE_SWITZERLAND
SL_USBD_HID_COUNTRY_CODE_TAIWAN
SL_USBD_HID_COUNTRY_CODE_TURKISH_Q
SL_USBD_HID_COUNTRY_CODE_UK
SL_USBD_HID_COUNTRY_CODE_US
SL_USBD_HID_COUNTRY_CODE_YUGOSLAVIA
SL_USBD_HID_COUNTRY_CODE_TURKISH_F

Typedef Documentation#

sl_usbd_hid_async_function_t#

typedef void(* sl_usbd_hid_async_function_t) (uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint32_t xfer_len, void *p_callback_arg, sl_status_t status) )(uint8_t class_nbr, void *p_buf, uint32_t buf_len, uint32_t xfer_len, void *p_callback_arg, sl_status_t status)

GLOBAL CONSTANTS.

DATA TYPES Async comm callback


Function Documentation#

sl_usbd_hid_init#

sl_status_t sl_usbd_hid_init (void )

GLOBAL CONSTANTS.

Parameters
TypeDirectionArgument NameDescription
voidN/A

FUNCTION PROTOTYPES HID FUNCTIONS

Initialize HID class.

Returns

  • Returns SL_STATUS_OK on success or another SL_STATUS code on failure.


sl_usbd_hid_create_instance#

sl_status_t sl_usbd_hid_create_instance (uint8_t subclass, uint8_t protocol, sl_usbd_hid_country_code_t country_code, uint16_t interval_in, uint16_t interval_out, bool ctrl_rd_en, sl_usbd_hid_callbacks_t * p_hid_callbacks, uint8_t * p_class_nbr)

Add a new instance of the HID class.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Asubclass

Subclass code.

uint8_tN/Aprotocol

protocol code.

sl_usbd_hid_country_code_tN/Acountry_code

Country code id.

uint16_tN/Ainterval_in

Polling interval for input transfers, in milliseconds. It must be a power of 2.

uint16_tN/Ainterval_out

Polling interval for output transfers, in milliseconds. It must be a power of 2. Used only when read operations are not through control transfers.

boolN/Actrl_rd_en

Enable read operations through the control transfers.

sl_usbd_hid_callbacks_t *N/Ap_hid_callbacks

Pointer to HID descriptor and request callback structure. [Content MUST be persistent]

uint8_t *N/Ap_class_nbr

Pointer to variable that will receive class instance number. The variable is set to class instance number if no errors are returned, otherwise it is set to SL_USBD_CLASS_NBR_NONE.

Returns

  • Returns SL_STATUS_OK on success or another SL_STATUS code on failure.


sl_usbd_hid_add_to_configuration#

sl_status_t sl_usbd_hid_add_to_configuration (uint8_t class_nbr, uint8_t config_nbr)

Add the HID class instance to the USB device configuration (see Note #1).

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aclass_nbr

Class instance number.

uint8_tN/Aconfig_nbr

Configuration index to add HID class instance to.

Returns

  • Returns SL_STATUS_OK on success or another SL_STATUS code on failure.

Note

  • (1) Called several times, it creates multiple instances and configurations. For instance, the following architecture could be created :

    *               FS
    *               |-- Configuration 0 (HID class 0)
    *                                   (HID class 1)
    *                                   (HID class 2)
    *                   |-- Interface 0
    *               |-- Configuration 1 (HID class 0)
    *                   |-- Interface 0
    *               
  • (2) Configuration Descriptor corresponding to a HID device uses the following format :

    *               Configuration Descriptor
    *               |-- Interface Descriptor (HID class)
    *                   |-- Endpoint Descriptor (Interrupt IN)
    *                   |-- Endpoint Descriptor (Interrupt OUT) - optional
    *               

sl_usbd_hid_is_enabled#

sl_status_t sl_usbd_hid_is_enabled (uint8_t class_nbr, bool * p_enabled)

Get the HID class enable state.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aclass_nbr

Class instance number.

bool *N/Ap_enabled

Pointer to a variable that will receive HID class enable state. The variable is set to true if HID class is enabled, and is set to false if it is NOT enabled.

Returns

  • Returns SL_STATUS_OK on success or another SL_STATUS code on failure.


sl_usbd_hid_write_sync#

sl_status_t sl_usbd_hid_write_sync (uint8_t class_nbr, void * p_buf, uint32_t buf_len, uint16_t timeout, uint32_t * p_xfer_len)

Send data to the host through the Interrupt IN endpoint.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aclass_nbr

Class instance number.

void *N/Ap_buf

Pointer to the transmit buffer. If more than one input report exists, the first byte must represent the report id.

uint32_tN/Abuf_len

Transmit buffer length, in octets.

uint16_tN/Atimeout

Timeout in milliseconds.

uint32_t *N/Ap_xfer_len

Pointer to a variable that will receive transfer length. The variable is set to number of octets received, if no errors are returned, or is set to 0 if any errors are returned.

This function is blocking.

Returns

  • Returns SL_STATUS_OK on success or another SL_STATUS code on failure.


sl_usbd_hid_read_sync#

sl_status_t sl_usbd_hid_read_sync (uint8_t class_nbr, void * p_buf, uint32_t buf_len, uint16_t timeout, uint32_t * p_xfer_len)

Receive data from the host through the Interrupt OUT endpoint.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aclass_nbr

Class instance number.

void *N/Ap_buf

Pointer to the receive buffer.

uint32_tN/Abuf_len

Receive the buffer length, in octets.

uint16_tN/Atimeout

Timeout, in milliseconds.

uint32_t *N/Ap_xfer_len

Pointer to a variable that will receive transfer length. The variable is set to number of octets received, if no errors are returned, or is set to 0 if any errors are returned.

This function is blocking.

Returns

  • Returns SL_STATUS_OK on success or another SL_STATUS code on failure.


sl_usbd_hid_read_async#

sl_status_t sl_usbd_hid_read_async (uint8_t class_nbr, void * p_buf, uint32_t buf_len, sl_usbd_hid_async_function_t async_fnct, void * p_async_arg)

Receive data from the host through the Interrupt OUT endpoint.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aclass_nbr

Class instance number.

void *N/Ap_buf

Pointer to receive buffer.

uint32_tN/Abuf_len

Receive buffer length, in octets.

sl_usbd_hid_async_function_tN/Aasync_fnct

Receive callback.

void *N/Ap_async_arg

Additional argument provided by application for receive callback.

This function is non-blocking and returns immediately after transfer preparation. Upon transfer completion, the provided callback is called to notify the application.

Returns

  • Returns SL_STATUS_OK on success or another SL_STATUS code on failure.


sl_usbd_hid_write_async#

sl_status_t sl_usbd_hid_write_async (uint8_t class_nbr, void * p_buf, uint32_t buf_len, sl_usbd_hid_async_function_t async_fnct, void * p_async_arg)

Send data to the host through the Interrupt IN endpoint.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aclass_nbr

Class instance number.

void *N/Ap_buf

Pointer to transmit buffer. If more than one input report exists, the first byte must represent the report id.

uint32_tN/Abuf_len

Transmit buffer length, in octets.

sl_usbd_hid_async_function_tN/Aasync_fnct

Transmit callback.

void *N/Ap_async_arg

Additional argument provided by application for transmit callback.

This function is non-blocking, and returns immediately after transfer preparation. Upon transfer completion, the provided callback is called to notify the application.

Returns

  • Returns SL_STATUS_OK on success or another SL_STATUS code on failure.