RAIL_TxPowerConfig_t Struct Reference

A structure containing values used to initialize the power amplifiers.

#include < rail_chip_specific.h >

Data Fields

RAIL_TxPowerMode_t mode
TX power mode.
uint16_t voltage
Power amplifier supply voltage in mV, generally: DCDC supply ~ 1800 mV (1.8 V) Battery supply ~ 3300 mV (3.3 V)
uint16_t rampTime
The amount of time to spend ramping for TX in uS.

A structure containing values used to initialize the power amplifiers.

Definition at line 782 of file rail_chip_specific.h .

Field Documentation

◆ rampTime

uint16_t RAIL_TxPowerConfig_t::rampTime

The amount of time to spend ramping for TX in uS.

Definition at line 791 of file rail_chip_specific.h .


The documentation for this struct was generated from the following file:
  • chip/efr32/efr32xg1x/ rail_chip_specific.h