Wireless M-Bus Thermometer Sensor#
The Wireless M-Bus Thermometer Sensor component is designed to monitor and measure temperature using a thermometer sensor. This component provides the necessary tools to integrate temperature data into Wireless M-Bus packets, ensuring that the data is correctly formatted and transmitted.
Key Features:
Temperature Measurement: Functions to measure temperature using a thermometer sensor.
Data Handling: Functions to retrieve and format temperature data for inclusion in Wireless M-Bus packets.
Packet Assembly: Tools to assemble packets with temperature data, ensuring that the data is correctly formatted and transmitted.
Modules#
Functions#
Wireless M-Bus Thermometer initialization function.
Wireless M-Bus Thermometer deinitialization function.
Wireless M-Bus Thermometer measure function function.
Retrieves the sensor data for the Wireless M-Bus thermo meter sensor.
Wireless M-Bus Thermometer 7 segment LCD print function.
Wireless M-Bus Thermometer button pressed function.
Function Documentation#
sl_rail_sdk_wmbus_sensor_thermometer_init#
sl_status_t sl_rail_sdk_wmbus_sensor_thermometer_init (void )
Wireless M-Bus Thermometer initialization function.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns
sl_status_t: SL_STATUS_OK if init was successful SL_STATUS_FAIL if init failed
sl_rail_sdk_wmbus_sensor_thermometer_deinit#
sl_status_t sl_rail_sdk_wmbus_sensor_thermometer_deinit (void )
Wireless M-Bus Thermometer deinitialization function.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns
sl_status_t: SL_STATUS_OK if init was successful SL_STATUS_FAIL if init failed
sl_rail_sdk_wmbus_sensor_thermometer_measure#
sl_status_t sl_rail_sdk_wmbus_sensor_thermometer_measure (void )
Wireless M-Bus Thermometer measure function function.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Read sensor data.
Returns
sl_status_t: SL_STATUS_OK if measure was successful SL_STATUS_FAIL if measure failed
sl_rail_sdk_wmbus_sensor_thermometer_get_data#
sl_rail_sdk_wmbus_sensor_data_t * sl_rail_sdk_wmbus_sensor_thermometer_get_data (void )
Retrieves the sensor data for the Wireless M-Bus thermo meter sensor.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns a pointer to the sl_rail_sdk_wmbus_sensor_data_t structure that contains the sensor data for the Wireless M-Bus thermo meter sensor.
Returns
Pointer to a sl_rail_sdk_wmbus_sensor_data_t, the sensor data for the Wireless M-Bus thermo meter sensor
sl_rail_sdk_wmbus_sensor_thermometer_print#
sl_status_t sl_rail_sdk_wmbus_sensor_thermometer_print (void )
Wireless M-Bus Thermometer 7 segment LCD print function.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns
sl_status_t: SL_STATUS_OK if measure was successful SL_STATUS_FAIL if measure failed
sl_rail_sdk_wmbus_sensor_thermometer_button_pressed
sl_status_t sl_rail_sdk_wmbus_sensor_thermometer_button_pressed (void )
Wireless M-Bus Thermometer button pressed function.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
This function handles the button press event for the Wireless M-Bus thermo meter sensor, in this case, it changes the displayed value between temperature and humidity.
Returns
sl_status_t: SL_STATUS_OK if measure was successful SL_STATUS_FAIL if measure failed