Channel Selector#
The RAIL Channel Selector component allows the application to dynamically select the communication channel at both compile-time and runtime. This flexibility is crucial for applications that need to operate on different channels based on environmental conditions or regulatory requirements. The component provides functions to set and get the selected channel, ensuring that the application can easily switch channels as needed.
Key functions include:
set_selected_channel(): Sets the communication channel.
get_selected_channel(): Retrieves the current communication channel.
restart_rx_channel(): Restarts the RX operation on the selected channel.
Modules#
Functions#
Sets the configured channel using the DEFAULT_CHANNEL define.
Sets which channel the app will communicate on.
Get which channel the app will communicate on.
Restarts the RX operation on the selected channel.
Function Documentation#
set_configured_channel#
void set_configured_channel (void )
Sets the configured channel using the DEFAULT_CHANNEL define.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Sets the configured channel to DEFAULT_CHANNEL
set_selected_channel#
uint8_t set_selected_channel (uint16_t new_channel)
Sets which channel the app will communicate on.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | new_channel | requested new channel number |
Tests the channel number with configured channel limits from radio configurator, if it is invalid first valid channel will be used. Also restarts the receiving by calling restart_rx_channel()
Returns
1 if channel number is valid else 0
get_selected_channel#
uint16_t get_selected_channel (void )
Get which channel the app will communicate on.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
current channel number used for communication
restart_rx_channel#
RAIL_Status_t restart_rx_channel (void )
Restarts the RX operation on the selected channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
status of the RAIL_StartRx() function