TrustZone#
APIs to use RAIL with TrustZone enabled and peripherals configured as secure.
RAIL internally accesses CMU, EMU, GPIO, LDMA, HFXO, PRS and SYSRTC. If some of them are configured as secure peripherals, some RAIL code must be executed as secure code. To do so, callbacks gathered in RAIL_TZ_Config_t must be implemented and passed to RAIL through RAIL_TZ_InitNonSecure(). Each callback must do the non-secure/secure transition, call RAIL_TZ_CheckPeripheralsSecureStates() and then call the corresponding RAIL API from secure world:
RAIL internally calls platform functions that access CMU, EMU, GPIO, LDMA HFXO and PRS. If some of them are configured as secure peripherals, some functions must be executed as secure code. To do so, those functions are prepended with weak symbols and must be overwritten to do the non-secure/secure transition and call the corresponding platform function from secure world:
Secure peripheral  | Platform functions to overwrite  | 
|---|---|
CMU  | CMU_ClockEnable, EMU_DCDCSetPFMXTimeoutMaxCtrl (DCDC access: SL_TRUSTZONE_PERIPHERAL_DCDC_S)  | 
HFXO  | CMU_HFXOCTuneSet, CMU_HFXOCTuneGet, CMU_HFXOCoreBiasCurrentCalibrate  | 
PRS  | PRS_SourceAsyncSignalSet, PRS_GetFreeChannel, PRS_ConnectConsumer, PRS_PinOutput, PRS_Combine  | 
When there is a combination of secure and non-secure peripherals, defines must be added in secure application slcp file so non-secure peripherals can properly accessed by secure code. Example with only CMU non-secure:
define:
  - name: SL_TRUSTZONE_PERIPHERAL_CMU_S
    value: 0
    condition: [trustzone_secure]
  - name: SL_TRUSTZONE_PERIPHERAL_EMU_S
    value: 1
    condition: [trustzone_secure]
  - name: SL_TRUSTZONE_PERIPHERAL_GPIO_S
    value: 1
    condition: [trustzone_secure]
  - name: SL_TRUSTZONE_PERIPHERAL_LDMA_S
    value: 1
    condition: [trustzone_secure]
  - name: SL_TRUSTZONE_PERIPHERAL_HFXO0_S
    value: 1
    condition: [trustzone_secure]
  - name: SL_TRUSTZONE_PERIPHERAL_PRS_S
    value: 1
    condition: [trustzone_secure]
  - name: SL_TRUSTZONE_PERIPHERAL_SYSRTC_S
    value: 1
    condition: [trustzone_secure]
Some RAIL API are not suppoted with EMU, GPIO, LDMA, HFXO, PRS or SYSRTC configured secure:
Modules#
Typedefs#
A pointer to the callback used to switch to secure world and run RAIL_ChangedDcdc().
A pointer to the callback used to switch to secure world and run RAIL_TZ_ConfigAntennaGpio().
A pointer to the callback used to switch to secure world and run RAIL_TZ_RadioClockEnable().
A pointer to the callback used to switch to secure world and run RAIL_GetRadioClockFreqHz().
A pointer to the callback used to switch to secure world and run RAIL_TZ_RfecaClockEnable().
A pointer to the callback used to switch to secure world and run RAIL_TZ_RfecaIsClockEnabled().
A pointer to the callback used to switch to secure world and run RAIL_TZ_ReadInternalTemperature().
A pointer to the callback used to switch to secure world and run RAIL_TZ_EnableSecureRadioIrqs().
A pointer to the callback used to switch to secure world and run RAIL_TZ_DisableSecureRadioIrqs().
A pointer to the callback used to switch to secure world and run RAIL_TZ_RadioPerformM2mLdma().
A pointer to the callback used to switch to secure world and run RAIL_TZ_ConfigureHfxo().
Functions#
Init RAIL TrustZone feature for non-secure world.
Init RAIL TrustZone feature for secure world.
Check the secure state of peripherals used by RAIL.
Enable radio clocks.
Enable RFECA clocks.
Indicate whether RFECA clocks are enabled.
Read the internal temperature.
Enable secure peripheral interrupts needed by the radio.
Disable secure peripheral interrupts needed by the radio.
Perform ldma transfer for the radio.
Configure HFXO.
Set GPIO for antenna config.
Typedef Documentation#
RAIL_TZ_ChangedDcdcCallbackPtr_t#
RAIL_TZ_ChangedDcdcCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_ChangedDcdc().
Returns
Status code indicating success of the function call.
RAIL_TZ_ConfigAntennaGpioCallbackPtr_t#
RAIL_TZ_ConfigAntennaGpioCallbackPtr_t )(const RAIL_AntennaConfig_t *config)
A pointer to the callback used to switch to secure world and run RAIL_TZ_ConfigAntennaGpio().
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| [in] | config | A pointer to a configuration structure applied to the relevant Antenna Configuration registers. A NULL configuration will produce undefined behavior.  | 
Returns
Status code indicating success of the function call.
RAIL_TZ_RadioClockEnableCallbackPtr_t#
RAIL_TZ_RadioClockEnableCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_RadioClockEnable().
RAIL_TZ_GetRadioClockFreqHzCallbackPtr_t#
RAIL_TZ_GetRadioClockFreqHzCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_GetRadioClockFreqHz().
Returns
Radio subsystem clock frequency in Hz.
RAIL_TZ_RfecaClockEnableCallbackPtr_t#
RAIL_TZ_RfecaClockEnableCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_RfecaClockEnable().
RAIL_TZ_RfecaIsClockEnabledCallbackPtr_t#
RAIL_TZ_RfecaIsClockEnabledCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_RfecaIsClockEnabled().
Returns
true if RFECA clocks are enabled; false otherwise
RAIL_TZ_ReadInternalTemperatureCallbackPtr_t#
RAIL_TZ_ReadInternalTemperatureCallbackPtr_t )(uint16_t *internalTemperatureKelvin, bool enableTemperatureInterrupts)
A pointer to the callback used to switch to secure world and run RAIL_TZ_ReadInternalTemperature().
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| [out] | internalTemperatureKelvin | A pointer to the internal temperature in Kelvin.  | |
| [in] | enableTemperatureInterrupts | Indicate whether temperature interrupts are enabled.  | 
Returns
Status code indicating success of the function call.
RAIL_TZ_EnableSecureRadioIrqsCallbackPtr_t#
RAIL_TZ_EnableSecureRadioIrqsCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_EnableSecureRadioIrqs().
RAIL_TZ_DisableSecureRadioIrqsCallbackPtr_t#
RAIL_TZ_DisableSecureRadioIrqsCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_DisableSecureRadioIrqs().
RAIL_TZ_RadioPerformM2mLdmaCallbackPtr_t#
RAIL_TZ_RadioPerformM2mLdmaCallbackPtr_t )(uint32_t *pDest, const uint32_t *pSrc, uint32_t numWords)
A pointer to the callback used to switch to secure world and run RAIL_TZ_RadioPerformM2mLdma().
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| [in] | pDest | A pointer to the destination data.  | |
| [in] | pSrc | A pointer to the source data.  | |
| [in] | numWords | Number of words to transfer.  | 
Returns
Status code indicating success of the function call.
RAIL_TZ_ConfigureHfxoCallbackPtr_t#
RAIL_TZ_ConfigureHfxoCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_ConfigureHfxo().
Function Documentation#
RAIL_TZ_InitNonSecure#
RAIL_Status_t RAIL_TZ_InitNonSecure (const RAIL_TZ_Config_t * pTzConfig)
Init RAIL TrustZone feature for non-secure world.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| const RAIL_TZ_Config_t * | [in] | pTzConfig | A non-NULL pointer to a RAIL_TZ_Config_t structure.  | 
Returns
Status code indicating success of the function call.
Note
This function must only be called from non-secure world (only if TrustZone is activated) on platforms having RAIL_SUPPORTS_TRUSTZONE_SECURE_PERIPHERALS. It must be called before RAIL_Init() and it must be called again with updated RAIL_TZ_Config_t if peripherals secure configuration has changed.
RAIL_TZ_InitSecure#
RAIL_Status_t RAIL_TZ_InitSecure (void )
Init RAIL TrustZone feature for secure world.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world (only if TrustZone is activated) on platforms having RAIL_SUPPORTS_TRUSTZONE_SECURE_PERIPHERALS. It must be called before starting the non-secure application.
RAIL_TZ_CheckPeripheralsSecureStates#
RAIL_Status_t RAIL_TZ_CheckPeripheralsSecureStates (void )
Check the secure state of peripherals used by RAIL.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world and it must be called at the beginning of each RAIL TrustZone callbacks (RAIL_TZ_Config_t) secure code to avoid secure fault.
RAIL_TZ_RadioClockEnable#
RAIL_Status_t RAIL_TZ_RadioClockEnable (void )
Enable radio clocks.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when CMU is configured as secure TrustZone peripheral.
RAIL_TZ_RfecaClockEnable#
RAIL_Status_t RAIL_TZ_RfecaClockEnable (void )
Enable RFECA clocks.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when CMU is configured as secure TrustZone peripheral.
RAIL_TZ_RfecaIsClockEnabled#
bool RAIL_TZ_RfecaIsClockEnabled (void )
Indicate whether RFECA clocks are enabled.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
true if RFECA clocks are enabled; false otherwise
Note
This function must only be called from secure world when CMU is configured as secure TrustZone peripheral.
RAIL_TZ_ReadInternalTemperature#
RAIL_Status_t RAIL_TZ_ReadInternalTemperature (uint16_t * internalTemperatureKelvin, bool enableTemperatureInterrupts)
Read the internal temperature.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t * | [out] | internalTemperatureKelvin | A pointer to the internal temperature in Kelvin.  | 
| bool | [in] | enableTemperatureInterrupts | Indicate whether temperature interrupts are enabled.  | 
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when EMU is configured as secure TrustZone peripheral.
RAIL_TZ_EnableSecureRadioIrqs#
RAIL_Status_t RAIL_TZ_EnableSecureRadioIrqs (void )
Enable secure peripheral interrupts needed by the radio.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when EMU is configured as secure TrustZone peripheral.
RAIL_TZ_DisableSecureRadioIrqs#
RAIL_Status_t RAIL_TZ_DisableSecureRadioIrqs (void )
Disable secure peripheral interrupts needed by the radio.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when EMU is configured as secure TrustZone peripheral.
RAIL_TZ_RadioPerformM2mLdma#
RAIL_Status_t RAIL_TZ_RadioPerformM2mLdma (uint32_t * pDest, const uint32_t * pSrc, uint32_t numWords)
Perform ldma transfer for the radio.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t * | [in] | pDest | A pointer to the destination data.  | 
| const uint32_t * | [in] | pSrc | A pointer to the source data.  | 
| uint32_t | [in] | numWords | Number of words to transfer.  | 
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when LDMA is configured as secure TrustZone peripheral.
RAIL_TZ_ConfigureHfxo#
RAIL_Status_t RAIL_TZ_ConfigureHfxo (void )
Configure HFXO.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when HFXO is configured as secure TrustZone peripheral.
RAIL_TZ_ConfigAntennaGpio#
RAIL_Status_t RAIL_TZ_ConfigAntennaGpio (const RAIL_AntennaConfig_t * config)
Set GPIO for antenna config.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| const RAIL_AntennaConfig_t * | [in] | config | A pointer to a configuration structure applied to the relevant Antenna Configuration registers. A NULL configuration will produce undefined behavior.  | 
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when CMU or GPIO are configured as secure TrustZone peripheral.