Data Management

Data management functions.

Data Structures

struct RAIL_DataConfig_t
RAIL data configuration structure.

Enumerations

enum RAIL_TxDataSource_t { TX_PACKET_DATA }
Transmit data sources supported by RAIL.
enum RAIL_RxDataSource_t {
RX_PACKET_DATA ,
RX_DEMOD_DATA ,
RX_IQDATA_FILTLSB ,
RX_IQDATA_FILTMSB
}
Receive data sources supported by RAIL.
enum RAIL_DataMethod_t {
PACKET_MODE ,
FIFO_MODE
}
Methods for the application to provide and retrieve data from RAIL.

Functions

RAIL_Status_t RAIL_ConfigData ( RAIL_Handle_t railHandle, const RAIL_DataConfig_t *dataConfig)
RAIL data management configuration.
uint16_t RAIL_WriteTxFifo ( RAIL_Handle_t railHandle, const uint8_t *dataPtr, uint16_t writeLength, bool reset)
Writes data to the transmit FIFO.
uint16_t RAIL_SetTxFifo ( RAIL_Handle_t railHandle, uint8_t *addr, uint16_t initLength, uint16_t size)
Set the address of the TX FIFO, a circular buffer used for TX data.
uint16_t RAIL_ReadRxFifo ( RAIL_Handle_t railHandle, uint8_t *dataPtr, uint16_t readLength)
Reads packet data from RAIL's internal receive FIFO buffer.
uint16_t RAIL_SetTxFifoThreshold ( RAIL_Handle_t railHandle, uint16_t txThreshold)
Configures the RAIL transmit FIFO almost empty threshold.
uint16_t RAIL_SetRxFifoThreshold ( RAIL_Handle_t railHandle, uint16_t rxThreshold)
Configures the RAIL receive FIFO almost full threshold.
uint16_t RAIL_GetTxFifoThreshold ( RAIL_Handle_t railHandle)
Gets the RAIL transmit FIFO almost empty threshold value.
uint16_t RAIL_GetRxFifoThreshold ( RAIL_Handle_t railHandle)
Gets the RAIL receive FIFO almost full threshold value.
void RAIL_ResetFifo ( RAIL_Handle_t railHandle, bool txFifo, bool rxFifo)
Resets the RAIL FIFOs.
uint16_t RAIL_GetRxFifoBytesAvailable ( RAIL_Handle_t railHandle)
Get the number of bytes available in the receive FIFO.
uint16_t RAIL_GetTxFifoSpaceAvailable ( RAIL_Handle_t railHandle)
Gets the number of bytes open in the transmit FIFO.

Detailed Description

Data management functions.

These functions allow the application to choose how data is presented to the application. RAIL provides data in a packet-based method or in a FIFO-based method which gives the application more granularity and responsibility in managing transmit and receive data, and allows packet sizes larger than the RX or TX FIFO buffers.

The application can configure RAIL data management through RAIL_ConfigData() . This function allows the application to specify the type of radio data ( RAIL_TxDataSource_t and RAIL_RxDataSource_t ) and the method of interacting with data ( RAIL_DataMethod_t ). By default, RAIL configures TX and RX both with packet data source and packet mode.

In packet based data management:

In FIFO based data management:

When trying to determine an appropriate threshold, the application needs to know each FIFO's size. The receive FIFO is internal to RAIL and its size is 512 bytes. The receive FIFO is level-based in that the RAIL_EVENT_RX_FIFO_ALMOST_FULL event will constantly pend if the threshold is exceeded. This normally means that inside this event's callback, the application should empty enough of the FIFO to go under the threshold. To defer reading the FIFO to main context, the application can disable or re-enable the receive FIFO threshold event using RAIL_ConfigEvents() with the mask RAIL_EVENT_RX_FIFO_ALMOST_FULL .

The transmit FIFO is specified by the application and its actual size is the value returned from the most recent call to RAIL_SetTxFifo() , The transmit FIFO is edge-based in that it only provides the RAIL_EVENT_TX_FIFO_ALMOST_EMPTY event once when the threshold is crossed in the emptying direction.

In FIFO mode, the FIFOs can store multiple packets. Depending on the traffic, RAIL can receive multiple packets into the receive FIFO before the application gets around to reading out the received data from the FIFO. RAIL_ReadRxFifo() won't allow reading beyond a packet boundary so process packet completion events promptly. Keep in mind that in FIFO mode, packet data already read from packets that are subsequently aborted, frameerror, or filtered should be flushed.

While RAIL defaults to packet mode, the application can explicitly initialize RAIL for packet mode in the following manner:

static const RAIL_DataConfig_t railDataConfig = {
.rxSource = RX_PACKET_DATA ,
.txMethod = PACKET_MODE ,
.rxMethod = PACKET_MODE ,
};
status = RAIL_ConfigData (&railDataConfig);
// Events that can occur in Packet Mode:
and optionally (packet data automatically dropped):

Initializing RAIL for FIFO Mode requires a few more function calls:

static const RAIL_DataConfig_t railDataConfig = {
.rxSource = RX_PACKET_DATA ,
.txMethod = FIFO_MODE ,
.rxMethod = FIFO_MODE ,
};
status = RAIL_ConfigData (&railDataConfig);
// Gets the size of the FIFOs.
// The transmit and receive FIFOs are the same size
uint16_t fifoSize = RAIL_GetTxFifoSpaceAvailable ();
// Sets the transmit and receive FIFO thresholds.
// For this example, set the threshold in the middle of each FIFO
// Events that can occur in FIFO mode:

On receive, an application can use multiple data sources that are only compatible with the FIFO method of data delivery. All that differs from the FIFO mode example above is the RAIL_DataConfig_t::rxSource setting. IQ data samples are taken at the hardware's oversample rate and the amount of data can easily overwhelm the CPU processing time. The sample rate depends on the chosen PHY, as determined by the data rate and the decimation chain. It is not recommended to use the IQ data source with sample rates above 300 k samples/second as the CPU might not be able to keep up with the data. Depending on the application and needed CPU bandwidth, slower data rates may be required.

// IQ data is provided into the receive FIFO
static const RAIL_DataConfig_t railDataConfig = {
.rxSource = RX_IQDATA_FILTLSB ,
.txMethod = FIFO_MODE ,
.rxMethod = FIFO_MODE ,
};
// When reading IQ data out of the FIFO, it comes in the following format:
//------------------------------------
// I[LSB] | I[MSB] | Q[LSB] | Q[MSB] |
//------------------------------------
Note
RAIL_DataConfig_t::txMethod and RAIL_DataConfig_t::rxMethod must have the same RAIL_DataMethod_t configuration.
Warning
Do not call RAIL_ReadRxFifo() function while in RAIL_DataMethod_t::PACKET_MODE .

Enumeration Type Documentation

RAIL_DataMethod_t

Methods for the application to provide and retrieve data from RAIL.

Enumerator
PACKET_MODE

Packet-based data method.

FIFO_MODE

FIFO-based data method.

Definition at line 1335 of file rail_types.h .

RAIL_RxDataSource_t

Receive data sources supported by RAIL.

Enumerator
RX_PACKET_DATA

Uses the frame hardware to packetize data.

RX_DEMOD_DATA

Gets 8-bit data output from the demodulator.

RX_IQDATA_FILTLSB

Gets lower 16 bits of I/Q data provided to the demodulator.

RX_IQDATA_FILTMSB

Gets highest 16 bits of I/Q data provided to the demodulator.

Definition at line 1322 of file rail_types.h .

RAIL_TxDataSource_t

Transmit data sources supported by RAIL.

Enumerator
TX_PACKET_DATA

Uses the frame hardware to packetize data.

Definition at line 1314 of file rail_types.h .

Function Documentation

RAIL_ConfigData()

RAIL_Status_t RAIL_ConfigData ( RAIL_Handle_t railHandle,
const RAIL_DataConfig_t * dataConfig
)

RAIL data management configuration.

Parameters
[in] railHandle A RAIL instance handle.
[in] dataConfig RAIL data configuration structure.
Returns
Status code indicating success of the function call.

This function configures how RAIL manages data. The application can configure RAIL to receive data in a packet-based or FIFO-based format. FIFO mode is necessary to support packets larger than the radio's FIFO buffers.

With FIFO mode, the application sets appropriate FIFO thresholds via RAIL_SetTxFifoThreshold() and RAIL_SetRxFifoThreshold() , and then enables and handles the RAIL_EVENT_TX_FIFO_ALMOST_EMPTY event callback (to feed more packet data via RAIL_WriteTxFifo() before the FIFO underflows), and the RAIL_EVENT_RX_FIFO_ALMOST_FULL event callback (to consume packet data via RAIL_ReadRxFifo() before the RX FIFO overflows).

When configuring TX or RX for FIFO mode, this function resets the configured FIFOs. When configuring TX or RX for Packet mode, this function will reset the corresponding FIFO thresholds such that they won't trigger the RAIL_EVENT_RX_FIFO_ALMOST_FULL or RAIL_EVENT_TX_FIFO_ALMOST_EMPTY events.

When RAIL_DataConfig_t::rxMethod is set to RAIL_DataMethod_t::FIFO_MODE , the radio won't drop packet data of aborted or CRC error packets, but will present it to the application to deal with accordingly. On completion of such erroneous packets, the RAIL_Config_t::eventsCallback with RAIL_EVENT_RX_PACKET_ABORTED , RAIL_EVENT_RX_FRAME_ERROR , or RAIL_EVENT_RX_ADDRESS_FILTERED will tell the application it can drop any data it read via RAIL_ReadRxFifo() during reception. For CRC error packets when the RAIL_RX_OPTION_IGNORE_CRC_ERRORS RX option is in effect, the application would check for that from the RAIL_RxPacketStatus_t obtained by calling RAIL_GetRxPacketInfo() . RAIL will automatically flush any remaining packet data after reporting one of these packet completion events, or the application can explicitly flush it by calling RAIL_ReleaseRxPacket() .

When RAIL_DataConfig_t::rxMethod is set to RAIL_DataMethod_t::PACKET_MODE , the radio will drop all packet data associated with aborted packets including those with CRC errors (unless configured to ignore CRC errors via the RAIL_RX_OPTION_IGNORE_CRC_ERRORS RX option). The application will never be bothered to deal with packet data from such packets.

In either mode, the application can set RX options as needed, and packet details are not available for aborted packets.

RAIL_GetRxFifoBytesAvailable()

uint16_t RAIL_GetRxFifoBytesAvailable ( RAIL_Handle_t railHandle )

Get the number of bytes available in the receive FIFO.

This function should only be used in RX FIFO mode; apps should probably be using RAIL_GetRxPacketInfo() instead.

Parameters
[in] railHandle A RAIL instance handle.
Returns
Number of raw bytes in the receive FIFO.
Note
The number of bytes returned may not just reflect the current packet's data but could also include raw appended info bytes added after successful packet reception and bytes from subsequently received packets. It is up to the app to never try to consume more than the packet's actual data when using the value returned here in a subsequent call to RAIL_ReadRxFifo() , otherwise the Rx buffer will be corrupted.

RAIL_GetRxFifoThreshold()

uint16_t RAIL_GetRxFifoThreshold ( RAIL_Handle_t railHandle )

Gets the RAIL receive FIFO almost full threshold value.

Parameters
[in] railHandle A RAIL instance handle.
Returns
Configured RX Threshold value.

Retrieves the configured RX threshold value.

RAIL_GetTxFifoSpaceAvailable()

uint16_t RAIL_GetTxFifoSpaceAvailable ( RAIL_Handle_t railHandle )

Gets the number of bytes open in the transmit FIFO.

Parameters
[in] railHandle A RAIL instance handle.
Returns
Number of bytes open in the transmit FIFO.

Gets the number of bytes open in the transmit FIFO.

RAIL_GetTxFifoThreshold()

uint16_t RAIL_GetTxFifoThreshold ( RAIL_Handle_t railHandle )

Gets the RAIL transmit FIFO almost empty threshold value.

Parameters
[in] railHandle A RAIL instance handle.
Returns
Configured TX Threshold value.

Retrieves the configured TX threshold value.

RAIL_ReadRxFifo()

uint16_t RAIL_ReadRxFifo ( RAIL_Handle_t railHandle,
uint8_t * dataPtr,
uint16_t readLength
)

Reads packet data from RAIL's internal receive FIFO buffer.

This function can be used in any RX mode, though in Packet mode it can only be used on the oldest unreleased packet whose RAIL_RxPacketStatus_t is among the RAIL_RX_PACKET_READY_ set.

Parameters
[in] railHandle A RAIL instance handle.
[out] dataPtr An application-provided pointer to store data. If NULL, the data is thrown away rather than copied out.
[in] readLength A number of packet bytes to read from the FIFO.
Returns
The number of packet bytes read from the receive FIFO.

This function reads packet data from the head of receive FIFO and writes it to the provided dataPtr. It does not permit reading more data than is available in the FIFO, nor does it permit reading more data than remains in the oldest unreleased packet.

Because this function does not have a critical section, either use it only in one context or make sure function calls are protected to prevent buffer corruption.

Note
When reading data from an arriving packet that is not yet complete keep in mind its data is highly suspect because it has not yet passed any CRC integrity checking. Also note the packet could be aborted, cancelled, or fail momentarily, invalidating its data in Packet mode. Furthermore, there is a small chance towards the end of packet reception that the RX FIFO could include not only packet data received so far, but also some raw radio-appended info detail bytes that RAIL's packet-completion processing will subsequently deal with. It's up to the application to know its packet format well enough to avoid reading this info as it will corrupt the packet's details and possibly corrupt the RX FIFO buffer.

RAIL_ResetFifo()

void RAIL_ResetFifo ( RAIL_Handle_t railHandle,
bool txFifo,
bool rxFifo
)

Resets the RAIL FIFOs.

Parameters
[in] railHandle A RAIL instance handle.
[in] txFifo If true, reset the transmit FIFO.
[in] rxFifo If true, reset the receive FIFO.
Returns
void.

This function can reset each FIFO. The application should not reset the RX FIFO while receiving a frame.

RAIL_SetRxFifoThreshold()

uint16_t RAIL_SetRxFifoThreshold ( RAIL_Handle_t railHandle,
uint16_t rxThreshold
)

Configures the RAIL receive FIFO almost full threshold.

Parameters
[in] railHandle A RAIL instance handle.
[in] rxThreshold The threshold once exceeded will fire RAIL_Config_t::eventsCallback with RAIL_EVENT_RX_FIFO_ALMOST_FULL set.
Returns
Configured receive FIFO threshold value.

This function configures the threshold for the receive FIFO. When the count of the receive FIFO is greater than the configured threshold, RAIL_Config_t::eventsCallback will fire with RAIL_EVENT_RX_FIFO_ALMOST_FULL set. A value of 0xFFFF is invalid and will not change the current configuration. Depending on the size of the receive FIFO hardware, the maximum value can vary. If the rxThreshold value exceeds the capability of the hardware, the RX threshold will be configured so that it fires only when the FIFO is one byte away from being full.

RAIL_SetTxFifo()

uint16_t RAIL_SetTxFifo ( RAIL_Handle_t railHandle,
uint8_t * addr,
uint16_t initLength,
uint16_t size
)

Set the address of the TX FIFO, a circular buffer used for TX data.

Parameters
[in] railHandle A RAIL instance handle.
[in,out] addr Pointer to a read-write memory location in RAM used as the TX FIFO. This memory must persist until the next call to this function.
[in] initLength Number of initial bytes already in the TX FIFO.
[in] size Desired size of the TX FIFO in bytes.
Returns
Returns the FIFO size in bytes that has been set.

This function is used to set the memory location for the TX FIFO. This function must be called at least once before any transmit operations occur.

The FIFO size can be determined by the return value of this function. The chosen size is determined based on the available FIFO sizes supported by the hardware. For more on supported FIFO sizes see chip-specific documentation, such as EFR32 . The returned FIFO size will be the closest allowed size less than or equal to the passed in size parameter, unless the size parameter is smaller than the minimum FIFO size. If the initLength parameter is larger than the returned size, than the FIFO will be full up to its size.

User may write to the custom memory location directly before calling this function, or use RAIL_WriteTxFifo to write to the memory location after calling this function. For previously-written memory to be set in the TX FIFO, user must specify its initLength.

This function reserves the block of RAM starting at txBufPtr with a length of the returned FIFO size. That RAM block is used internally as a circular buffer for the transmit FIFO. The FIFO must be able to hold the entire FIFO size. The caller must guarantee the custom FIFO remains intact and unchanged (except via calls to RAIL_WriteTxFifo ) until the next call to this function.

Note
It is the protocol's packet configuration, as set up by the radio configurator or via RAIL_SetFixedLength() , that determines how many bytes of data are consumed from the TX FIFO for a successful transmit operation, not the initLength value passed in. If not enough data has been put into the TX FIFO, a RAIL_EVENT_TX_UNDERFLOW event will occur. If too much data, the extra data will either become the first bytes sent in a subsequent packet, or will be thrown away if the FIFO gets reset prior to the next transmit. In general, the proper number of packet bytes to put into the TX FIFO are all payload bytes except for any CRC bytes which the packet configuration would cause to be sent automatically.

RAIL_SetTxFifoThreshold()

uint16_t RAIL_SetTxFifoThreshold ( RAIL_Handle_t railHandle,
uint16_t txThreshold
)

Configures the RAIL transmit FIFO almost empty threshold.

Parameters
[in] railHandle A RAIL instance handle.
[in] txThreshold The threshold once fallen under will fire RAIL_Config_t::eventsCallback with RAIL_EVENT_TX_FIFO_ALMOST_EMPTY set.
Returns
Configured transmit FIFO threshold value.

This function configures the threshold for the transmit FIFO. When the count of the transmit FIFO is less than the configured threshold, RAIL_Config_t::eventsCallback will fire with RAIL_EVENT_TX_FIFO_ALMOST_EMPTY set. A value of 0 is invalid and will not change the current configuration.

RAIL_WriteTxFifo()

uint16_t RAIL_WriteTxFifo ( RAIL_Handle_t railHandle,
const uint8_t * dataPtr,
uint16_t writeLength,
bool reset
)

Writes data to the transmit FIFO.

Parameters
[in] railHandle A RAIL instance handle.
[in] dataPtr Application provided pointer to transmit data
[in] writeLength Number of bytes to write to the transmit FIFO
[in] reset If true resets TX FIFO before writing the data.
Returns
The number of bytes written to the transmit FIFO.

This function reads data from the provided dataPtr and writes it to the TX FIFO. If the requested writeLength exceeds the current number of bytes open in the transmit FIFO, the function only writes until the transmit FIFO is full. The function returns the number of bytes written to the transmit FIFO, and returns zero if railHandle is NULL or if the TX FIFO is full.

Note
It is the protocol's packet configuration, as set up by the radio configurator or via RAIL_SetFixedLength() , that determines how many bytes of data are consumed from the TX FIFO for a successful transmit operation, not the writeLength value passed in. If not enough data has been put into the TX FIFO, a RAIL_EVENT_TX_UNDERFLOW event will occur. If too much data, the extra data will either become the first bytes sent in a subsequent packet, or will be thrown away if the FIFO gets reset prior to the next transmit. In general, the proper number of packet bytes to put into the TX FIFO are all payload bytes except for any CRC bytes which the packet configuration would cause to be sent automatically.
This function does not create a critical section but, depending on the application, a critical section could be appropriate.