State Transitions
Data Structures |
|
struct | RAIL_StateTransitions_t |
Used to specify radio states to transition to on success or failure.
|
|
struct | RAIL_StateTiming_t |
Timing configuration structure for the RAIL State Machine.
|
Enumerations |
|
enum |
RAIL_RadioState_t
{
RAIL_RF_STATE_INACTIVE = 0u, RAIL_RF_STATE_ACTIVE = (1u << 0), RAIL_RF_STATE_RX = (1u << 1), RAIL_RF_STATE_TX = (1u << 2), RAIL_RF_STATE_IDLE = (RAIL_RF_STATE_ACTIVE), RAIL_RF_STATE_RX_ACTIVE = (RAIL_RF_STATE_RX | RAIL_RF_STATE_ACTIVE), RAIL_RF_STATE_TX_ACTIVE = (RAIL_RF_STATE_TX | RAIL_RF_STATE_ACTIVE) } |
The state of the radio.
|
|
enum |
RAIL_IdleMode_t
{
RAIL_IDLE , RAIL_IDLE_ABORT , RAIL_IDLE_FORCE_SHUTDOWN , RAIL_IDLE_FORCE_SHUTDOWN_CLEAR_FLAGS } |
Enumeration for the different types of supported idle modes.
|
Functions |
|
RAIL_Status_t | RAIL_SetRxTransitions ( RAIL_Handle_t railHandle, const RAIL_StateTransitions_t *transitions) |
Configures RAIL automatic state transitions after RX.
|
|
RAIL_Status_t | RAIL_SetTxTransitions ( RAIL_Handle_t railHandle, const RAIL_StateTransitions_t *transitions) |
Configures RAIL automatic state transitions after TX.
|
|
RAIL_Status_t | RAIL_SetStateTiming ( RAIL_Handle_t railHandle, RAIL_StateTiming_t *timings) |
Configures RAIL automatic state transition timing.
|
|
void | RAIL_Idle ( RAIL_Handle_t railHandle, RAIL_IdleMode_t mode, bool wait) |
Places the radio into an idle state.
|
|
RAIL_RadioState_t | RAIL_GetRadioState ( RAIL_Handle_t railHandle) |
Gets the current radio state.
|
Enumeration Type Documentation
◆ RAIL_IdleMode_t
enum RAIL_IdleMode_t |
Enumeration for the different types of supported idle modes.
These vary how quickly and destructively they put the radio into idle.
Enumerator | |
---|---|
RAIL_IDLE |
Idles the radio by turning off receive and canceling any future scheduled receive or transmit operations. It does not abort a receive or transmit in progress. |
RAIL_IDLE_ABORT |
Idles the radio by turning off receive and any scheduled events. It also aborts any receive, transmit, or scheduled events in progress. |
RAIL_IDLE_FORCE_SHUTDOWN |
Forces the radio into a shutdown mode as quickly as possible. It aborts all current operations and cancels any pending scheduled operations. It may also corrupt receive or transmit buffers and end up clearing them. |
RAIL_IDLE_FORCE_SHUTDOWN_CLEAR_FLAGS |
Similar to the RAIL_IDLE_FORCE_SHUTDOWN command, it quickly puts the radio into idle state. Additionally, it clears any pending receive or transmit callbacks and clear both the receive and transmit storage. |
Definition at line
1423
of file
rail_types.h
.
◆ RAIL_RadioState_t
enum RAIL_RadioState_t |
The state of the radio.
Definition at line
1368
of file
rail_types.h
.
Function Documentation
◆ RAIL_GetRadioState()
RAIL_RadioState_t RAIL_GetRadioState | ( | RAIL_Handle_t |
railHandle
|
) |
Gets the current radio state.
- Parameters
-
[in] railHandle
A RAIL instance handle.
- Returns
- An enumeration for the current radio state.
Returns the state of the radio as a bitmask containing: RAIL_RF_STATE_IDLE , RAIL_RF_STATE_RX , RAIL_RF_STATE_TX , and RAIL_RF_STATE_ACTIVE . RAIL_RF_STATE_IDLE , RAIL_RF_STATE_RX , and RAIL_RF_STATE_TX bits are mutually exclusive. The radio can transition through intermediate states, which are not reported but are instead bucketed into the state being transitioned into. For example, when the transmitter is in the process of shutting down, this function will return TX, as if the shutdown process hadn't started yet.
◆ RAIL_Idle()
void RAIL_Idle | ( | RAIL_Handle_t |
railHandle,
|
RAIL_IdleMode_t |
mode,
|
||
bool |
wait
|
||
) |
Places the radio into an idle state.
- Parameters
-
[in] railHandle
A RAIL instance handle. [in] mode
The method for shutting down the radio. [in] wait
Whether this function should wait for the radio to reach idle before returning.
- Returns
- void.
This function is used to remove the radio from TX and RX states. How these states are left is defined by the mode parameter.
In multiprotocol, this API will also cause the radio to be yielded so that other tasks can be run. See Yielding the radio for more details.
◆ RAIL_SetRxTransitions()
RAIL_Status_t RAIL_SetRxTransitions | ( | RAIL_Handle_t |
railHandle,
|
const RAIL_StateTransitions_t * |
transitions
|
||
) |
Configures RAIL automatic state transitions after RX.
- Parameters
-
[in] railHandle
A RAIL instance handle. [in] transitions
The state transitions to apply after reception.
- Returns
- Status code indicating success of the function call.
This function fails if unsupported transitions are passed in or if the radio is currently in the RX state. Success can transition to TX, RX, or IDLE, while error can transition to RX or IDLE.
◆ RAIL_SetStateTiming()
RAIL_Status_t RAIL_SetStateTiming | ( | RAIL_Handle_t |
railHandle,
|
RAIL_StateTiming_t * |
timings
|
||
) |
Configures RAIL automatic state transition timing.
- Parameters
-
[in] railHandle
A RAIL instance handle. [in,out] timings
The timings used to configure the RAIL state machine. This structure is overwritten with the actual times that were set, if an input timing is invalid.
- Returns
- Status code indicating a success of the function call.
The timings given are close to the actual transition time. However, a still uncharacterized software overhead occurs. Also, timings are not always adhered to when using an automatic transition after an error, due to the cleanup required to recover from the error.
◆ RAIL_SetTxTransitions()
RAIL_Status_t RAIL_SetTxTransitions | ( | RAIL_Handle_t |
railHandle,
|
const RAIL_StateTransitions_t * |
transitions
|
||
) |
Configures RAIL automatic state transitions after TX.
- Parameters
-
[in] railHandle
A RAIL instance handle. [in] transitions
The state transitions to apply after transmission.
- Returns
- Status code indicating a success of the function call.
This function fails if unsupported transitions are passed in or if the radio is currently in the TX state. Success and error can each transition to RX or IDLE.