RAIL_Config_t Struct Reference
RAIL configuration and internal state structure.
#include <
rail_chip_specific.h
>
Data Fields |
|
| void(* | eventsCallback )( RAIL_Handle_t railHandle, RAIL_Events_t events) |
|
A pointer to a function, which is called whenever a RAIL event occurs.
|
|
| void * | protocol |
|
A pointer to a protocol-specific state structure allocated in global read-write memory and initialized to all zeros.
|
|
| RAILSched_Config_t * | scheduler |
|
A pointer to a RAIL scheduler state object allocated in global read-write memory and initialized to all zeros.
|
|
RAIL_StateBuffer_t
|
buffer |
|
A structure for RAIL to maintain its internal state, which must be initialized to all zeros.
|
|
RAIL configuration and internal state structure.
This structure must be allocated in application global read-write memory that persists for the duration of RAIL usage. It cannot be allocated in read-only memory or on the call stack.
Definition at line
145
of file
rail_chip_specific.h
.
Field Documentation
| void(* RAIL_Config_t::eventsCallback) ( RAIL_Handle_t railHandle, RAIL_Events_t events) |
A pointer to a function, which is called whenever a RAIL event occurs.
- Parameters
-
[in] railHandleA handle for a RAIL instance. [in] eventsA bit mask of RAIL events.
- Returns
- void.
See the RAIL_Events_t documentation for the list of RAIL events.
Definition at line
155
of file
rail_chip_specific.h
.
| void* RAIL_Config_t::protocol |
A pointer to a protocol-specific state structure allocated in global read-write memory and initialized to all zeros.
For the BLE protocol, it should point to a RAIL_BLE_State_t structure. For IEEE802154, it should be NULL.
Definition at line
162
of file
rail_chip_specific.h
.
| RAILSched_Config_t * RAIL_Config_t::scheduler |
A pointer to a RAIL scheduler state object allocated in global read-write memory and initialized to all zeros.
When not using a multiprotocol scheduler, it should be NULL.
Definition at line
168
of file
rail_chip_specific.h
.
The documentation for this struct was generated from the following file:
-
chip/efr32/
rail_chip_specific.h