Receive
APIs related to packet receive.
Modules |
|
| Address Filtering | |
|
Configuration APIs for receive packet address filtering.
|
|
Data Structures |
|
| struct | RAIL_ScheduleRxConfig_t |
|
Configures the scheduled RX algorithm.
|
|
| struct | RAIL_RxPacketInfo_t |
|
Basic information about a packet being received or already completed and awaiting processing, including memory pointers to its data in the circular receive FIFO buffer.
|
|
| struct | RAIL_RxPacketDetails_t |
|
Received packet details obtained via
RAIL_GetRxPacketDetails()
or
RAIL_GetRxPacketDetailsAlt()
.
|
|
Macros |
|
| #define | RAIL_RX_OPTIONS_NONE 0 |
|
A value representing no options enabled.
|
|
| #define | RAIL_RX_OPTIONS_DEFAULT RAIL_RX_OPTIONS_NONE |
|
All options are disabled by default.
|
|
| #define | RAIL_RX_OPTION_STORE_CRC (1UL << RAIL_RX_OPTION_STORE_CRC_SHIFT) |
|
An option to configure whether the CRC portion of the packet is included in the packet payload exposed to the app on packet reception.
|
|
| #define | RAIL_RX_OPTION_IGNORE_CRC_ERRORS (1UL << RAIL_RX_OPTION_IGNORE_CRC_ERRORS_SHIFT) |
|
An option to configure whether CRC errors will be ignored.
|
|
| #define | RAIL_RX_OPTION_ENABLE_DUALSYNC (1UL << RAIL_RX_OPTION_ENABLE_DUALSYNC_SHIFT) |
|
An option to control which sync words will be accepted.
|
|
| #define | RAIL_RX_OPTION_TRACK_ABORTED_FRAMES (1UL << RAIL_RX_OPTION_TRACK_ABORTED_FRAMES_SHIFT) |
|
An option to configure whether frames which are aborted during reception should continue to be tracked.
|
|
| #define | RAIL_RX_OPTION_REMOVE_APPENDED_INFO (1UL << RAIL_RX_OPTION_REMOVE_APPENDED_INFO_SHIFT) |
|
An option to suppress capturing the appended information after received frames.
|
|
| #define | RAIL_RX_OPTION_ANTENNA0 (1UL << RAIL_RX_OPTION_ANTENNA0_SHIFT) |
|
An option to select the use of antenna 0 when doing RX.
|
|
| #define | RAIL_RX_OPTION_ANTENNA1 (1UL << RAIL_RX_OPTION_ANTENNA1_SHIFT) |
|
An option to select the use of antenna 1 when doing RX.
|
|
| #define | RAIL_RX_OPTION_ANTENNA_AUTO ( RAIL_RX_OPTION_ANTENNA0 | RAIL_RX_OPTION_ANTENNA1 ) |
|
Am option to automatically choose an antenna.
|
|
| #define | RAIL_RX_OPTION_DISABLE_FRAME_DETECTION (1UL << RAIL_RX_OPTION_DISABLE_FRAME_DETECTION_SHIFT) |
|
An option to disable frame detection.
|
|
| #define | RAIL_RX_OPTIONS_ALL 0xFFFFFFFFUL |
|
A value representing all possible options.
|
|
| #define | RAIL_RSSI_INVALID_DBM (-128) |
|
The value returned by RAIL for an invalid RSSI, in dBm.
|
|
| #define | RAIL_RSSI_INVALID ((int16_t)( RAIL_RSSI_INVALID_DBM * 4)) |
|
The value returned by RAIL for an invalid RSSI: in quarter dBm.
|
|
| #define | RAIL_RX_PACKET_HANDLE_INVALID (NULL) |
|
An invalid RX packet handle value.
|
|
| #define | RAIL_RX_PACKET_HANDLE_OLDEST (( RAIL_RxPacketHandle_t ) 1) |
|
A special RX packet handle to refer to the oldest unreleased packet.
|
|
| #define | RAIL_RX_PACKET_HANDLE_NEWEST (( RAIL_RxPacketHandle_t ) 2) |
|
A special RX packet handle to refer to the newest unreleased packet when in callback context.
|
|
Typedefs |
|
| typedef const void * | RAIL_RxPacketHandle_t |
|
A handle used to reference a packet during reception processing.
|
|
| typedef uint8_t(* | RAIL_ConvertLqiCallback_t ) (uint8_t lqi, int8_t rssi) |
|
A pointer to a funcation called before LQI is copied into the
RAIL_RxPacketDetails_t
structure.
|
|
Enumerations |
|
| enum |
RAIL_RxOptions_t
{
RAIL_RX_OPTION_STORE_CRC_SHIFT = 0, RAIL_RX_OPTION_IGNORE_CRC_ERRORS_SHIFT , RAIL_RX_OPTION_ENABLE_DUALSYNC_SHIFT , RAIL_RX_OPTION_TRACK_ABORTED_FRAMES_SHIFT , RAIL_RX_OPTION_REMOVE_APPENDED_INFO_SHIFT , RAIL_RX_OPTION_ANTENNA0_SHIFT , RAIL_RX_OPTION_ANTENNA1_SHIFT , RAIL_RX_OPTION_DISABLE_FRAME_DETECTION_SHIFT } |
|
Receive options, in reality a bitmask.
|
|
| enum |
RAIL_RxPacketStatus_t
{
RAIL_RX_PACKET_NONE = 0, RAIL_RX_PACKET_ABORT_FORMAT , RAIL_RX_PACKET_ABORT_FILTERED , RAIL_RX_PACKET_ABORT_ABORTED , RAIL_RX_PACKET_ABORT_OVERFLOW , RAIL_RX_PACKET_ABORT_CRC_ERROR , RAIL_RX_PACKET_READY_CRC_ERROR , RAIL_RX_PACKET_READY_SUCCESS , RAIL_RX_PACKET_RECEIVING } |
|
The packet status code associated with a packet received or currently being received.
|
|
Functions |
|
| RAIL_Status_t | RAIL_ConfigRxOptions ( RAIL_Handle_t railHandle, RAIL_RxOptions_t mask, RAIL_RxOptions_t options) |
|
Configures receive options.
|
|
| RAIL_Status_t | RAIL_StartRx ( RAIL_Handle_t railHandle, uint16_t channel, const RAIL_SchedulerInfo_t *schedulerInfo) |
|
Starts the receiver on a specific channel.
|
|
| RAIL_Status_t | RAIL_ScheduleRx ( RAIL_Handle_t railHandle, uint16_t channel, const RAIL_ScheduleRxConfig_t *cfg, const RAIL_SchedulerInfo_t *schedulerInfo) |
|
Schedules a receive window for some future time.
|
|
| RAIL_RxPacketHandle_t | RAIL_GetRxPacketInfo ( RAIL_Handle_t railHandle, RAIL_RxPacketHandle_t packetHandle, RAIL_RxPacketInfo_t *pPacketInfo) |
|
Gets basic information about a pending or received packet.
|
|
| static void | RAIL_CopyRxPacket (uint8_t *pDest, const RAIL_RxPacketInfo_t *pPacketInfo) |
|
Convenience helper function to copy a full packet to a user-specified contiguous buffer.
|
|
| RAIL_Status_t | RAIL_GetRxPacketDetails ( RAIL_Handle_t railHandle, RAIL_RxPacketHandle_t packetHandle, RAIL_RxPacketDetails_t *pPacketDetails) |
|
Gets detailed information about a received packet.
|
|
| RAIL_Status_t | RAIL_GetRxPacketDetailsAlt ( RAIL_Handle_t railHandle, RAIL_RxPacketHandle_t packetHandle, RAIL_RxPacketDetails_t *pPacketDetails) |
|
Gets detailed information about a received packet.
|
|
| RAIL_Status_t | RAIL_GetRxTimePreambleStart ( RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) |
|
Adjust a RAIL RX timestamp to refer to the start of the preamble.
|
|
| RAIL_Status_t | RAIL_GetRxTimeSyncWordEnd ( RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) |
|
Adjust a RAIL RX timestamp to refer to the end of the sync word.
|
|
| RAIL_Status_t | RAIL_GetRxTimeFrameEnd ( RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime) |
|
Adjust a RAIL RX timestamp to refer to the end of frame.
|
|
| RAIL_RxPacketHandle_t | RAIL_HoldRxPacket ( RAIL_Handle_t railHandle) |
|
Place a temporary hold on this packet's data and information resources within RAIL.
|
|
| uint16_t | RAIL_PeekRxPacket ( RAIL_Handle_t railHandle, RAIL_RxPacketHandle_t packetHandle, uint8_t *pDst, uint16_t len, uint16_t offset) |
|
Copies 'len' bytes of packet data starting from 'offset' from the receive FIFO.
|
|
| RAIL_Status_t | RAIL_ReleaseRxPacket ( RAIL_Handle_t railHandle, RAIL_RxPacketHandle_t packetHandle) |
|
Releases RAIL's internal resources for the packet.
|
|
| int16_t | RAIL_GetRssi ( RAIL_Handle_t railHandle, bool wait) |
|
Returns the current raw RSSI.
|
|
| RAIL_Status_t | RAIL_StartAverageRssi ( RAIL_Handle_t railHandle, uint16_t channel, RAIL_Time_t averagingTimeUs, const RAIL_SchedulerInfo_t *schedulerInfo) |
|
Starts the RSSI averaging over a specified time in us.
|
|
| bool | RAIL_IsAverageRssiReady ( RAIL_Handle_t railHandle) |
|
Queries whether the RSSI averaging is done.
|
|
| int16_t | RAIL_GetAverageRssi ( RAIL_Handle_t railHandle) |
|
Gets the RSSI averaged over a specified time in us.
|
|
| RAIL_Status_t | RAIL_SetRssiOffset ( RAIL_Handle_t railHandle, int8_t rssiOffset) |
|
Sets the RSSI offset.
|
|
| int8_t | RAIL_GetRssiOffset ( RAIL_Handle_t railHandle) |
|
Gets the RSSI offset.
|
|
| RAIL_Status_t | RAIL_ConvertLqi ( RAIL_Handle_t railHandle, RAIL_ConvertLqiCallback_t cb) |
|
Setup a callback function capable of converting a RX packet's LQI value before being consumed by application code.
|
|
Detailed Description
APIs related to packet receive.
Macro Definition Documentation
| #define RAIL_RSSI_INVALID ((int16_t)( RAIL_RSSI_INVALID_DBM * 4)) |
The value returned by RAIL for an invalid RSSI: in quarter dBm.
Definition at line
1851
of file
rail_types.h
.
| #define RAIL_RSSI_INVALID_DBM (-128) |
The value returned by RAIL for an invalid RSSI, in dBm.
Definition at line
1849
of file
rail_types.h
.
| #define RAIL_RX_OPTION_ANTENNA0 (1UL << RAIL_RX_OPTION_ANTENNA0_SHIFT) |
An option to select the use of antenna 0 when doing RX.
If no antenna option is selected, the RX may take place on either antenna depending on the last RX or TX configuration. Defaults to false. This option is only valid on platforms that support antenna selection.
Definition at line
1820
of file
rail_types.h
.
| #define RAIL_RX_OPTION_ANTENNA1 (1UL << RAIL_RX_OPTION_ANTENNA1_SHIFT) |
An option to select the use of antenna 1 when doing RX.
If no antenna option is selected, the RX may take place on either antenna depending on the last RX or TX configuration. Defaults to false. This option is only valid on platforms that support antenna selection.
Definition at line
1828
of file
rail_types.h
.
| #define RAIL_RX_OPTION_ANTENNA_AUTO ( RAIL_RX_OPTION_ANTENNA0 | RAIL_RX_OPTION_ANTENNA1 ) |
Am option to automatically choose an antenna.
If both antenna 0 and antenna 1 options are set, the chip will switch between antennas and will automatically choose one.
Definition at line
1835
of file
rail_types.h
.
| #define RAIL_RX_OPTION_DISABLE_FRAME_DETECTION (1UL << RAIL_RX_OPTION_DISABLE_FRAME_DETECTION_SHIFT) |
An option to disable frame detection.
This can be useful for doing energy detection without risking packet reception. Enabling this will abort any frame currently being received in addition to preventing further frames from being received. Defaults to false.
Definition at line
1843
of file
rail_types.h
.
| #define RAIL_RX_OPTION_ENABLE_DUALSYNC (1UL << RAIL_RX_OPTION_ENABLE_DUALSYNC_SHIFT) |
An option to control which sync words will be accepted.
Setting it to 0 (default) will cause the receiver to listen for SYNC1 only. Setting it to 1 causes the receiver to listen for either SYNC1 or SYNC2. RX appended info will contain which sync word was detected. Note, this only affects which sync word(s) are received, but not what each of the sync words actually are. This feature may not be available on some combinations of chips, PHYs, and protocols. See the data sheet or support team for more details.
Definition at line
1796
of file
rail_types.h
.
| #define RAIL_RX_OPTION_IGNORE_CRC_ERRORS (1UL << RAIL_RX_OPTION_IGNORE_CRC_ERRORS_SHIFT) |
An option to configure whether CRC errors will be ignored.
If this is set, RX will still be successful, even if the CRC does not pass the check. Defaults to false.
Definition at line
1785
of file
rail_types.h
.
| #define RAIL_RX_OPTION_REMOVE_APPENDED_INFO (1UL << RAIL_RX_OPTION_REMOVE_APPENDED_INFO_SHIFT) |
An option to suppress capturing the appended information after received frames.
Defaults to false. When suppressed, certain RAIL_RxPacketDetails_t details will not be available for received packets whose RAIL_RxPacketStatus_t is among the RAIL_RX_PACKET_READY_ set.
Definition at line
1812
of file
rail_types.h
.
| #define RAIL_RX_OPTION_STORE_CRC (1UL << RAIL_RX_OPTION_STORE_CRC_SHIFT) |
An option to configure whether the CRC portion of the packet is included in the packet payload exposed to the app on packet reception.
Defaults to false.
Definition at line
1779
of file
rail_types.h
.
| #define RAIL_RX_OPTION_TRACK_ABORTED_FRAMES (1UL << RAIL_RX_OPTION_TRACK_ABORTED_FRAMES_SHIFT) |
An option to configure whether frames which are aborted during reception should continue to be tracked.
Setting this option allows viewing Packet Trace information for frames which get discarded. Defaults to false.
Definition at line
1803
of file
rail_types.h
.
| #define RAIL_RX_OPTIONS_ALL 0xFFFFFFFFUL |
A value representing all possible options.
Definition at line
1846
of file
rail_types.h
.
| #define RAIL_RX_OPTIONS_DEFAULT RAIL_RX_OPTIONS_NONE |
All options are disabled by default.
Definition at line
1772
of file
rail_types.h
.
| #define RAIL_RX_OPTIONS_NONE 0 |
A value representing no options enabled.
Definition at line
1770
of file
rail_types.h
.
| #define RAIL_RX_PACKET_HANDLE_INVALID (NULL) |
An invalid RX packet handle value.
Definition at line
1940
of file
rail_types.h
.
| #define RAIL_RX_PACKET_HANDLE_NEWEST (( RAIL_RxPacketHandle_t ) 2) |
A special RX packet handle to refer to the newest unreleased packet when in callback context.
For a callback involving a completed receive event, this refers to the packet just completed. For other callback events, this refers to the next packet to be completed, which might be in-progress or might not have even started yet.
Definition at line
1950
of file
rail_types.h
.
| #define RAIL_RX_PACKET_HANDLE_OLDEST (( RAIL_RxPacketHandle_t ) 1) |
A special RX packet handle to refer to the oldest unreleased packet.
Definition at line
1942
of file
rail_types.h
.
Typedef Documentation
| RAIL_ConvertLqiCallback_t |
A pointer to a funcation called before LQI is copied into the RAIL_RxPacketDetails_t structure.
- Parameters
-
[in] lqiThe LQI value obtained by hardware and being readied for application consumption. This LQI value is in integral units ranging from 0 to 255. [in] rssiThe RSSI value corresponding to the packet from which the hardware LQI value was obtained. This RSSI value is in integral dBm units.
- Returns
- uint8_t The converted LQI value that will be loaded into the RAIL_RxPacketDetails_t structure in preparation for application consumption. This value should likewise be in integral units ranging from 0 to 255.
Definition at line
2225
of file
rail_types.h
.
A handle used to reference a packet during reception processing.
There are several sentinel handle values that pertain to certain circumstances: RAIL_RX_PACKET_HANDLE_INVALID , RAIL_RX_PACKET_HANDLE_OLDEST and RAIL_RX_PACKET_HANDLE_NEWEST .
Definition at line
1937
of file
rail_types.h
.
Enumeration Type Documentation
| enum RAIL_RxOptions_t |
Receive options, in reality a bitmask.
| Enumerator | |
|---|---|
| RAIL_RX_OPTION_STORE_CRC_SHIFT |
Shift position of RAIL_RX_OPTION_STORE_CRC bit. |
| RAIL_RX_OPTION_IGNORE_CRC_ERRORS_SHIFT |
Shift position of RAIL_RX_OPTION_IGNORE_CRC_ERRORS bit. |
| RAIL_RX_OPTION_ENABLE_DUALSYNC_SHIFT |
Shift position of RAIL_RX_OPTION_ENABLE_DUALSYNC bit. |
| RAIL_RX_OPTION_TRACK_ABORTED_FRAMES_SHIFT |
Shift position of RAIL_RX_OPTION_TRACK_ABORTED_FRAMES bit. |
| RAIL_RX_OPTION_REMOVE_APPENDED_INFO_SHIFT |
Shift position of RAIL_RX_OPTION_REMOVE_APPENDED_INFO bit. |
| RAIL_RX_OPTION_ANTENNA0_SHIFT |
Shift position of RAIL_RX_OPTION_ANTENNA0 bit. |
| RAIL_RX_OPTION_ANTENNA1_SHIFT |
Shift position of RAIL_RX_OPTION_ANTENNA1 bit. |
| RAIL_RX_OPTION_DISABLE_FRAME_DETECTION_SHIFT |
Shift position of RAIL_RX_OPTION_DISABLE_FRAME_DETECTION bit. |
Definition at line
1750
of file
rail_types.h
.
The packet status code associated with a packet received or currently being received.
- Note
- RECEIVING implies some packet data may be available, but is untrustworthy (not CRC-verified) and might disappear if the packet is rolled back on error. No packet details are yet available.
- In RX RAIL_DataMethod_t::FIFO_MODE , ABORT statuses imply some packet data may be available, but it's incomplete and not trustworthy.
Definition at line
1918
of file
rail_types.h
.
Function Documentation
| RAIL_Status_t RAIL_ConfigRxOptions | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_RxOptions_t |
mask,
|
||
| RAIL_RxOptions_t |
options
|
||
| ) |
Configures receive options.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] maskA bitmask containing which options should be modified. [in] optionsA bitmask containing desired configuration settings. Bit positions for each option are found in the RAIL_RxOptions_t .
- Returns
- Status code indicating success of the function call.
Configures the radio receive flow based on the list of available options. Only the options indicated by the mask parameter will be affected. Pass RAIL_RX_OPTIONS_ALL to set all parameters. The previous settings may affect the current frame if a packet is received during this configuration.
| RAIL_Status_t RAIL_ConvertLqi | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_ConvertLqiCallback_t |
cb
|
||
| ) |
Setup a callback function capable of converting a RX packet's LQI value before being consumed by application code.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] cbA callback of type RAIL_ConvertLqiCallback_t that is called before the RX packet LQI value is loaded into the RAIL_RxPacketDetails_t structure for application consumption.
- Returns
- Status code indicating success of the function call.
|
inline static |
Convenience helper function to copy a full packet to a user-specified contiguous buffer.
- Parameters
-
[out] pDestAn application-provided pointer to a buffer of at least pPacketInfo->packetBytes in size to store the packet data contiguously. This buffer must never overlay RAIL's receive FIFO buffer. Exactly pPacketInfo->packetBytes of packet data will be written into it. [out] pPacketInfoRAIL_RxPacketInfo_t for the requested packet.
- Returns
- void.
- Note
- This helper is intended to be expedient. As a result, it does not check the validity of its arguments, so don't pass either as NULL, and don't pass a pDest pointer to a buffer that's too small for the packet's data.
- If only a portion of the packet is needed, use RAIL_PeekRxPacket() instead.
Definition at line
2233
of file
rail.h
.
| int16_t RAIL_GetAverageRssi | ( | RAIL_Handle_t |
railHandle
|
) |
Gets the RSSI averaged over a specified time in us.
- Parameters
-
[in] railHandleA RAIL instance handle.
- Returns
- Return RAIL_RSSI_INVALID if the receiver is disabled an RSSI value can't be obtained. Otherwise, return the RSSI in quarter dBm,dbm*4.
Gets the hardware RSSI average after issuing RAIL_StartAverageRssi. It should be used after RAIL_StartAverageRssi .
| int16_t RAIL_GetRssi | ( | RAIL_Handle_t |
railHandle,
|
| bool |
wait
|
||
| ) |
Returns the current raw RSSI.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] waitif false returns instant RSSI with no checks.
- Returns
- RAIL_RSSI_INVALID if the receiver is disabled and an RSSI value can't be obtained. Otherwise, return the RSSI in quarter dBm, dbm*4.
Gets the current RSSI value. This value represents the current energy of the channel. It can change rapidly and will be low if no RF energy is in the current channel. The function from the value reported to dBm is an offset dependent on the PHY and the PCB layout. Users should characterize the RSSI received on their hardware and apply an offset in the application to account for board and PHY parameters. 'Wait' argument doesn't guarantee a valid RSSI reading.'Wait' being true gives assurance that that the RSSI is current and not a stale value from a previous radio state. If GetRssi is called during RX-to-RX, RX-to-IDLE, or RX-to-TX transition, the RSSI is considered stale and RAIL_RSSI_INVALID is returned if wait=true. 'Wait' being false will return either the current RSSI or a stale RSSI measurement (if called during RX-to-RX, RX-to-IDLE, or RX-to-TX transition). RAIL_RSSI_INVALID is returned if radio hasn't been in RX longer than 'idleToRx' time (see RAIL_StateTiming_t ), regardless of wait argument.
In multiprotocol, this function returns RAIL_RSSI_INVALID immediately if railHandle is not the current active RAIL_Handle_t . Additionally, 'wait' should never be set 'true' in multiprotocol as the wait time is not consistent, so scheduling a scheduler slot cannot be done accurately.
| int8_t RAIL_GetRssiOffset | ( | RAIL_Handle_t |
railHandle
|
) |
Gets the RSSI offset.
- Parameters
-
[in] railHandlea RAIL instance handle.
- Returns
- rssiOffset in dBm corresponding to the current handle.
| RAIL_Status_t RAIL_GetRxPacketDetails | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_RxPacketHandle_t |
packetHandle,
|
||
| RAIL_RxPacketDetails_t * |
pPacketDetails
|
||
| ) |
Gets detailed information about a received packet.
This function can be used in any RX mode; it does not free up any internal resources.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] packetHandleA packet handle for the unreleased packet as returned from a previous call to RAIL_GetRxPacketInfo() or RAIL_HoldRxPacket() , or sentinel values RAIL_RX_PACKET_HANDLE_OLDEST or RAIL_RX_PACKET_HANDLE_NEWEST . [in,out] pPacketDetailsAn application-provided non-NULL pointer to store RAIL_RxPacketDetails_t for the requested packet. For RAIL_RxPacketStatus_t RAIL_RX_PACKET_READY_ packets, the timeReceived fields totalPacketBytes and timePosition must be initialized prior to each call: - totalPacketBytes with the total number of bytes of the received packet for RAIL to use when calculating the specified timestamp. This should account for all bytes received over the air after the Preamble and Sync word(s), including CRC bytes.
- timePosition with a RAIL_PacketTimePosition_t value specifying the packet position to put in the timeReceived field on return. This field will also be updated with the actual position corresponding to the timeReceived value filled in.
- Returns
- RAIL_STATUS_NO_ERROR if pPacketDetails was filled in, or an appropriate error code otherwise.
- Note
- Certain details are always available, while others are only available if the RAIL_RxOptions_t RAIL_RX_OPTION_REMOVE_APPENDED_INFO option is not in effect and the received packet's RAIL_RxPacketStatus_t is among the RAIL_RX_PACKET_READY_ set. See RAIL_RxPacketDetails_t for clarification.
- Consider using RAIL_GetRxPacketDetailsAlt for smaller code size.
| RAIL_Status_t RAIL_GetRxPacketDetailsAlt | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_RxPacketHandle_t |
packetHandle,
|
||
| RAIL_RxPacketDetails_t * |
pPacketDetails
|
||
| ) |
Gets detailed information about a received packet.
This function can be used in any RX mode; it does not free up any internal resources.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] packetHandleA packet handle for the unreleased packet as returned from a previous call to RAIL_GetRxPacketInfo() or RAIL_HoldRxPacket() , or sentinel values RAIL_RX_PACKET_HANDLE_OLDEST or RAIL_RX_PACKET_HANDLE_NEWEST . [out] pPacketDetailsAn application-provided non-NULL pointer to store RAIL_RxPacketDetails_t for the requested packet. For RAIL_RxPacketStatus_t RAIL_RX_PACKET_READY_ packets, the timeReceived field packetTime will be populated with a timestamp corresponding to an arbitrary location in the packet. Call RAIL_GetRxTimePreambleStart , RAIL_GetRxTimeSyncWordEnd , or RAIL_GetRxTimeFrameEnd to adjust that timestamp for different locations in the packet.
- Returns
- RAIL_STATUS_NO_ERROR if pPacketDetails was filled in, or an appropriate error code otherwise.
This alternative API allows for smaller code size by deadstripping the timestamp adjustment algorithms which are not in use.
- Note
- Certain details are always available, while others are only available if the RAIL_RxOptions_t RAIL_RX_OPTION_REMOVE_APPENDED_INFO option is not in effect and the received packet's RAIL_RxPacketStatus_t is among the RAIL_RX_PACKET_READY_ set. See RAIL_RxPacketDetails_t for clarification.
| RAIL_RxPacketHandle_t RAIL_GetRxPacketInfo | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_RxPacketHandle_t |
packetHandle,
|
||
| RAIL_RxPacketInfo_t * |
pPacketInfo
|
||
| ) |
Gets basic information about a pending or received packet.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] packetHandleA packet handle for the unreleased packet as returned from a previous call, or sentinel values RAIL_RX_PACKET_HANDLE_OLDEST or RAIL_RX_PACKET_HANDLE_NEWEST . [out] pPacketInfoAn application-provided pointer to store RAIL_RxPacketInfo_t for the requested packet. Must be non-NULL.
- Returns
- The packet handle for the requested packet: if packetHandle was one of the sentinel values, returns the actual packet handle for that packet, otherwise returns packetHandle. It may return RAIL_RX_PACKET_HANDLE_INVALID to indicate an error.
This function can be used in any RX mode; it does not free up any internal resources. If used in RX RAIL_DataMethod_t::FIFO_MODE , the value in RAIL_RxPacketInfo_t::packetBytes will only return the data remaining in the FIFO. Any data read via earlier earlier calls to RAIL_ReadRxFifo() is not included.
- Note
- When getting information about an arriving packet that is not yet complete (i.e., pPacketInfo->packetStatus == RAIL_RX_PACKET_RECEIVING ), keep in mind its data is highly suspect because it has not yet passed any CRC integrity checking. Also note that the packet could be aborted, canceled, or fail momentarily, invalidating its data in Packet mode. Furthermore, there is a small chance towards the end of packet reception that the filled-in RAIL_RxPacketInfo_t could include not only packet data received so far, but also some raw radio-appended info detail bytes that RAIL's packet-completion processing will subsequently deal with. It's up to the application to know its packet format well enough to avoid confusing such info as packet data.
| RAIL_Status_t RAIL_GetRxTimeFrameEnd | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
totalPacketBytes,
|
||
| RAIL_Time_t * |
pPacketTime
|
||
| ) |
Adjust a RAIL RX timestamp to refer to the end of frame.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] totalPacketBytesThe total number of bytes of the received packet for RAIL to use when calculating the specified timestamp. This should account for all bytes received over the air after the Preamble and Sync word(s), including CRC bytes. [in,out] pPacketTimeThe time that was returned in the RAIL_PacketTimeStamp_t::packetTime field of RAIL_RxPacketDetails_t::timeReceived from a previous call to RAIL_GetRxPacketDetailsAlt for this same packet. After this function, the time at that location will be updated with the time that this packet finished on air. Must be non-NULL.
- Returns
- RAIL_STATUS_NO_ERROR if pPacketTime was successfully calculated, or an appropriate error code otherwise.
This API must be called while the given railHandle is active, or it will return an error code of RAIL_STATUS_INVALID_STATE .
| RAIL_Status_t RAIL_GetRxTimePreambleStart | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
totalPacketBytes,
|
||
| RAIL_Time_t * |
pPacketTime
|
||
| ) |
Adjust a RAIL RX timestamp to refer to the start of the preamble.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] totalPacketBytesThe total number of bytes of the received packet for RAIL to use when calculating the specified timestamp. This should account for all bytes received over the air after the Preamble and Sync word(s), including CRC bytes. [in,out] pPacketTimeThe time that was returned in the RAIL_PacketTimeStamp_t::packetTime field of RAIL_RxPacketDetails_t::timeReceived from a previous call to RAIL_GetRxPacketDetailsAlt for this same packet. After this function, the time at that location will be updated with the time that the preamble for this packet started on air. Must be non-NULL.
- Returns
- RAIL_STATUS_NO_ERROR if pPacketTime was successfully calculated, or an appropriate error code otherwise.
This API must be called while the given railHandle is active, or it will return an error code of RAIL_STATUS_INVALID_STATE .
| RAIL_Status_t RAIL_GetRxTimeSyncWordEnd | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
totalPacketBytes,
|
||
| RAIL_Time_t * |
pPacketTime
|
||
| ) |
Adjust a RAIL RX timestamp to refer to the end of the sync word.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] totalPacketBytesThe total number of bytes of the received packet for RAIL to use when calculating the specified timestamp. This should account for all bytes received over the air after the Preamble and Sync word(s), including CRC bytes. [in,out] pPacketTimeThe time that was returned in the RAIL_PacketTimeStamp_t::packetTime field of RAIL_RxPacketDetails_t::timeReceived from a previous call to RAIL_GetRxPacketDetailsAlt for this same packet. After this function, the time at that location will be updated with the time that the sync word for this packet finished on air. Must be non-NULL.
- Returns
- RAIL_STATUS_NO_ERROR if pPacketTime was successfully calculated, or an appropriate error code otherwise.
This API must be called while the given railHandle is active, or it will return an error code of RAIL_STATUS_INVALID_STATE .
| RAIL_RxPacketHandle_t RAIL_HoldRxPacket | ( | RAIL_Handle_t |
railHandle
|
) |
Place a temporary hold on this packet's data and information resources within RAIL.
This function can only be called from within RAIL callback context. It can be used in any RX mode.
Normally, when RAIL issues its callback indicating a packet is ready or aborted, it expects the application's callback to retrieve and copy (or discard) the packet's information and data, and will free up its internal packet data after the callback returns. This function tells RAIL to hold onto those resources after the callback returns in case the application wants to defer processing the packet to a later time, e.g., outside of callback context.
- Parameters
-
[in] railHandleA RAIL instance handle.
- Returns
- The packet handle for the packet associated with the callback, RAIL_RX_PACKET_HANDLE_INVALID if no such packet yet exists or railHandle is not active.
| bool RAIL_IsAverageRssiReady | ( | RAIL_Handle_t |
railHandle
|
) |
Queries whether the RSSI averaging is done.
- Parameters
-
[in] railHandleA RAIL instance handle.
- Returns
- Returns true if done and false otherwise.
This function can be used to poll for completion of the RSSI averaging to avoid relying on an interrupt-based callback.
| uint16_t RAIL_PeekRxPacket | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_RxPacketHandle_t |
packetHandle,
|
||
| uint8_t * |
pDst,
|
||
| uint16_t |
len,
|
||
| uint16_t |
offset
|
||
| ) |
Copies 'len' bytes of packet data starting from 'offset' from the receive FIFO.
Those bytes remain valid for re-peeking.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] packetHandleA packet handle as returned from a previous RAIL_GetRxPacketInfo() or RAIL_HoldRxPacket() call, or sentinel values RAIL_RX_PACKET_HANDLE_OLDEST or RAIL_RX_PACKET_HANDLE_NEWEST . [out] pDstA pointer to the location where the received bytes will be copied. If NULL, no copying occurs. [in] lenA number of packet data bytes to copy. [in] offsetA byte offset within remaining packet data from which to copy.
- Returns
- Number of packet bytes copied.
- Note
- Peek does not permit peeking beyond the requested packet's available packet data (though there is a small chance it might for a RAIL_RX_PACKET_HANDLE_NEWEST packet at the very end of still being received). Nor can one peek into already-consumed data read by RAIL_ReadRxFifo() . len and offset are relative to the remaining data available in the packet, if any was already consumed by RAIL_ReadRxFifo() .
| RAIL_Status_t RAIL_ReleaseRxPacket | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_RxPacketHandle_t |
packetHandle
|
||
| ) |
Releases RAIL's internal resources for the packet.
This function must be called for any packet previously held via RAIL_HoldRxPacket() . It may optionally be called within a callback context to release RAIL resources sooner than at callback completion time when not holding the packet. This function can be used in any RX mode.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] packetHandleA packet handle as returned from a previous RAIL_HoldRxPacket() call, or sentinel values RAIL_RX_PACKET_HANDLE_OLDEST or RAIL_RX_PACKET_HANDLE_NEWEST . The latter might be used within RAIL callback context to explicitly release the packet associated with the callback early, before it's released automatically by RAIL on callback return (unless explicitly held).
- Returns
- RAIL_STATUS_NO_ERROR if the held packet was released or an appropriate error code otherwise.
| RAIL_Status_t RAIL_ScheduleRx | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
channel,
|
||
| const RAIL_ScheduleRxConfig_t * |
cfg,
|
||
| const RAIL_SchedulerInfo_t * |
schedulerInfo
|
||
| ) |
Schedules a receive window for some future time.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] channelA channel to listen on. [in] cfgThe configuration structure to define the receive window. [in] schedulerInfoInformation to allow the radio scheduler to place this receive appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.
- Returns
- Status code indicating success of the function call.
This API immediately changes the channel and schedules receive to start at the specified time and end at the given end time. If you do not specify an end time, you may call this API later with an end time as long as you set the start time to disabled. You can also terminate the receive operation immediately using the RAIL_Idle() function. Note that relative end times are always relative to the start unless no start time is specified. If changing channels, aborts any ongoing packet transmission or reception.
In multiprotocol, ensure that you properly yield the radio after this call. See Yielding the radio for more details.
| RAIL_Status_t RAIL_SetRssiOffset | ( | RAIL_Handle_t |
railHandle,
|
| int8_t |
rssiOffset
|
||
| ) |
Sets the RSSI offset.
- Parameters
-
[in] railHandlea RAIL instance handle. [in] rssiOffsetdesired offset to be added to the RSSI measurements.
- Returns
- Status code indicating success of the function call.
Adds an offset to the RSSI in dBm. This offset affects all functionality that depends on RSSI values, such as CCA fuctions. The offset should not be modified dynamically during the RX of a packet.
| RAIL_Status_t RAIL_StartAverageRssi | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
channel,
|
||
| RAIL_Time_t |
averagingTimeUs,
|
||
| const RAIL_SchedulerInfo_t * |
schedulerInfo
|
||
| ) |
Starts the RSSI averaging over a specified time in us.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] channelThe physical channel to set. [in] averagingTimeUsAveraging time in microseconds. [in] schedulerInfoInformation to allow the radio scheduler to place this operation appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.
- Returns
- Status code indicating success of the function call.
Starts a non-blocking hardware-based RSSI averaging mechanism. Only a single instance of RSSI averaging can be run at any time and the radio must be idle to start.
In multiprotocol, this is a scheduled event. It will start when railHandle becomes active. railHandle needs to stay active until the averaging completes. If the averaging is interrupted, calls to RAIL_GetAverageRssi will return RAIL_RSSI_INVALID .
Also in multiprotocol, the user is required to call RAIL_YieldRadio after this event completes (i.e., when RAIL_EVENT_RSSI_AVERAGE_DONE occurs).
| RAIL_Status_t RAIL_StartRx | ( | RAIL_Handle_t |
railHandle,
|
| uint16_t |
channel,
|
||
| const RAIL_SchedulerInfo_t * |
schedulerInfo
|
||
| ) |
Starts the receiver on a specific channel.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] channelThe channel to listen on. [in] schedulerInfoInformation to allow the radio scheduler to place this receive appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.
- Returns
- Status code indicating success of the function call.
This is a non-blocking function. Whenever a packet is received, RAIL_Config_t::eventsCallback will fire with RAIL_EVENT_RX_PACKET_RECEIVED set. If you call this while not idle but with a different channel, any ongoing receive or transmit operation will be aborted.