Rail Native Modules
      Here is a list of all modules:
     
     | Chip-specific | |
| EFR32xG1x_Interrupts | EFR32xG1x-specific interrupt sources | 
| RAIL API | This is the primary API layer for the Radio Abstraction Interface Layer (RAIL) | 
| Antenna Control | Basic APIs to control the Antenna functionality | 
| EFR32 | EFR32 Antenna Control FunctionalityThese enumerations and structures are used with RAIL Antenna Control API | 
| Assertions | Callbacks called by assertions | 
| Auto ACK | APIs for configuring auto ACK functionality | 
| Calibration | APIs for calibrating the radio | 
| EFR32 | EFR32-specific CalibrationsThe EFR32 supports the Image Rejection (IR) calibration and a temperature-dependent calibration | 
| Data Management | Data management functions | 
| Diagnostic | APIs for diagnostic and test chip modes | 
| EFR32 | Types specific to the EFR32 for the diagnostic routines | 
| Events | APIs related to events | 
| General | Basic APIs to set up and interact with the RAIL library | 
| Multiprotocol | Multiprotocol scheduler APIs to support multiple time-sliced PHYs | 
| EFR32 | EFR32-specific multiprotocol support defines | 
| Packet Trace (PTI) | Basic APIs to set up and interact with PTI settings | 
| EFR32 | EFR32 PTI functionalityThese enumerations and structures are used with RAIL PTI API | 
| Protocol-specific | Protocol-specific RAIL APIs | 
| BLE | Accelerator routines for Bluetooth Low Energy (BLE) | 
| IEEE 802.15.4 | IEEE 802.15.4 configuration routines | 
| Z-Wave | Z-Wave configuration routines | 
| RF Sense | |
| RX Channel Hopping | Hardware accelerated hopping between channels while waiting for a packet in receive | 
| Radio Configuration | Routines for setting up and querying radio configuration information | 
| EFR32 | Types specific to the EFR32 for radio configuration | 
| Receive | APIs related to packet receive | 
| Address Filtering | Configuration APIs for receive packet address filtering | 
| State Transitions | |
| System Timing | Functionality related to the RAIL timer and general system time | 
| Transmit | APIs related to transmitting data packets | 
| Power Amplifier (PA) | APIs for interacting with one of the on chip PAs | 
| EFR32 | Types specific to the EFR32 for dealing with the on-chip PAs |