Enables/disables the auto ACK algorithm, based on "enable".
#include <
rail_types.h
>
Data Fields |
|
| bool | enable |
|
Indicates whether auto-ACKing should be enabled or disabled.
|
|
| uint16_t | ackTimeout |
|
Defines the RX ACK timeout duration in us.
|
|
| RAIL_StateTransitions_t | rxTransitions |
|
State transitions to do after receiving a packet.
|
|
| RAIL_StateTransitions_t | txTransitions |
|
State transitions to do after transmitting a packet.
|
|
Enables/disables the auto ACK algorithm, based on "enable".
The structure provides a default state (the "success" of tx/rxTransitions when ACKing is enabled) for the radio to return to after an ACK operation occurs (transmitting or attempting to receive an ACK), or normal state transitions to return to in the case ACKing is disabled. Regardless whether the ACK operation was successful, the radio returns to the specified success state.
ackTimeout specifies how long to stay in receive and wait for an ACK before issuing a RAIL_EVENT_RX_ACK_TIMEOUT event and return to the default state.
Definition at line
2151
of file
rail_types.h
.
Field Documentation
| uint16_t RAIL_AutoAckConfig_t::ackTimeout |
Defines the RX ACK timeout duration in us.
Limited to a maximum 65535 us. Only applied when auto ACKing is enabled. Triggers a RAIL_EVENT_RX_ACK_TIMEOUT event if this threshold is exceeded.
Definition at line
2161
of file
rail_types.h
.
| RAIL_StateTransitions_t RAIL_AutoAckConfig_t::rxTransitions |
State transitions to do after receiving a packet.
When auto ACKing is enabled, the "error" transition is always ignored and the radio will return to the "success" state after any ACKing sequence. See RAIL_ConfigAutoAck for more details on this.
Definition at line
2168
of file
rail_types.h
.
| RAIL_StateTransitions_t RAIL_AutoAckConfig_t::txTransitions |
State transitions to do after transmitting a packet.
When auto ACKing is enabled, the "error" transition is always ignored and the radio will return to the "success" state after any ACKing sequence. See RAIL_ConfigAutoAck for more details on this.
Definition at line
2175
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h