RAIL_CalValues_t Struct Reference
A calibration value structure.
      
       #include <
       
     
        rail_chip_specific.h
       
       >
      
         Data Fields | 
       |
| uint32_t | imageRejection | 
| 
         An Image Rejection (IR) calibration value.
          | 
       |
A calibration value structure.
This structure contains the set of persistent calibration values for EFR32. You can set these beforehand and apply them at startup to save the time required to compute them. Any of these values may be set to RAIL_CAL_INVALID_VALUE to force the code to compute that calibration value.
       Definition at line
       
        351
       
       of file
       
        rail_chip_specific.h
       
       .
      
The documentation for this struct was generated from the following file:
- 
       chip/efr32/efr32xg1x/
       
rail_chip_specific.h