Contains RAIL Library Version Information.
#include <
rail_types.h
>
Data Fields |
|
| uint32_t | hash |
|
Git hash.
|
|
| uint8_t | major |
|
Major number.
|
|
| uint8_t | minor |
|
Minor number.
|
|
| uint8_t | rev |
|
Revision number.
|
|
| uint8_t | build |
|
Build number.
|
|
| uint8_t | flags |
|
Build flags.
|
|
| bool | multiprotocol |
|
Boolean to indicate whether this is a multiprotocol library or not.
|
|
Contains RAIL Library Version Information.
It is filled in by RAIL_GetVersion() .
Definition at line
677
of file
rail_types.h
.
Field Documentation
| bool RAIL_Version_t::multiprotocol |
Boolean to indicate whether this is a multiprotocol library or not.
Definition at line
685
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h