RAIL_IEEE802154_AddrConfig_t Struct Reference
A configuration structure for IEEE 802.15.4 Address Filtering.
#include <
rail_ieee802154.h
>
Data Fields |
|
| uint16_t | panId [3] |
|
PAN IDs for destination filtering.
|
|
| uint16_t | shortAddr [3] |
|
A short network addresses for destination filtering.
|
|
| uint8_t | longAddr [3][8] |
|
A 64-bit address for destination filtering.
|
|
A configuration structure for IEEE 802.15.4 Address Filtering.
The broadcast addresses are handled separately and do not need to be specified here. Any address to be ignored should be set with all bits high.
This structure allows configuration of multi-PAN functionality by specifying multiple PAN IDs and short addresses. A packet will be received if it matches an address and it's corresponding PAN ID. Long address 0 and short address 0 match against PAN ID 0, etc. The broadcast PAN ID and address will work with any address or PAN ID, respectively.
Definition at line
208
of file
rail_ieee802154.h
.
Field Documentation
| uint8_t RAIL_IEEE802154_AddrConfig_t::longAddr[3][8] |
A 64-bit address for destination filtering.
All must be specified. This field is parsed in over-the-air (OTA) byte order. To disable a long address, set it to the reserved value of 0x00 00 00 00 00 00 00 00.
Definition at line
224
of file
rail_ieee802154.h
.
| uint16_t RAIL_IEEE802154_AddrConfig_t::panId[3] |
PAN IDs for destination filtering.
All must be specified. To disable a PAN ID, set it to the broadcast value, 0xFFFF.
Definition at line
213
of file
rail_ieee802154.h
.
| uint16_t RAIL_IEEE802154_AddrConfig_t::shortAddr[3] |
A short network addresses for destination filtering.
All must be specified. To disable a short address, set it to the broadcast value, 0xFFFF.
Definition at line
218
of file
rail_ieee802154.h
.
The documentation for this struct was generated from the following file:
-
protocol/ieee802154/
rail_ieee802154.h