RAIL_IEEE802154_Config_t Struct Reference
A configuration structure for IEEE 802.15.4 in RAIL.
#include <
rail_ieee802154.h
>
Data Fields |
|
| const RAIL_IEEE802154_AddrConfig_t * | addresses |
|
Configure the RAIL Address Filter to allow the given destination addresses.
|
|
| RAIL_AutoAckConfig_t | ackConfig |
|
Defines the acking configuration for the IEEE 802.15.4 implementation.
|
|
| RAIL_StateTiming_t | timings |
|
Defines state timings for the IEEE 802.15.4 implementation.
|
|
| uint8_t | framesMask |
|
Sets which 802.15.4 frame types will be received, of Beacon, Data, ACK, and Command.
|
|
| bool | promiscuousMode |
|
Enables promiscuous mode during configuration.
|
|
| bool | isPanCoordinator |
|
Sets whether the device is a PAN Coordinator during configuration.
|
|
A configuration structure for IEEE 802.15.4 in RAIL.
Definition at line
231
of file
rail_ieee802154.h
.
Field Documentation
| const RAIL_IEEE802154_AddrConfig_t * RAIL_IEEE802154_Config_t::addresses |
Configure the RAIL Address Filter to allow the given destination addresses.
If this pointer is NULL, defer destination address configuration. If a member of addresses is NULL, defer configuration of just that member. This can be overridden via RAIL_IEEE802154_SetAddresses() , or the individual members can be changed via RAIL_IEEE802154_SetPanId() , RAIL_IEEE802154_SetShortAddress() , and RAIL_IEEE802154_SetLongAddress() .
Definition at line
240
of file
rail_ieee802154.h
.
| uint8_t RAIL_IEEE802154_Config_t::framesMask |
Sets which 802.15.4 frame types will be received, of Beacon, Data, ACK, and Command.
This setting can be overridden via RAIL_IEEE802154_AcceptFrames() .
Definition at line
253
of file
rail_ieee802154.h
.
| bool RAIL_IEEE802154_Config_t::isPanCoordinator |
Sets whether the device is a PAN Coordinator during configuration.
This can be overridden via RAIL_IEEE802154_SetPanCoordinator() afterwards.
Definition at line
263
of file
rail_ieee802154.h
.
| bool RAIL_IEEE802154_Config_t::promiscuousMode |
Enables promiscuous mode during configuration.
This can be overridden via RAIL_IEEE802154_SetPromiscuousMode() afterwards.
Definition at line
258
of file
rail_ieee802154.h
.
The documentation for this struct was generated from the following file:
-
protocol/ieee802154/
rail_ieee802154.h