RAIL_IEEE802154_Address_t Struct Reference
Representation of 802.15.4 address This structure is only used for received source address information needed to perform frame pending lookup.
#include <
rail_ieee802154.h
>
Data Fields |
|
| union { | |
| uint16_t shortAddress | |
|
Present for 2 byte addresses.
|
|
| uint8_t longAddress [8] | |
|
Present for 8 byte addresses.
|
|
| }; | |
|
Convenient storage for different address types.
|
|
| RAIL_IEEE802154_AddressLength_t | length |
|
Enumeration of the received address length.
|
|
Representation of 802.15.4 address This structure is only used for received source address information needed to perform frame pending lookup.
Definition at line
181
of file
rail_ieee802154.h
.
Field Documentation
| union { ... } |
Convenient storage for different address types.
| uint8_t RAIL_IEEE802154_Address_t::longAddress[8] |
Present for 8 byte addresses.
Definition at line
185
of file
rail_ieee802154.h
.
| uint16_t RAIL_IEEE802154_Address_t::shortAddress |
Present for 2 byte addresses.
Definition at line
184
of file
rail_ieee802154.h
.
The documentation for this struct was generated from the following file:
-
protocol/ieee802154/
rail_ieee802154.h