RAIL_BLE_AoxConfig_t Struct Reference
Contains arguments for RAIL_BLE_ConfigAox function.
#include <
rail_ble.h
>
Data Fields |
|
| RAIL_BLE_AoxOptions_t | aoxOptions |
|
See RAIL_BLE_AOX_OPTIONS_* for bitfield defines for different AoX features.
|
|
| uint16_t | cteBuffSize |
|
Size of the raw AoX CTE (continuous tone extension) data capture buffer in bytes.
|
|
| uint32_t * | cteBuffAddr |
|
Address to where the received CTE is written.
|
|
| uint32_t * | antArrayAddr |
|
Address to first element of antenna pattern array.
|
|
| uint8_t | antArraySize |
|
Size of the antenna pattern array.
|
|
Contains arguments for RAIL_BLE_ConfigAox function.
Definition at line
460
of file
rail_ble.h
.
The documentation for this struct was generated from the following file:
-
protocol/ble/
rail_ble.h