A configuration structure for the LBT transmit algorithm.
      
       #include <
       
     
        rail_types.h
       
       >
      
| Data Fields | |
| uint8_t | lbtMinBoRand | 
| The minimum backoff random multiplier. | |
| uint8_t | lbtMaxBoRand | 
| The maximum backoff random multiplier. | |
| uint8_t | lbtTries | 
| The number of LBT iterations that can fail before reporting
         
          RAIL_EVENT_TX_CHANNEL_BUSY
         
         . | |
| int8_t | lbtThreshold | 
| The LBT RSSI threshold, in dBm, above which the channel is considered 'busy'. | |
| uint16_t | lbtBackoff | 
| The backoff unit period, in RAIL's microsecond time base. | |
| uint16_t | lbtDuration | 
| The minimum desired LBT check duration in microseconds. | |
| RAIL_Time_t | lbtTimeout | 
| An overall timeout, in RAIL's microsecond time base, for the operation. | |
A configuration structure for the LBT transmit algorithm.
       One of RAIL's schemes for polite spectrum access is an implementation of a Listen-Before-Talk (LBT) algorithm, loosely based on ETSI 300 220-1.
       
       Currently, however, it is constrained by the EFR32's CSMA-oriented hardware so is turned into an equivalent
       
        RAIL_CsmaConfig_t
       
       configuration and passed to the CSMA engine:
      
       Definition at line
       
        2235
       
       of file
       
        rail_types.h
       
       .
      
Field Documentation
◆ lbtBackoff
| uint16_t RAIL_LbtConfig_t::lbtBackoff | 
The backoff unit period, in RAIL's microsecond time base.
It is multiplied by the random backoff multiplier controlled by lbtMinBoRand and lbtMaxBoRand to determine the overall backoff period. For random backoffs, any value above 511 microseconds will be truncated. For fixed backoffs, it can go up to 65535 microseconds.
        Definition at line
        
         2267
        
        of file
        
         rail_types.h
        
        .
       
◆ lbtDuration
| uint16_t RAIL_LbtConfig_t::lbtDuration | 
The minimum desired LBT check duration in microseconds.
- Note
- Depending on the radio configuration, due to hardware constraints, the actual duration may be longer. Also, if the requested duration is too large for the radio to accommodate, RAIL_StartCcaLbtTx() will fail returning RAIL_STATUS_INVALID_PARAMETER .
        Definition at line
        
         2276
        
        of file
        
         rail_types.h
        
        .
       
◆ lbtMaxBoRand
| uint8_t RAIL_LbtConfig_t::lbtMaxBoRand | 
The maximum backoff random multiplier.
        It must be greater than or equal to
        
         lbtMinBoRand
        
        .
        
        If both backoff multipliers are identical, a non-random fixed backoff of
        
         lbtBackoff
        
        times the multiplier (minimum 1) duration results.
       
        Definition at line
        
         2246
        
        of file
        
         rail_types.h
        
        .
       
◆ lbtTimeout
| RAIL_Time_t RAIL_LbtConfig_t::lbtTimeout | 
An overall timeout, in RAIL's microsecond time base, for the operation.
If the transmission doesn't start before this timeout expires, the transmission will fail with RAIL_EVENT_TX_CHANNEL_BUSY . This is important for limiting LBT due to LBT's unbounded requirement that if the channel is busy, the next try must wait for the channel to clear. A value 0 means no timeout is imposed.
        Definition at line
        
         2285
        
        of file
        
         rail_types.h
        
        .
       
◆ lbtTries
| uint8_t RAIL_LbtConfig_t::lbtTries | 
The number of LBT iterations that can fail before reporting RAIL_EVENT_TX_CHANNEL_BUSY .
Typically ranges from 1 to RAIL_MAX_LBT_TRIES ; higher values are disallowed. A value 0 always transmits immediately without performing LBT, similar to calling RAIL_StartTx() .
        Definition at line
        
         2254
        
        of file
        
         rail_types.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       common/
       rail_types.h