Migration Guide#
RAIL SDK 3.0.0#
Highlights:
Uses RAIL LIB 3.0.0
PA configuration APIs updated to use RAIL handle parameter
Protocol enum
BTCrenamed toBPSK
Breaking Changes in Version 3.0.0#
PA Configuration API Changes#
The mode switch PA configuration functions now require or have modified parameters:
// Version 2.19.0 (OLD)
void init_rail_pa_settings(void);
void update_rail_pa_settings(sl_rail_handle_t rail_handle, uint16_t channel);
// Version 3.0.0 (NEW)
void init_rail_pa_settings(sl_rail_handle_t rail_handle);
void update_rail_pa_settings(sl_rail_handle_t rail_handle);
Migration Steps:
Update calls to
init_rail_pa_settings()to pass the RAIL handleRemove the
channelparameter from calls toupdate_rail_pa_settings()
Protocol Enum Rename#
The protocol enum value BTC has been renamed to BPSK:
// Version 2.19.0 (OLD)
RAIL_SDK_Protocol_t protocol = BTC;
// Version 3.0.0 (NEW)
RAIL_SDK_Protocol_t protocol = BPSK;
Removed Function#
The function sl_rail_sdk_wmbus_phy_software() has been removed as software-based PHY processing is no longer required.
RAIL SDK 2.19.0#
Highlights:
Uses RAIL LIB 2.19.0
Examples now use
sl_maininstead ofsl_system
Detailed API Change#
API Naming:
Switched from
CamelCasetosnake_casefor most APIs and typedefs.All public APIs now use
sl_rail_handle_t,sl_rail_status_t, etc., instead of the oldRAIL_Handle_t,RAIL_Status_t, etc.
Breaking Changes in Version 2.19.0#
Example of API Change:
// Version 2.18.2 (OLD)
uint16_t unpack_packet(
uint8_t *rx_destination,
const RAIL_RxPacketInfo_t *packet_information,
uint8_t **start_of_payload,
phy_modulation_e modulation
);
// Version 2.19.0 (NEW)
uint16_t unpack_packet(
sl_rail_handle_t rail_handle, // New first parameter
uint8_t *rx_destination,
const sl_rail_rx_packet_info_t *packet_information, // Renamed type
uint8_t **start_of_payload,
phy_modulation_e modulation
);
Manual Update for Range Test Projects:
If your project directory name contains
range_test, you should manually:Remove any lines declaring
static RAIL_Handle_t rail_handle;from all.cand.hfiles.Remove
rail_handlefrom function parameter lists, regardless of its position (beginning, middle, or end).Remove any assignments to
rail_handleand any standalone usages ofrail_handlein your code, to ensure no obsolete references remain.
RAIL SDK 2.18.0#
Directory and SDK Structure Changes#
SiSDK-2024.12 Release:
RAIL and Connect SDKs are now separated.
The former
FLEX SDKis split into:RAIL SDKConnect SDK
Directory changes: files moved from
app/flextoapp/railandapp/connect.
Component and API Renames#
Component file names and APIs updated:
Any occurrence of
flexin APIs or definitions updated to match the new structure.
Table of Changes#
Old File | New File | Changes | Details |
|---|---|---|---|
simple_rail_assistance.h | sl_rail_sdk_simple_assistance.h | - | |
simple_rail_heartbeat.h | Deleted | - | |
simple_rail_rx.h | Deleted | - | |
simple_rail_rx_cli.h | Deleted | - | |
simple_rail_tx.h | Deleted | - | |
sl_flex_mode_switch.h | sl_rail_sdk_mode_switch.h | Rename API: prepare_package -> prepare_packet | |
sl_flex_ieee802154_support.h | sl_rail_sdk_ieee802154_support.h | Change part of names: FLEX -> RAIL_SDK , flex -> rail_sdk | |
sl_flex_rail_package_assistant.h | Rename API: prepare_package -> prepare_packet | ||
sl_flex_packet_asm.h | sl_rail_sdk_packet_asm.h | Change part of names: FLEX -> RAIL_SDK, flex -> rail_sdk | |
sl_flex_rail_sleep.h | Rename API: sl_flex_rail_sleep_init -> sl_rail_sdk_sleep_init | ||
sl_flex_util_802154_init.h | sl_rail_sdk_util_802154_init.h | Change part of names: sl_flex_util_init -> sl_rail_sdk_util_init, sl_flex_util_get_handle -> sl_rail_sdk_util_get_handle | |
sl_flex_util_ble_init.h | sl_rail_sdk_util_ble_init.h | Change part of names: sl_flex_util_init -> sl_rail_sdk_util_init, sl_flex_util_get_handle -> sl_rail_sdk_util_get_handle | |
sl_flex_util_ble_protocol.h | sl_rail_sdk_util_ble_protocol.h | Rename include sl_flex_util_ble_protocol_config -> sl_rail_sdk_util_ble_protocol_config | |
sl_rail_simple_cpc.h | sl_rail_sdk_simple_cpc.h | Change part of names: rail -> rail_sdk | |
sl_wmbus_packet_assembler.h | Change part of names: wmbus -> rail_sdk_wmbus | ||
sl_wmbus_sensor_pulse_counter.h | Change part of names: wmbus -> rail_sdk_wmbus | ||
sl_wmbus_sensor_pulse_counter.h | Change part of names: wmbus -> rail_sdk_wmbus | ||
sl_wmbus_sensor_thermometer.h | Change part of names: wmbus -> rail_sdk_wmbus | ||
sl_wmbus_sensor_virtual_water_meter.h | Change part of names: wmbus -> rail_sdk_wmbus |