Auto-Ack#
APIs for configuring Auto-Ack functionality.
These APIs configure the radio for automatic acknowledgment features. Auto-Ack inherently changes how the underlying state machine behaves so users should not modify RAIL_SetRxTransitions() and RAIL_SetTxTransitions() while using Auto-Ack features.
// Go to RX after Ack operation.
RAIL_AutoAckConfig_t autoAckConfig = {
.enable = true,
.ackTimeout = 1000,
.rxTransitions = {
.success = RAIL_RF_STATE_RX,
.error = RAIL_RF_STATE_RX
},
.txTransitions = {
.success = RAIL_RF_STATE_RX,
.error = RAIL_RF_STATE_RX,
},
};
RAIL_Status_t status = RAIL_ConfigAutoAck(railHandle, &autoAckConfig);
uint8_t ackData[] = {0x05, 0x02, 0x10, 0x00};
RAIL_Status_t status = RAIL_WriteAutoAckFifo(railHandle,
ackData,
sizeof(ackData));
The acknowledgment transmits based on the frame format configured via the Radio Configurator. For example, if the frame format is using a variable length scheme, the Ack will be sent according to that scheme. If a 10-byte packet is loaded into the Ack, but the variable length field of the Ack payload specifies a length of 5, only 5 bytes will transmit for the Ack. The converse is also true, if the frame length is configured to be a fixed 10-byte packet but only 5 bytes are loaded into the Ack buffer, a TX underflow occurs during the Ack transmit.
Unlike in non-Auto-Ack mode, Auto-Ack mode will always return to a single state after all Ack sequences complete, regardless of whether the Ack was successfully received/sent or not. See the documentation of RAIL_ConfigAutoAck() for configuration information. To suspend automatic acknowledgment of a series of packets after transmit or receive call RAIL_PauseTxAutoAck() or RAIL_PauseRxAutoAck() respectively with the pause parameter set to true. When Auto-Acking is paused, after receiving or transmitting a packet (regardless of success), the radio transitions to the same state it would use while Acking. To return to normal state transition logic outside of Acking, call RAIL_ConfigAutoAck() with the RAIL_AutoAckConfig_t::enable field false and specify the desired transitions in the RAIL_AutoAckConfig_t::rxTransitions and RAIL_AutoAckConfig_t::txTransitions fields. To get out of a paused state and resume Auto-Acking, call RAIL_PauseTxAutoAck() and/or RAIL_PauseRxAutoAck() with the pause parameter set to false.
Applications can cancel the transmission of an Ack with RAIL_CancelAutoAck(). Conversely, applications can control if a transmit operation should wait for an Ack after transmitting by using the RAIL_TX_OPTION_WAIT_FOR_ACK option.
When Antenna Control is used for multiple antennas, Acks are transmitted on the antenna that was selected to receive the packet being acknowledged. When receiving an Ack, the RAIL_RxOptions_t antenna options are used just like for any other receive.
If the Ack payload is dynamic, the application must call RAIL_WriteAutoAckFifo() with the appropriate Ack payload after the application processes the receive. RAIL can Auto-Ack from the normal transmit buffer if RAIL_UseTxFifoForAutoAck() is called before the radio transmits the Ack. Ensure the transmit buffer contains data loaded by RAIL_WriteTxFifo().
Standard-based protocols that contain Auto-Ack functionality are normally configured in the protocol-specific configuration function. For example, RAIL_IEEE802154_Init() provides Auto-Ack configuration parameters in RAIL_IEEE802154_Config_t and should only be configured through that function. It is not advisable to call both RAIL_IEEE802154_Init() and RAIL_ConfigAutoAck(). However, Ack modification functions are still valid to use with protocol-specific Acks. To cancel an IEEE 802.15.4 Ack transmit, use RAIL_CancelAutoAck().
These APIs configure the radio for automatic acknowledgment features. Auto-Ack inherently changes how the underlying state machine behaves so users should not modify sl_rail_set_rx_transitions() and sl_rail_set_tx_transitions() while using Auto-Ack features.
// Go to RX after Ack operation.
sl_rail_auto_ack_config_t auto_ack_config = {
.enable = true,
.ack_timeout_us = 1000,
// "error" param ignored
.rx_transitions = {
.success = SL_RAIL_RF_STATE_RX,
.error = SL_RAIL_RF_STATE_RX
},
// "error" param ignored
.tx_transitions = {
.success = SL_RAIL_RF_STATE_RX,
.error = SL_RAIL_RF_STATE_RX,
},
};
sl_rail_status_t status = sl_rail_config_auto_ack(rail_handle, &auto_ack_config);
uint8_t ack_data[] = {0x05, 0x02, 0x10, 0x00};
sl_rail_status_t status = sl_rail_write_auto_ack_fifo(rail_handle,
ack_data,
sizeof(ack_data));
The acknowledgment transmits based on the frame format configured via the Radio Configurator. For example, if the frame format is using a variable length scheme, the Ack will be sent according to that scheme. If a 10-byte packet is loaded into the Ack, but the variable length field of the Ack payload specifies a length of 5, only 5 bytes will transmit for the Ack. The converse is also true, if the frame length is configured to be a fixed 10-byte packet but only 5 bytes are loaded into the Ack buffer, a TX underflow occurs during the Ack transmit.
Unlike in non-Auto-Ack mode, Auto-Ack mode will always return to a single state after all Ack sequences complete, regardless of whether the Ack was successfully received/sent or not. See the documentation of sl_rail_config_auto_ack() for configuration information. To suspend automatic acknowledgment of a series of packets after transmit or receive call sl_rail_pause_tx_auto_ack() or sl_rail_pause_rx_auto_ack() respectively with the pause parameter set to true. When Auto-Acking is paused, after receiving or transmitting a packet (regardless of success), the radio transitions to the same state it would use while Acking. To return to normal state transition logic outside of Acking, call sl_rail_config_auto_ack() with the sl_rail_auto_ack_config_t::enable field false and specify the desired transitions in the sl_rail_auto_ack_config_t::rx_transitions and sl_rail_auto_ack_config_t::tx_transitions fields. To get out of a paused state and resume Auto-Acking, call sl_rail_pause_tx_auto_ack() and/or sl_rail_pause_rx_auto_ack() with the pause parameter set to false.
Applications can cancel the transmission of an Ack with sl_rail_cancel_auto_ack(). Conversely, applications can control if a transmit operation should wait for an Ack after transmitting by using the SL_RAIL_TX_OPTION_WAIT_FOR_ACK option.
When Antenna Control is used for multiple antennas, Acks are transmitted on the antenna that was selected to receive the packet being acknowledged. When receiving an Ack, the sl_rail_rx_options_t antenna options are used just like for any other receive.
If the Ack payload is dynamic, the application must call sl_rail_write_auto_ack_fifo() with the appropriate Ack payload after the application processes the receive. RAIL can Auto-Ack from the normal transmit buffer if sl_rail_use_tx_fifo_for_auto_ack() is called before the radio transmits the Ack. Ensure the transmit buffer contains data loaded by sl_rail_write_tx_fifo().
Standard-based protocols that contain Auto-Ack functionality are normally configured in the protocol-specific configuration function. For example, sl_rail_ieee802154_init() provides Auto-Ack configuration parameters in sl_rail_ieee802154_config_t and should only be configured through that function. It is not advisable to call both sl_rail_ieee802154_init() and sl_rail_config_auto_ack(). However, Ack modification functions are still valid to use with protocol-specific Acks. To cancel an IEEE 802.15.4 Ack transmit, use sl_rail_cancel_auto_ack().
Modules#
Functions#
Configure and enable automatic acknowledgment.
Return the enable status of the Auto-Ack feature.
Load the Auto-Ack buffer with Ack data.
Get the address and size of the Auto-Ack transmit buffer for direct access.
Pause/resume RX Auto-Ack functionality.
Return whether the RX Auto-Ack is paused.
Pause/resume TX Auto-Ack functionality.
Return whether the TX Auto-Ack is paused.
Modify the upcoming Ack to use the transmit FIFO.
Cancel the upcoming Ack.
Return whether the radio is currently waiting for an Ack.
Configure and enable automatic acknowledgment.
Return the enable status of the Auto-Ack feature.
Load the Auto-Ack buffer with Ack data.
Get the address and size of the Auto-Ack transmit buffer for direct access.
Set the address and size of the Auto-Ack transmit buffer, possibly pre-populated with some Ack data.
Pause/resume RX Auto-Ack functionality.
Return whether the RX Auto-Ack is paused.
Pause/resume TX Auto-Ack functionality.
Return whether the TX Auto-Ack is paused.
Modify the upcoming Ack to use the transmit FIFO.
Cancel the upcoming Ack.
Return whether the radio is currently waiting for an Ack.
Macros#
Acknowledgment packets cannot be longer than 64 bytes.
The default size in bytes of the built-in per-protocol Auto-Ack FIFO.
Function Documentation#
RAIL_ConfigAutoAck#
RAIL_Status_t RAIL_ConfigAutoAck (RAIL_Handle_t railHandle, const RAIL_AutoAckConfig_t * config)
Configure and enable automatic acknowledgment.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| const RAIL_AutoAckConfig_t * | [in] | config | A pointer to an Auto-Ack configuration structure. |
Returns
Status code indicating success of the function call.
Configures the RAIL state machine for hardware-accelerated automatic acknowledgment. Ack timing parameters are defined in the configuration structure.
While Auto-Acking is enabled, do not call the following RAIL functions:
When Auto-Acking is enabled, only one state transition can be defined (without notion of success or error). Thus if you are enabling Auto-Ack (i.e., config->enable field is true) the "error" states of config->rxTransitions and config->txTransitions are ignored. After all Ack sequences, (success or fail) the state machine will return the radio to the "success" state, which can be either RAIL_RF_STATE_RX or RAIL_RF_STATE_IDLE (returning to RAIL_RF_STATE_TX is not supported). Alternatively when Auto-Acking is disabled (i.e., config->enable field is false), transitions are reconfigured using all fields of config->rxTransitions and config->txTransitions. When disabling, the "ackTimeout" field isn't used.
If you need information about the actual success of the Ack sequence, use RAIL events such as RAIL_EVENT_TXACK_PACKET_SENT to make sure an Ack was sent, or RAIL_EVENT_RX_ACK_TIMEOUT to make sure that an Ack was received within the specified timeout.
To set a certain turnaround time (i.e., txToRx and rxToTx in RAIL_StateTiming_t), make txToRx lower than desired to ensure you get to RX in time to receive the Ack. Silicon Labs recommends setting 10 us lower than desired:
void setAutoAckStateTimings(void)
{
RAIL_StateTiming_t timings;
// User is already in Auto-Ack and wants a turnaround of 192 us.
timings.rxToTx = 192;
timings.txToRx = 192 - 10;
// Set other fields of timings...
timings.idleToRx = 100;
timings.idleToTx = 100;
timings.rxSearchTimeout = 0;
timings.txToRxSearchTimeout = 0;
RAIL_SetStateTiming(railHandle, &timings);
}
Note
Auto-Acking may not be enabled while RX Channel Hopping is enabled, or when BLE is enabled.
DeprecatedRAIL 2.x synonym of sl_rail_config_auto_ack().
RAIL_IsAutoAckEnabled#
bool RAIL_IsAutoAckEnabled (RAIL_Handle_t railHandle)
Return the enable status of the Auto-Ack feature.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
Returns
true if Auto-Ack is enabled, false if disabled.
DeprecatedRAIL 2.x synonym of sl_rail_is_auto_ack_enabled().
RAIL_WriteAutoAckFifo#
RAIL_Status_t RAIL_WriteAutoAckFifo (RAIL_Handle_t railHandle, const uint8_t * ackData, uint16_t ackDataLen)
Load the Auto-Ack buffer with Ack data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| const uint8_t * | [in] | ackData | A pointer to Ack data to transmit. This may be NULL, in which case it's assumed the data has already been emplaced into the Ack buffer and RAIL just needs to be told how many bytes are there. Use RAIL_GetAutoAckFifo() to get the address of RAIL's Auto-Ack buffer in RAM and its size. |
| uint16_t | [in] | ackDataLen | The number of bytes in Ack data. |
Returns
Status code indicating success of the function call.
If the Ack buffer is available for updates, load the Ack buffer with data. If it is not available, RAIL_STATUS_INVALID_STATE is returned. If ackDataLen exceeds RAIL_AUTOACK_MAX_LENGTH then RAIL_STATUS_INVALID_PARAMETER will be returned and nothing is written to the Ack buffer (unless ackData is NULL in which case this indicates the application has already likely corrupted RAM).
DeprecatedRAIL 2.x synonym of sl_rail_write_auto_ack_fifo().
RAIL_GetAutoAckFifo#
RAIL_Status_t RAIL_GetAutoAckFifo (RAIL_Handle_t railHandle, uint8_t ** ackBuffer, uint16_t * ackBufferBytes)
Get the address and size of the Auto-Ack transmit buffer for direct access.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| uint8_t ** | [inout] | ackBuffer | A pointer to a uint8_t pointer that will be updated to the RAM base address of the Auto-Ack FIFO buffer. |
| uint16_t * | [inout] | ackBufferBytes | A pointer to a uint16_t that will be updated to the size of the Auto-Ack FIFO buffer, in bytes, currently RAIL_AUTOACK_MAX_LENGTH. |
Returns
Status code indicating success of the function call.
Applications can use this to more flexibly write Auto-Ack data into the buffer directly and in pieces, passing NULL ackData parameter to RAIL_WriteAutoAckFifo() or RAIL_IEEE802154_WriteEnhAck() to inform RAIL of its final length.
DeprecatedRAIL 2.x synonym of sl_rail_get_auto_ack_fifo().
RAIL_PauseRxAutoAck#
RAIL_Status_t RAIL_PauseRxAutoAck (RAIL_Handle_t railHandle, bool pause)
Pause/resume RX Auto-Ack functionality.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| bool | [in] | pause | Pause or resume RX Auto-Acking. |
Returns
Status code indicating success of the function call.
When RX Auto-Acking is paused, the radio transitions to RAIL_AutoAckConfig_t::rxTransitions's RAIL_StateTransitions_t::success state after receiving a packet and does not transmit an Ack. When RX Auto-Ack is resumed, the radio resumes automatically Acking every successfully received packet.
DeprecatedRAIL 2.x synonym of sl_rail_pause_rx_auto_ack().
RAIL_IsRxAutoAckPaused#
bool RAIL_IsRxAutoAckPaused (RAIL_Handle_t railHandle)
Return whether the RX Auto-Ack is paused.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
Returns
true if RX Auto-Ack is paused, false if not paused.
DeprecatedRAIL 2.x synonym of sl_rail_is_rx_auto_ack_paused().
RAIL_PauseTxAutoAck#
RAIL_Status_t RAIL_PauseTxAutoAck (RAIL_Handle_t railHandle, bool pause)
Pause/resume TX Auto-Ack functionality.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| bool | [in] | pause | Pause or resume TX Auto-Acking. |
Returns
Status code indicating success of the function call.
When TX Auto-Acking is paused, the radio transitions to RAIL_AutoAckConfig_t::txTransitions's RAIL_StateTransitions_t::success state after transmitting a packet and does not wait for an Ack. When TX Auto-Ack is resumed, the radio resumes automatically waiting for an Ack after a successful transmit.
DeprecatedRAIL 2.x synonym of sl_rail_pause_tx_auto_ack().
RAIL_IsTxAutoAckPaused#
bool RAIL_IsTxAutoAckPaused (RAIL_Handle_t railHandle)
Return whether the TX Auto-Ack is paused.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
Returns
true if TX Auto-Ack is paused, false if not paused.
DeprecatedRAIL 2.x synonym of sl_rail_is_tx_auto_ack_paused().
RAIL_UseTxFifoForAutoAck#
RAIL_Status_t RAIL_UseTxFifoForAutoAck (RAIL_Handle_t railHandle)
Modify the upcoming Ack to use the transmit FIFO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
Returns
Status code indicating success of the function call. The call will fail if it is too late to modify the outgoing Ack.
This function allows the application to use the normal transmit FIFO as the data source for the upcoming Ack. The Ack modification to use the transmit FIFO only applies to one Ack transmission.
This function only returns true if the following conditions are met:
Radio has not already decided to use the Ack buffer AND
Radio is either looking for sync, receiving the packet after sync, or in the RAIL_StateTiming_t::rxToTx turnaround before the Ack is sent.
Note
Call before RAIL_EVENT_RX_PACKET_RECEIVED (for example from RAIL_EVENT_RX_FILTER_PASSED) so Auto-Ack can use the transmit FIFO.
The transmit FIFO must not be used for Auto-Ack when IEEE 802.15.4, Z-Wave, or BLE protocols are active.
DeprecatedRAIL 2.x synonym of sl_rail_use_tx_fifo_for_auto_ack().
RAIL_CancelAutoAck#
RAIL_Status_t RAIL_CancelAutoAck (RAIL_Handle_t railHandle)
Cancel the upcoming Ack.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
Returns
Status code indicating success of the function call. This call will fail if it is too late to modify the outgoing Ack.
This function allows the application to cancel the upcoming automatic acknowledgment.
This function only returns true if the following conditions are met:
Radio has not already decided to transmit the Ack, and
Radio is either looking for sync, receiving the packet after sync or in the RAIL_StateTiming_t::rxToTx turnaround before the Ack is sent.
Note
Call before RAIL_EVENT_RX_PACKET_RECEIVED (for example from RAIL_EVENT_RX_FILTER_PASSED) so Auto-Ack can cancel the upcoming Ack.
DeprecatedRAIL 2.x synonym of sl_rail_cancel_auto_ack().
RAIL_IsAutoAckWaitingForAck#
bool RAIL_IsAutoAckWaitingForAck (RAIL_Handle_t railHandle)
Return whether the radio is currently waiting for an Ack.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
Returns
true if radio is waiting for Ack, false if radio is not waiting for an Ack.
This function allows the application to query whether the radio is currently waiting for an Ack after a transmit operation.
DeprecatedRAIL 2.x synonym of sl_rail_is_auto_ack_waiting_for_ack().
sl_rail_config_auto_ack#
sl_rail_status_t sl_rail_config_auto_ack (sl_rail_handle_t rail_handle, const sl_rail_auto_ack_config_t * p_auto_ack_config)
Configure and enable automatic acknowledgment.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| const sl_rail_auto_ack_config_t * | [in] | p_auto_ack_config | A pointer to an Auto-Ack configuration structure. |
Returns
Status code indicating success of the function call.
Configures the RAIL state machine for hardware-accelerated automatic acknowledgment. Ack timing parameters are defined in the configuration structure.
While Auto-Acking is enabled, do not call the following RAIL functions:
When Auto-Acking is enabled, only one state transition can be defined (without notion of success or error). Thus if you are enabling Auto-Ack (i.e., p_config->enable field is true) the "error" states of p_config->rx_transitions and p_config->tx_transitions are ignored. After all Ack sequences, (success or fail) the state machine will return the radio to the "success" state, which can be either SL_RAIL_RF_STATE_RX or SL_RAIL_RF_STATE_IDLE (returning to SL_RAIL_RF_STATE_TX is not supported). Alternatively when Auto-Acking is disabled (i.e., p_config->enable field is false), transitions are reconfigured using all fields of p_config->rx_transitions and p_config->tx_transitions. When disabling, the "ack_timeout" field isn't used.
If you need information about the actual success of the Ack sequence, use RAIL events such as SL_RAIL_EVENT_TXACK_PACKET_SENT to make sure an Ack was sent, or SL_RAIL_EVENT_RX_ACK_TIMEOUT to make sure that an Ack was received within the specified timeout.
To set a certain turnaround time (i.e., tx_to_rx and rx_to_tx in sl_rail_state_timing_t), make tx_to_rx lower than desired to ensure you get to RX in time to receive the Ack. Silicon Labs recommends setting 10 us lower than desired:
void set_auto_ack_state_timings(void)
{
sl_rail_state_timing_t timings;
// User is already in Auto-Ack and wants a turnaround of 192 us.
timings.rx_to_tx = 192;
timings.tx_to_rx = 192 - 10;
// Set other fields of timings...
timings.idle_to_rx = 100;
timings.idle_to_tx = 100;
timings.rxsearch_timeout = 0;
timings.tx_to_rxsearch_timeout = 0;
sl_rail_set_state_timing(rail_handle, &timings);
}
Note
Auto-Acking may not be enabled while RX Channel Hopping is enabled, or when BLE is enabled.
sl_rail_is_auto_ack_enabled#
bool sl_rail_is_auto_ack_enabled (sl_rail_handle_t rail_handle)
Return the enable status of the Auto-Ack feature.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
Returns
true if Auto-Ack is enabled, false if disabled.
sl_rail_write_auto_ack_fifo#
sl_rail_status_t sl_rail_write_auto_ack_fifo (sl_rail_handle_t rail_handle, const uint8_t * p_ack_data, uint16_t ack_bytes)
Load the Auto-Ack buffer with Ack data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| const uint8_t * | [in] | p_ack_data | A pointer to Ack data to transmit. This may be NULL, in which case it's assumed the data has already been emplaced into the Ack buffer and RAIL just needs to be told how many bytes are there. Use sl_rail_get_auto_ack_fifo() to get the address of RAIL's Auto-Ack buffer in RAM and its size. |
| uint16_t | [in] | ack_bytes | The number of bytes in Ack data. |
Returns
Status code indicating success of the function call.
If the Ack buffer is available for updates, load the Ack buffer with data. If it is not available, SL_RAIL_STATUS_INVALID_STATE is returned. If ack_bytes exceeds the size of the Auto-Ack FIFO buffer then SL_RAIL_STATUS_INVALID_PARAMETER will be returned and nothing is written to the Ack buffer (unless p_ack_data is NULL in which case this indicates the application has already likely corrupted RAM).
sl_rail_get_auto_ack_fifo#
sl_rail_status_t sl_rail_get_auto_ack_fifo (sl_rail_handle_t rail_handle, uint8_t ** pp_ack_buffer, uint16_t * p_ack_buffer_bytes)
Get the address and size of the Auto-Ack transmit buffer for direct access.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| uint8_t ** | [inout] | pp_ack_buffer | A pointer to a uint8_t pointer that will be updated to the RAM base address of the Auto-Ack FIFO buffer. |
| uint16_t * | [inout] | p_ack_buffer_bytes | A pointer to a uint16_t that will be updated to the size of the Auto-Ack FIFO buffer, in bytes. |
Returns
Status code indicating success of the function call.
Applications can use this to more flexibly write Auto-Ack data into the buffer directly and in pieces, passing NULL p_ack_data parameter to sl_rail_write_auto_ack_fifo() or sl_rail_ieee802154_write_enh_ack() to inform RAIL of its final length.
sl_rail_set_auto_ack_fifo#
sl_rail_status_t sl_rail_set_auto_ack_fifo (sl_rail_handle_t rail_handle, sl_rail_fifo_buffer_align_t * p_ack_fifo, uint16_t size_bytes, uint16_t init_bytes)
Set the address and size of the Auto-Ack transmit buffer, possibly pre-populated with some Ack data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| sl_rail_fifo_buffer_align_t * | [inout] | p_ack_fifo | An appropriately-aligned (see sl_rail_set_tx_fifo description) pointer to a read-write memory location in RAM used as the transmit FIFO for acknowledgement packets. This memory must persist until the next call to this function. If NULL, will re-establish the built-in per-protocol FIFO of size SL_RAIL_DEFAULT_AUTO_ACK_FIFO_BYTES (offset must be 0 in this case). |
| uint16_t | [in] | size_bytes | The desired size of the buffer in bytes. Must be greater than SL_RAIL_DEFAULT_AUTO_ACK_FIFO_BYTES and less than or equal to SL_RAIL_MAXIMUM_FIFO_BYTES. |
| uint16_t | [in] | init_bytes | The number of valid bytes already populated in the buffer. Must be less than or equal to size_bytes. |
Returns
Status code indicating success of the function call.
sl_rail_pause_rx_auto_ack#
sl_rail_status_t sl_rail_pause_rx_auto_ack (sl_rail_handle_t rail_handle, bool pause)
Pause/resume RX Auto-Ack functionality.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| bool | [in] | pause | Pause or resume RX Auto-Acking. |
Returns
Status code indicating success of the function call.
When RX Auto-Acking is paused, the radio transitions to sl_rail_auto_ack_config_t::rx_transitions's sl_rail_state_transitions_t::success state after receiving a packet and does not transmit an Ack. When RX Auto-Ack is resumed, the radio resumes automatically Acking every successfully received packet.
sl_rail_is_rx_auto_ack_paused#
bool sl_rail_is_rx_auto_ack_paused (sl_rail_handle_t rail_handle)
Return whether the RX Auto-Ack is paused.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
Returns
true if RX Auto-Ack is paused, false if not paused.
sl_rail_pause_tx_auto_ack#
sl_rail_status_t sl_rail_pause_tx_auto_ack (sl_rail_handle_t rail_handle, bool pause)
Pause/resume TX Auto-Ack functionality.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| bool | [in] | pause | Pause or resume TX Auto-Acking. |
Returns
Status code indicating success of the function call.
When TX Auto-Acking is paused, the radio transitions to sl_rail_auto_ack_config_t::tx_transitions's sl_rail_state_transitions_t::success state after transmitting a packet and does not wait for an Ack. When TX Auto-Ack is resumed, the radio resumes automatically waiting for an Ack after a successful transmit.
sl_rail_is_tx_auto_ack_paused#
bool sl_rail_is_tx_auto_ack_paused (sl_rail_handle_t rail_handle)
Return whether the TX Auto-Ack is paused.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
Returns
true if TX Auto-Ack is paused, false if not paused.
sl_rail_use_tx_fifo_for_auto_ack#
sl_rail_status_t sl_rail_use_tx_fifo_for_auto_ack (sl_rail_handle_t rail_handle)
Modify the upcoming Ack to use the transmit FIFO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
Returns
Status code indicating success of the function call. The call will fail if it is too late to modify the outgoing Ack.
This function allows the application to use the normal transmit FIFO as the data source for the upcoming Ack. The Ack modification to use the transmit FIFO only applies to one Ack transmission.
This function only returns true if the following conditions are met:
Radio has not already decided to use the Ack buffer AND
Radio is either looking for sync, receiving the packet after sync, or in the sl_rail_state_timing_t::rx_to_tx turnaround before the Ack is sent.
Note
Call before SL_RAIL_EVENT_RX_PACKET_RECEIVED (for example from SL_RAIL_EVENT_RX_FILTER_PASSED) so Auto-Ack can use the transmit FIFO.
The transmit FIFO must not be used for Auto-Ack when IEEE 802.15.4, Z-Wave, or BLE protocols are active.
sl_rail_cancel_auto_ack#
sl_rail_status_t sl_rail_cancel_auto_ack (sl_rail_handle_t rail_handle)
Cancel the upcoming Ack.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
Returns
Status code indicating success of the function call. This call will fail if it is too late to modify the outgoing Ack.
This function allows the application to cancel the upcoming automatic acknowledgment.
This function only returns true if the following conditions are met:
Radio has not already decided to transmit the Ack, and
Radio is either looking for sync, receiving the packet after sync, or in the sl_rail_state_timing_t::rx_to_tx turnaround before the Ack is sent.
Note
Call before SL_RAIL_EVENT_RX_PACKET_RECEIVED (for example from SL_RAIL_EVENT_RX_FILTER_PASSED) so Auto-Ack can cancel the upcoming Ack.
sl_rail_is_auto_ack_waiting_for_ack#
bool sl_rail_is_auto_ack_waiting_for_ack (sl_rail_handle_t rail_handle)
Return whether the radio is currently waiting for an Ack.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
Returns
true if radio is waiting for Ack, false if radio is not waiting for an Ack.
This function allows the application to query whether the radio is currently waiting for an Ack after a transmit operation.