Opermode Parameters#

In rsi_wireless_init() API, configured feature bitmaps are internally processed and sent to firmware. Default configurations (for reference) are available in rsi_wlan_common_config.h. Based on the features required for a specific example, modify the rsi_wlan_config.h provided in the respective example folder. The following configuration parameters are used to configure feature bitmaps.

RSI_FEATURE_BIT_MAP#

This bitmap is used to enable the following WLAN features.

feature_bit_map

Macro defined in SAPI

Functionality

Set to 0

Set to 1

Additional Notes

feature_bit_map[0]

FEAT_SECURITY_OPEN

Open mode feature

Disable

Enable

Supported in client mode

feature_bit_map[1]

FEAT_SECURITY_PSK

PSK security

Disable

Enable

Supported in client mode

feature_bit_map[2]

FEAT_AGGREGATION

Aggregation

Disable

Enable

feature_bit_map[3]

FEAT_LP_GPIO_BASED_HANDSHAKE

LP GPIO hand shake

Disable

Enable

feature_bit_map[4]

FEAT_ULP_GPIO_BASED_HANDSHAKE

ULP GPIO hand shake

Disable

Enable

feature_bit_map[5]

FEAT_DEV_TO_HOST_ULP_GPIO_1

Reserved

Reserved

Reserved

feature_bit_map[6]

FEAT_RF_SUPPY_VOL_3_3_VOLT

Reserved

Reserved

Reserved

feature_bit_map[7]

FEAT_WPS_DISABLE

WPS support

Enable

Disable

feature_bit_map[8]

FEAT_EAP_LEAP_IN_COEX

To support EAP/LEAP in Wi-Fi + BT Coex mode

Disable

Enable

feature_bit_map[9]

FEAT_HIDE_PSK_CREDENTIALS

To hide PSK, PMK and EAP credentials from the user

Disable

Enable

feature_bit_map[11]

TLS_PATH_LENGTH_SUPPORT

To support certificate pathlength

Disable

Enable

This feature need to be enable when pathLenConstraint field is present in given certificate.it gives the maximum number of non-self-issued intermediate certificates that may follow this certificate in a valid certification path.A pathLenConstraint of zero indicates that no non self-issued intermediate CA certificates may follow in a valid certification path.

feature_bit_map[12:31]

-

Reserved. Should be set to 0


Note!feature_bit_map[0], feature_bit_map[1] are valid only in Wi-Fi Client mode.

Note!feature_bit_map[11] This is not enabled by default, because this feature can't be used along with window scaling or certificate bypass features as these are mutually exclusive.


RSI_TCP_IP_FEATURE_BIT_MAP#

To enable TCP/IP related features.

tcp_ip_feature_bit_map

Macro defined in SAPI

Functionality

Set to 0

Set to 1

Additional Notes

tcp_ip_feature_bit_map[0]

TCP_IP_FEAT_BYPASS

TCP/IP bypass

Disable

Enable

When this feature is enabled, the TCP/IP stack processing is bypassed, allowing raw Ethernet frames to be sent and received. This is useful for applications that require direct control over Ethernet frames or for implementing custom network protocols, This is defined as a bit flag that can be set in the feature configuration to enable the TCP/IP bypass.

tcp_ip_feature_bit_map[1]

-

Reserved

Set to 0

tcp_ip_feature_bit_map[2]

TCP_IP_FEAT_DHCPV4_CLIENT

DHCPv4 client

Disable

Enable

This feature allows the device to obtain an IPv4 address, subnet mask, default gateway, and DNS server from a DHCP server.

tcp_ip_feature_bit_map[3]

TCP_IP_FEAT_DHCPV6_CLIENT

DHCPv6 client

Disable

Enable

This feature allows the device to obtain an IPv6 address, and other network configuration details from a DHCPv6 server.

tcp_ip_feature_bit_map[4]

TCP_IP_FEAT_DHCPV4_SERVER

DHCPv4 server

Disable

Enable

This feature allows the device to act as a DHCPv4 server, providing IPv4 addresses and network configuration to DHCPv4 clients on the network.

tcp_ip_feature_bit_map[5]

TCP_IP_FEAT_DHCPV6_SERVER

DHCPv6 server

Disable

Enable

This feature allows the device to act as a DHCPv6 server, providing IPv6 addresses and network configuration to DHCPv6 clients on the network.

tcp_ip_feature_bit_map[6]

TCP_IP_FEAT_JSON_OBJECTS

Dynamic update of web pages (JSON objects)

Disable

Enable

This feature allows the device to handle JSON (JavaScript Object Notation) objects, which can be used for data interchange in web applications.

tcp_ip_feature_bit_map[7]

TCP_IP_FEAT_HTTP_CLIENT

HTTP client

Disable

Enable

This feature allows the device to send HTTP requests and receive HTTP responses from web servers, enabling web-based communication.

tcp_ip_feature_bit_map[8]

TCP_IP_FEAT_DNS_CLIENT

DNS client

Disable

Enable

This feature allows the device to resolve domain names to IP addresses using the Domain Name System (DNS), enabling communication with servers by hostname.

tcp_ip_feature_bit_map[9]

TCP_IP_FEAT_SNMP_AGENT

SNMP agent

Disable

Enable

This feature allows the device to act as an SNMP (Simple Network Management Protocol) agent, enabling network management and monitoring.

tcp_ip_feature_bit_map[10]

TCP_IP_FEAT_SSL

SSL/TLS

Disable

Enable

This feature allows the device to use SSL (Secure Sockets Layer) for secure communication over the network, providing encryption and authentication.

tcp_ip_feature_bit_map[11]

TCP_IP_FEAT_ICMP

PING from device (ICMP)

Disable

Enable

This feature allows the device to use ICMP (Internet Control Message Protocol) for network diagnostics, such as sending ping requests.

tcp_ip_feature_bit_map[12]

-

Reserved

Set to 0

tcp_ip_feature_bit_map[13]

-

Set to 0

tcp_ip_feature_bit_map[14]

TCP_IP_FEAT_SEND_CONFIGS_TO_HOST

Sending configuration data to the host

Disable

Enable

This feature allows the device to send web page configuration data to the host system from the wireless configuration page.

tcp_ip_feature_bit_map[15]

TCP_IP_FEAT_FTP_CLIENT

FTP client

Disable

Enable

This feature allows the device to act as an FTP (File Transfer Protocol)client, enabling file transfers to and from FTP servers.

tcp_ip_feature_bit_map[16]

TCP_IP_FEAT_SNTP_CLIENT

SNTP client

Disable

Enable

This feature allows the device to synchronize its clock with an SNTP(Simple Network Time Protocol) server, ensuring accurate timekeeping.

tcp_ip_feature_bit_map[17]

TCP_IP_FEAT_IPV6

IPv6 mode

Disable

Enable

This feature allows the device to use IPv6 (Internet Protocol version 6),providing a larger address space and improved routing capabilities,IPv6 will also be enabled if the DHCPv6 client or DHCPv6 server feature is enabled, regardless of the tcp_ip_feature_bit_map[17] setting.

tcp_ip_feature_bit_map[18]

TCP_IP_FEAT_RAW_DATA

RAW Socket feature

Disable

Enable

This feature allows the device to handle raw data frames, bypassing the TCP/IP stack. It is supported only in AP mode and requires the TCP_BYPASS feature to be disabled. If any packet from the host with frame type 0x1 is received by the firmware, the packet will be sent on air without TCP/IP stack processing. ARP and broadcast packets (other than DHCP packets) received on air will be sent to the host.

tcp_ip_feature_bit_map[19]

TCP_IP_FEAT_MDNSD

To MDNS and DNS-SD

Disable

Enable

This feature allows the device to use Multicast DNS (mDNS) for local network service discovery, enabling devices to find each other without a central DNS server.

tcp_ip_feature_bit_map[20]

TCP_IP_FEAT_SMTP_CLIENT

SMTP client

Disable

Enable

This feature allows the device to act as an SMTP (Simple Mail Transfer Protocol) client, enabling it to send emails.

tcp_ip_feature_bit_map[21:24]

TCP_IP_TOTAL_SOCKETS_1 TCP_IP_TOTAL_SOCKETS_2 TCP_IP_TOTAL_SOCKETS_3 TCP_IP_TOTAL_SOCKETS_4 TCP_IP_TOTAL_SOCKETS_5 TCP_IP_TOTAL_SOCKETS_6 TCP_IP_TOTAL_SOCKETS_7 TCP_IP_TOTAL_SOCKETS_8 TCP_IP_TOTAL_SOCKETS_9 TCP_IP_TOTAL_SOCKETS_10

To select no of sockets

Defined to maintain the socket related info on firmware side

tcp_ip_feature_bit_map[25]

TCP_IP_FEAT_SINGLE_SSL_SOCKET

Single SSL/TLS socket

Disable

Enable

This feature allows the device to use a single SSL socket for secure communication.

tcp_ip_feature_bit_map[26]

TCP_IP_FEAT_LOAD_PUBLIC_PRIVATE_CERTS

Private & Public certificate

Disable

Enable

If a secure handshake is to be done using only a CA-certificate, then loading of private and public keys can be disabled, and these certificates can be erased from the flash using the load_cert API. If secure handshake verification of private and public keys is needed, then loading of these keys must be enabled.

tcp_ip_feature_bit_map[27]

TCP_IP_FEAT_LOAD_CERTS_INTO_RAM

SSL/TLS certificate on to the RAM

Disable

Enable

This feature allows the device to load SSL certificates into RAM for faster access during secure communications.

tcp_ip_feature_bit_map[28]

Not defined

TCP-IP data packet Dump on UART2

Disable

Enable

tcp_ip_feature_bit_map[29]

TCP_IP_FEAT_POP3_CLIENT

POP3 client

Disable

Enable

This feature allows the device to act as a POP3 (Post Office Protocol version 3) client, enabling it to retrieve emails from a POP3 server.

tcp_ip_feature_bit_map[30]

TCP_IP_FEAT_OTAF

Enable OTAF (Over-the-Air Firmware) update.

Disable

Enable

This feature allows the device to perform over-the-air firmware (OTAF)updates, enabling it to download and install firmware updates remotely.

tcp_ip_feature_bit_map[31]

TCP_IP_FEAT_EXTENSION_VALID

tcp_ip_ext_feature_bitmap validity

Disable

Enable

This feature allows the device to use extended TCP/IP features, providing additional functionality and capabilities.


Note! A feature selection spreadsheet is provided in the WiSeConnect SDK. The device supports the selected combination of features only if it is feasible as per WiSeConnect_TCPIP_Feature_Selection_vx.x.x.xlsx.


RSI_CUSTOM_FEATURE_BIT_MAP#

This bitmap is used to enable following custom features.

custom_feature_bit_map

Macro defined in SAPI

Functionality

Set to 0

Set to 1

Additional Notes

custom_feature_bit_map[0]

-

Reserved

Set to 0

custom_feature_bit_map[1]

-

Reserved

Set to 0

custom_feature_bit_map[2]

CUSTOM_FEAT_DISABLE_GATEWAY_IN_RSI_AP

Disables gateway config sent to STA from RSI AP

Disable

Enable

If this bit is set to 1, the DHCP server behavior changes when the device is in AP mode. The DHCP server, when it assigns IP addresses to the client nodes, does not send out a Gateway address, and sends only the assigned IP and Subnet values to the client. It is highly recommended to keep this value at '0' as the changed behavior is required in only very specialized use cases and not in normal AP functionality. The default value of this bit is '0'.

custom_feature_bit_map[3]

-

Reserved

Set to 0

custom_feature_bit_map[4]

CUSTOM_FEAT_SOC_CLK_CONFIG_160MHZ

To run NWP (Network Processor) at Higher clock frequency (160 MHz)

Disable

Enable

Need to set pll_mode to '1' in the feature frame command to configure the clock for NWP SOC to 160Mhz. If higher performance is needed, such as high throughput, then this configuration is required.

custom_feature_bit_map[5]

CUSTOM_FEAT_AP_IN_HIDDEN_MODE

Hidden SSID in AP mode

Disable

Enable

This bit is only valid in AP mode. If set, the AP will be created in hidden mode.

custom_feature_bit_map[6]

CUSTOM_FEAT_DNS_SERVER_IN_DHCP_OFFER

DNS server IP address in DHCP offer response in AP mode.

Disable

Enable

This bit is valid only AP mode, DNS server IP address in DHCP offer response in AP mode

custom_feature_bit_map[7]

-

Reserved

Set to 0

custom_feature_bit_map[8]

CUSTOM_FEAT_DFS_CHANNEL_SUPPORT

DFS channel passive scan support

Disable

Enable

it's mandatory to set region before scanning DFS channel.

custom_feature_bit_map[10]

CUSTOM_FEAT_ASYNC_CONNECTION_STATUS

Asynchronous messages to host to indicate the device state.

Disable

Enable

If this bit is enabled,module indicates the host the wlan connection status asynchronously This bit is valid in case of Wifi client mode

custom_feature_bit_map[11]

CUSTOM_FEAT_WAKE_ON_WIRELESS

Packet pending wake on wireless indication in UART mode

Disable

Enable

If this bit is enabled,Wake on wireless indication in UART mode

custom_feature_bit_map[12]

CUSTOM_FEAT_ENABLE_AP_BLACKLIST

Bypass AP Blacklist in client mode

Disable

Enable

By default client maintains AP blacklist internally to avoid some access points. To bypass AP blacklist feature in client mode during roaming or rejoin, this feature should be enabled.

custom_feature_bit_map[17]

CUSTOM_FEAT_ROAM_WITH_DEAUTH_OR_NULLDATA

To select between de-authentication or null data (with power management bit set) based roaming.Depending on selected method station, it will send de-auth or Null data to the connected AP when roaming from connected AP to the newly selected AP.

Disable

Enable

custom_feature_bit_map[18]

-

Reserved

Set to 0

custom_feature_bit_map[19]

-

Reserved

Set to 0

custom_feature_bit_map[20]

CUSTOM_FEAT_TRIGGER_AUTO_CONFIG

Trigger Auto Configuration

Disable

Enable

custom_feature_bit_map[21]

-

Reserved

Set to 0

custom_feature_bit_map[22]

CUSTOM_FEAT_LIMIT_PACKETS_PER_STA

Used to enable per station power save packet buffer limit in AP mode.When enabled, only two packets per station will be buffered when station is in power save

Disable

Enable

custom_feature_bit_map[23]

CUSTOM_FEAT_HTTP_HTTPS_AUTH

HTTP/HTTPs authentication

Disable

Enable

custom_feature_bit_map[24]

CUSTOM_FEAT_SOC_CLK_CONFIG_120MHZ

To run the network processor on the device at a Higher clock frequency (120 MHz)

Disable

Enable

Need to set pll_mode to 1 in feature frame command

custom_feature_bit_map[25]

-

Reserved

Set to 0

custom_feature_bit_map[26]

CUSTOM_FEAT_REJECT_CONNECT_REQ_IMMEDIATELY

To accept or reject new connection request when maximum clients are connected in case of LTCP.

Disable

Enable

By default this bit value is zero. When BIT[26] = 0: For a LTCP socket when maximum clients are connected if a new connection request is received, then this connection request will not be rejected. Instead device will maintain this connection request in LTCP pending list. This request will be served when any of the connected client is disconnected. When BIT[26] = 1: For a LTCP socket when maximum clients are connected if a new connection request is received, then this connection request will be rejected immediately. Device will not maintain this connection request in LTCP pending list.

custom_feature_bit_map[27]

CUSTOM_FEAT_DUAL_BAND_ROAM_VCSAFD

Dual band roaming and vcsafd feature

Disable

Enable

custom_feature_bit_map[28]

CUSTOM_FEAT_RTC_FROM_HOST

Real time clock from host

Disable

Enable

custom_feature_bit_map[29]

CUSTOM_FEAT_BT_IAP

IAP support in BT mode

Disable

Enable

custom_feature_bit_map[30]

-

Reserved

Set to 0

custom_feature_bit_map[31]

FEAT_CUSTOM_FEAT_EXTENTION_VALID

ext_custom_feat_bitmap validity

Disable

Enable

RSI_EXT_CUSTOM_FEATURE_BIT_MAP#

This feature bitmap is an extension of custom_feature_bit_map and is valid only if custom_feature_bit_map[31] = 1. This enables the following features.

ext_custom_feature_bit_map

Macro defined in SAPI

Functionality

Set to 0

Set to 1

Additional Notes

ext_custom_feature_bit_map[0]

Reserved

Reserved

Disable

Enable

ext_custom_feature_bit_map[1]

EXT_FEAT_RSA_KEY_WITH_4096_SUPPORT

Reserves memory for EAP certificates with 4096 bit RSA keys.

Disable

Enable

This bit is required to be set for 4096 bit RSA key support. This bit does not denote feature enable/disable, i.e., eap connection with 4096 key certs may establish even though this bit is disabled if memory is available due to any reason. If key size is 4096 bit, device will use software routine for exponentiation, so connection time will increase.

ext_custom_feature_bit_map[2]

-

Reserved

ext_custom_feature_bit_map[3]

EXT_FEAT_SSL_CERT_WITH_4096_KEY_SUPPORT

SSL/TLS certificate with 4096 bit key support

Disable

Enable

ext_custom_feature_bit_map[4]

EXT_FEAT_AP_BROADCAST_PKT_SND_B4_DTIM

This bit is applicable only in AP and concurrent AP mode. If this bit is set, the device will send broadcast data (if any) immediately without waiting for DTIM.

Disable (AP sends broadcast packet at DTIM only.)

Enable (Enable sending broadcast without waiting for DTIM)

If this bit is enable then connected client who is in power save may miss the packet.

ext_custom_feature_bit_map[5]

EXT_FEAT_FCC_LOW_PWR

Pre authentication Support.

Disable

Enable

Extended custom bitmap to support FCC

ext_custom_feature_bit_map[6]

-

Reserved

ext_custom_feature_bit_map[7:8]

-

Reserved

ext_custom_feature_bit_map[9]

EXT_HTTP_SKIP_DEFAULT_LEADING_CHARACTER

EXT_HTTP_SKIP_DEFAULT_LEADING_CHARACTER. To skip default leading character ("\") in resource name

Extended feature bit map to skip default leading character '\' in HTTP header

ext_custom_feature_bit_map[10]

-

Reserved

ext_custom_feature_bit_map[11]

EXT_FEAT_ENABLE_11R_OTA

802.11R Over the Air Roaming Support

Disable

Enable

1. Resource Request Support is not Present. 2. If both BIT[11] and BIT[16] are not enabled then it will select as Legacy Roaming.

ext_custom_feature_bit_map[12]

EXT_FEAT_IEEE_80211J

802.11J support.

Disable

Enable

If this bit is enable, set region command is mandatory with setting it to Japan region and band value must be 1 (5GHz).

ext_custom_feature_bit_map[13]

EXT_FEAT_IEEE_80211W

802.11W support.

Disable

Enable

This bit must be set for enabling WPA3 Personal Mode and WPA3 Personal Transition mode.

ext_custom_feature_bit_map[14]

EXT_FEAT_SSL_VERSIONS_SUPPORT

TLS Multiple versions Support in SSL.

Disable

Enable

To enable the Multiverion TCP over SSL support

ext_custom_feature_bit_map[15]

EXT_FEAT_16th_STATION_IN_AP_MODE

Support 16 Stations in AP Mode.

If this bit is enable then 16 stations can connect in AP mode otherwise Maximum of 8 stations can connect.

ext_custom_feature_bit_map[16]

EXT_FEAT_ENABLE_11R_ODS

802.11R Over the Distributed System Roaming Support

1. Resource Request Support is not Present. 2. If both BIT[11] and BIT[16] are not enabled then it will select as Legacy Roaming.

ext_custom_feature_bit_map[17:18]

-

Reserved

ext_custom_feature_bit_map[19]

EXT_FEAT_LOW_POWER_MODE

Low power mode in GPIO based or M4 based ULP power save

EXT_FEAT_LOW_POWER_MODE is not supported for 1.3 version chipset.

ext_custom_feature_bit_map[20:21]

EXT_FEAT_320K_MODE EXT_FEAT_256K_MODE BIT EXT_FEAT_384K_MODE

Default memory configuration (RAM) is 192KB. User can set these bits to change the memory configuration as below:

Memory ConfigurationMemory Configuration
384k memory configuration is applicable only in WiSeConnect product mode.

ext_custom_feature_bit_map[22:23]

EXT_FEAT_XTAL_CLK_ENABLE

To configure sleep clock source selection, either crystal clock or RC clock

Sleep Clock TaSleep Clock Ta

If BIT[23] = 1 and BIT[22] = 0 in ext_custom_feature_bit_map, then user has to use UULP_GPIO_0 for sleep indication to host.

ext_custom_feature_bit_map[24]

EXT_FEAT_HOMEKIT_WAC_ENABLED

Reserved

ext_custom_feature_bit_map[25]

EXT_FEAT_1P8V_SUPPORT

To enable 1.8v supply for TA

Disable

Enable

To enable 1.8v support for TA

ext_custom_feature_bit_map[26]

Not defined

To enable 3.3v supply for TA

Disable

Enable

ext_custom_feature_bit_map[27]

EXT_FEAT_UART_SEL_FOR_DEBUG_PRINTS

To select UART port for the device network Processor debug prints

Disable (Enable debug prints on UART2)

Enable (Enable debug prints on UART1 and is applicable only if Host Interface is not UART)

By default all the debug prints from device network processor will be coming on UART2 if this bit is not enabled. UART1 pins are mapped to the following pins w.r.t to the device network processor. User needs to ensure that these pins are not used in MCU applications in SoC mode to avoid conflicts of pins usage based on the requirement. This bit is valid only if BIT[28] in ext_custom_feature_bit_map is set to 0. UART1-TX: GPIO_9 UART1-RX: GPIO_8 UART2-TX: GPIO_6 UART2-RX: GPIO_10 There is no functionality on rx pins for debug prints.

ext_custom_feature_bit_map[28]

EXT_FEAT_DISABLE_DEBUG_PRINTS

UART debug prints from device network processor

Disable (Enable debug prints)

Enable (Disable debug prints on either UART1 or UART2)

To select UART debug prints pin selection,If BIT(27) is enabled,Debug prints are supported on UART1, If BIT(27) is disabled,Debug prints are supported on UART2

ext_custom_feature_bit_map[29:30]

-

Reserved

ext_custom_feature_bit_map[31]

Not defined

BT and BLE Feature_Bit_Map validity

Disable

Enable

RSI_EXT_TCPIP_FEATURE_BITMAP#

ext_tcp_ip_feature_bit_map

Macro defined in SAPI

Functionality

Set to 0

Set to 1

Additional Notes

ext_tcp_ip_feature_bit_map[1]

EXT_TCP_FEAT_DHCP_OPT77

DHCP USER CLASS

Disable

Enable

This feature enable the DHCP option 77

ext_tcp_ip_feature_bit_map[2]

-

Reserved

Set to 0

ext_tcp_ip_feature_bit_map[3]

EXT_TCP_IP_BI_DIR_ACK_UPDATE

Correcting the ACK sequence number in the TCP packet retransmission path

Disable

Enable

Need to enable this bit if user wants to run the bi-directional data transfer.

ext_tcp_ip_feature_bit_map[4]

EXT_TCP_IP_WINDOW_DIV

To enable TCP ACK division factor feature

Disable

Enable

This feature enable window divsion factor for tcp socket

ext_tcp_ip_feature_bit_map[5]

EXT_TCP_IP_CERT_BYPASS

Reserved.

ext_tcp_ip_feature_bit_map[6]

EXT_TCP_IP_SSL_16K_RECORD

Support for SSL/TLS 16K record size

Disable

Enable

When the TLS/SSL record size of Cloud Server is more than 8 KB, this feature should be enabled

ext_tcp_ip_feature_bit_map[7]

EXT_TCP_IP_DNS_CLIENT_BYPASS

To enable DNS_CLIENT_BYPASS by host

Disable

Enable

ext_tcp_ip_feature_bit_map[8]

EXT_TCP_IP_WINDOW_SCALING

To enable TCP window scaling feature

Disable

Enable

If this feature is not enabled, then the maximum possible rx window size is 64 KB. If user wants to use more than 64KB window size, tcp_rx_window_size_cap in rsi_socket_config() is used to increase the window size.

ext_tcp_ip_feature_bit_map[9]

EXT_TCP_IP_DUAL_MODE_ENABLE

To enable Dual Mode feature

Disable

Enable

Enabling this feature allows to use both bypass and non bypass modes simultaneously.

ext_tcp_ip_feature_bit_map[10]

EXT_TCP_IP_ETH_WIFI_BRIDGE

To enable Ethernet wifi bridge feature

Disable

Enable

This feature enable Ethernet wifi bridge feature

ext_tcp_ip_feature_bit_map[11]

EXT_DYNAMIC_COEX_MEMORY

To enable the dynamic coex memory

Disable

Enable

To enable or disable the coex and update TCP RX window accordingly.

ext_tcp_ip_feature_bit_map[12:15]

EXT_TCP_IP_TOTAL_SELECTS_1 EXT_TCP_IP_TOTAL_SELECTS_2 EXT_TCP_IP_TOTAL_SELECTS_3 EXT_TCP_IP_TOTAL_SELECTS_4 EXT_TCP_IP_TOTAL_SELECTS_5 EXT_TCP_IP_TOTAL_SELECTS_6 EXT_TCP_IP_TOTAL_SELECTS_7 EXT_TCP_IP_TOTAL_SELECTS_8 EXT_TCP_IP_TOTAL_SELECTS_9 EXT_TCP_IP_TOTAL_SELECTS_10

Configures the number of selects

Disable

Enable

This feature allows Configure the number of selects modules

ext_tcp_ip_feature_bit_map[16]

EXT_TCP_IP_WAIT_FOR_SOCKET_CLOSE

To enable socket wait close

Disable

Enable

If it is set socket will not be closed until the shutdown is called from host. Refer to rsi_shutdown(). It is recommended to enable this bit when using TCP sockets.

ext_tcp_ip_feature_bit_map[17]

EXT_EMB_MQTT_ENABLE

To enable MQTT feature

Disable

Enable

If user wants to use AT command for MQTT, enable this bit in the Opermode Command

ext_tcp_ip_feature_bit_map[18]

EXT_TCP_IP_FEAT_SSL_HIGH_PERFORMANCE

To enable HTTP OTAF Feature

Disable

Enable

To do firmware upgrade with HTTP this bit should be enabled

ext_tcp_ip_feature_bit_map[19:28]

-

Reserved

ext_tcp_ip_feature_bit_map[29]

EXT_TCP_IP_FEAT_SSL_THREE_SOCKETS

Enable three SSL/TLS sockets

Disable

Enable

Set tcp_ip_feature_bit_map[31] and ext_tcp_ip_feature_bit_map[29] to open 3 TLS sockets

ext_tcp_ip_feature_bit_map[30]

EXT_TCP_IP_FEAT_SSL_MEMORY_CLOUD

To configure additional memory for SSL/TLS connection typically to a cloud server

Disable

Enable

If user connects to a cloud server using two SSL/TLS connections then it is required to set this bit to avoid 0xD2 error

ext_tcp_ip_feature_bit_map[31]

CONFIG_FEAT_EXTENTION_VALID

config_feature_bit_map validity

Disable

Enable


Note!

  1. The three SSL/TLS socket feature is only supported in Opermode WLAN.

  2. The total number of TLS sockets opened includes sockets opened by the host application and internal sockets.


RSI_BT_FEATURE_BITMAP#

This bitmap is valid only if BIT[31] of extended custom feature bit map is set to 1.

bt_feature_bit_map

Macro defined in SAPI

Functionality

Set to 0

Set to 1

Additional Notes

bt_feature_bit_map[0]

BT_BDR_MODE_ENABLE

BT Mode Enable

Disable

Enable

This feature enables or disables the BT mode. If this bit is set, the controller will send/receive packets in 1Mbps mode. Otherwise, the controller will be operable in both BR/EDR mode.

bt_feature_bit_map[1]

BT_BDR_MODE_LP_CHAIN_ENABLE

BT Mode LP Chain Enable

Disable

Enable

bt_feature_bit_map[2]

BT_PWR_CTRL

BT Power Control Disable

Enable

Disable

To make Fixed/Adaptive Power

bt_feature_bit_map[3:7]

Not defined

Reserved

bt_feature_bit_map[8]

BT_EDR_3MBPS_DISABLE

BT EDR 3Mbps Feature Disable

Enable

Disable

3Mbps Disable means using 2Mbps DataRate

bt_feature_bit_map[9]

BT_EDR_2MBPS_DISABLE

BT EDR 2Mbps Feature Disable

Enable

Disable

2Mbps Disable means using 3Mbps DataRate

bt_feature_bit_map[10]

BT_5_SLOT_PACKETS_DISABLE

BT 5 Slot Packet Feature Disable

Enable

Disable

Disabling 5 Slot Packets

bt_feature_bit_map[11]

BT_3_SLOT_PACKETS_DISABLE

BT 3 Slot Packet Feature Disable

Enable

Disable

Disabling 3 Slot Packets

bt_feature_bit_map[12]

Not defined

Noise Figure Feature

Disable

Enable

Note! This feature is not supported in the current release

bt_feature_bit_map[13]

Not defined

SNIFF Feature Disable

Enable

Disable

Note! This feature is not supported in the current release

bt_feature_bit_map[14]

TA_BASED_ENCODER_ENABLE

TA based encoder

Disable

Enable

To Enable/Disable SBC Encoder in Firmware. Note! This feature is not supported in the current release

bt_feature_bit_map[15]

Not defined

HFP profile bit enable

Disable

Enable

Note! This feature is not supported in the current release

bt_feature_bit_map[16:19]

Not defined

Reserved for future use

bt_feature_bit_map[20:22]

Not defined

number of secondaries supported by BT

Maximum no of bt secondaries : 1

bt_feature_bit_map[23]

A2DP_PROFILE_ENABLE

A2DP profile bit enable

Disable

Enable

bt_feature_bit_map[24]

A2DP_SOURCE_ROLE_ENABLE

A2DP profile role selection

Disable

Enable

bt_feature_bit_map[25]

A2DP_ACCELERATOR_MODE_ENABLE

A2DP accelerated mode selection

Disable

Enable

Note! This feature is not supported in the current release

bt_feature_bit_map[26]

Not defined

A2DP i2s mode selection

Disable

Enable

Note! This feature is not supported in the current release

bt_feature_bit_map[27]

BT_BLE_CP_BUFF_SIZE

enable Buffer Alignment for Test Mode

Disable

Enable

This feature enables buffer alignment for Test Mode. By enabling this feature, the bt_feature_bit_map[27] and BT_BLE_CP_BUFF_SIZE will be modified to allow obtaining 512 bytes from the common pool. If this feature is disabled, the fixed buffer size will be 320 bytes.

bt_feature_bit_map[28]

Not defined

Reserved

bt_feature_bit_map[29]

Not defined

Att Over Classic Enable

Disable

Enable

Note! This feature is not supported in the current release

bt_feature_bit_map[30]

BT_RF_TYPE

RF Type selection

Disable

Enable

Enable to use Internal Antenna and Disable to use External Antenna

bt_feature_bit_map[31]

ENABLE_BLE_PROTOCOL

ble_feature_bit_map is valid only when this bit is set

Disable

Enable

This macro is used to enable the BLE (Bluetooth Low Energy) protocol

RSI_BLE_FEATURE_BIT_MAP#

This bitmap is valid only if BIT[31] of bt_feature_bit_map is set.

ble_feature_bit_map

Macro defined in SAPI

Functionality

Set to 0

Set to 1

Additional Notes

ble_feature_bit_map[0:7]

RSI_BLE_MAX_NBR_ATT_REC

BLE number of attributes

The maximum number of BLE attributes is 124, refer NOTE given below for more info

ble_feature_bit_map[8:11]

RSI_BLE_MAX_NBR_ATT_SERV

BLE number of GATT services

The maximum number of services is 10, refer NOTE given below for more info

ble_feature_bit_map[12:15]

RSI_BLE_MAX_NBR_SLAVES

BLE number of peripherals

The maximum number of BLE peripherals is 8, refer NOTE given below for more info

ble_feature_bit_map[16:23]

RSI_BLE_PWR_INX

BLE Tx power index

Sets the BLE Tx power index value. Default value for BLE Tx Power Index is 31.Range for the BLE Tx Power Index is 1 to 127 (0, 32 index is invalid).1 - 31: BLE - 0dBm Mode, 33 - 63: BLE - 10dBm Mode, 64 - 127: BLE - HP Mode.

ble_feature_bit_map[24:26]

RSI_BLE_PWR_SAVE_OPTIONS

BLE powersave options BLE_DISABLE_DUTY_CYCLING(0) BLE_DUTY_CYCLING BIT(24) BLR_DUTY_CYCLING BIT(25) BLE_4X_PWR_SAVE_MODE BIT(26)

Default BLE_DISABLE_DUTY_CYCLING**Note!** This feature is not supported in the current release

ble_feature_bit_map[27:28]

RSI_BLE_MAX_NBR_MASTERS

Number of Masters

The maximum number of BLE Masters is 2. refer to the note below for more info.

ble_feature_bit_map[29]

RSI_BLE_GATT_ASYNC_ENABLE

GATT ASYNC BIT

Disable

Enable

Default is disabled. When enabled, the response structure will be filled in the Event, which will come later, not in sync with the response for the query command.

ble_feature_bit_map[30]

Not defined

Reserved

Disable

Enable

ble_feature_bit_map[31]

ble_custom_ext_feature_bit_map is valid only when this bit is set

Disable

Enable

RSI_BLE_CUSTOM_EXT_FEATURE_BIT_MAP#

This bitmap is valid only if BIT[31] of ble_feature_bit_map map is set.

ble_custom_ext_feature_bit_map

Macro defined in SAPI

Functionality

Set to 0

Set to 1

Additional Notes

ble_custom_ext_feature_bit_map[0:4]

RSI_BLE_NUM_CONN_EVENTS

BLE number of Connection Events

Describes the number of buffers that need to be allocated for BLE on the opermode.By default, each role (central/peripheral) will be allocated with 1 buffer for the notify/write command.Increasing the buffer capacity for the notify/write commands helps achieve the best throughput. See rsi_ble_set_wo_resp_notify_buf_info() to set more buffers for the notify/write commands.

ble_custom_ext_feature_bit_map[5:12]

RSI_BLE_NUM_REC_BYTES

BLE number of record size in bytes (n)

Specifies the number of record bytes in multiples of 16.**Note!** n*16 : (n=60, Default 1024 bytes(1K))

ble_custom_ext_feature_bit_map[13]

RSI_BLE_GATT_INIT

GATT INIT( GATT initialization mode)

- 0 : GATT Init in Firmware. Both the GAP service and GATT service will be maintained by the firmware. 1: GATT Init in Host. The GAP service and GATT service should be created by the APP/Host/User, and the ATT transactions like read, write, notify, and indicate shall be handled by the APP/Host/User Default : GATT Init in Firmware

ble_custom_ext_feature_bit_map[14]

RSI_BLE_INDICATE_CONFIRMATION_FROM_HOST

Indication response from APP

Disable

Enable

Default Disabled Note! As per the ATT protocol, every indication received from the server should be acknowledged (indication response) by the client.If this bit is disabled, the firmware will send the acknowledgment (indication response).If this bit is enabled, the APP/Host/User needs to send the acknowledgment (indication response).

ble_custom_ext_feature_bit_map[15]

RSI_BLE_MTU_EXCHANGE_FROM_HOST

MTU Exchange request initiation from APP

Disable

Enable

Default Disabled. - If this bit is disabled, the firmware will initiate the MTU request to the remote device on a successful connection. If the peer initiates an MTU exchange request, the firmware will send an Exchange MTU Response in reply to the received Exchange MTU Request.If this bit is enabled, the APP/Host/User needs to initiate the MTU request using the rsi_ble_mtu_exchange_event API.If the peer initiates an MTU exchange request, the APP/Host/User shall send an Exchange MTU Response using the rsi_ble_mtu_exchange_resp API.

ble_custom_ext_feature_bit_map[16]

RSI_BLE_SET_SCAN_RESP_DATA_FROM_HOST

Set SCAN Resp Data from APP

Disable

Enable

Default Disabled .The device will maintain some default scan response data to be used in the scan_response controller frame.Enabling this bit will make the default data Null (empty).

ble_custom_ext_feature_bit_map[17]

RSI_BLE_DISABLE_CODED_PHY_FROM_HOST

Disable Coded PHY from APP

Disable

Enable

Default Disabled. The device supports the LE-coded PHY feature (i.e., LR - 125kbps and 500kbps) by default.If this bit is enabled, the device will not support the LE-coded PHY rates.

ble_custom_ext_feature_bit_map[18:31]

Not defined

Reserved


Note! If bt_feature_bit_map[31] = 1:

  1. User can enter maximum of 8 BLE peripherals.

  2. User can enter maximum of 2 BLE centrals.

  3. Maximum of 10 services in total can exist out of which two services namely GAP and GATT are added by default. So if this bitmap has value 10 user can add upto 8 services.

  4. Maximum of 124 attributes in total can exist out of which nine attributes of GAP and GATT are added by default. So if this bitmap has value 124 user can add upto 115 attributes.

  5. RSI_BLE_NUM_CONN_EVENTS >= RSI_BLE_MAX_NBR_SLAVES + RSI_BLE_MAX_NBR_MASTERS.

If bt_feature_bit_map[31] = 0:

  1. Default number of BLE peripherals supported is 3.

  2. Default number of BLE centrals supported is 1.

  3. Maximum of 5 services in total can exist out of which two services namely GAP and GATT are added by default. So user can add upto 3 services.

  4. Maximum of 20 attributes in total can exist out of which ten attributes of GAP and GATT are added by default. So user can add upto 10 attributes.


RSI_CONFIG_FEATURE_BITMAP#

This bitmap is valid only if ext_tcp_ip_feature_bit_map[31] is set.

config_feature_bit_map

Macro defined in SAPI

Functionality

Set to 0

Set to 1

Note and info

config_feature_bit_map[0]

RSI_FEAT_SLEEP_GPIO_SEL_BITMAP

To select wakeup indication to host. If it is disabled UULP_GPIO_3 is used as a wakeup indication to host. If it is enabled UULP_GPIO_0 is used as a wakeup indication to host.

Disable

Enable

config_feature_bit_map[5:2]

RSI_FEAT_DVS_SEL_CONFIG_1 RSI_FEAT_DVS_SEL_CONFIG_2 RSI_FEAT_DVS_SEL_CONFIG_3 RSI_FEAT_DVS_SEL_CONFIG_4

Dynamic Voltage SelectionDynamic Voltage Selection

These bits are used for dynamic voltage selection

config_feature_bit_map[9:6]

RSI_EXTERNAL_PMU_GOOD_TIME_100us RSI_EXTERNAL_PMU_GOOD_TIME_200us RSI_EXTERNAL_PMU_GOOD_TIME_300us RSI_EXTERNAL_PMU_GOOD_TIME_400us RSI_EXTERNAL_PMU_GOOD_TIME_500us RSI_EXTERNAL_PMU_GOOD_TIME_600us RSI_EXTERNAL_PMU_GOOD_TIME_700us RSI_EXTERNAL_PMU_GOOD_TIME_800us RSI_EXTERNAL_PMU_GOOD_TIME_900us RSI_EXTERNAL_PMU_GOOD_TIME_1000us RSI_EXTERNAL_PMU_GOOD_TIME_1100us RSI_EXTERNAL_PMU_GOOD_TIME_1200us RSI_EXTERNAL_PMU_GOOD_TIME_1300us RSI_EXTERNAL_PMU_GOOD_TIME_1400us RSI_EXTERNAL_PMU_GOOD_TIME_1500us

External Pmu Good TimeExternal Pmu Good Time

These bits are used to select external PMU good time.1 to 15 means 100usec to 1500usec (in 100usec granularity)

config_feature_bit_map[11:10]

RSI_FEAT_EXTERNAL_LDO_SEL BIT RSI_FEAT_EXTERNAL_LDO_VOL

External LdoExternal Ldo

These bits are used for External LDO selection External PMU : 1.In case of External PMU, User has to set EXTERNAL_PMU_GOOD_TIME_CONFIGURATION value to external PMU good time, If this is zero then it indicates using Internal PMU. 2. Incase of External PMU 1.0v or 1.05v, User has to set both the bits config_feature_bit_map[11] & config_feature_bit_map[10].

config_feature_bit_map[13:12]

Not defined

Uulp Gpio 0Uulp Gpio 0

If these bits are not set, then by default UULP_GPIO_0 will be used.

config_feature_bit_map[14]

RSI_FEAT_EAP_TLS_V1P0

To select EAP TLS 1.0 version

Disable

Enable

config_feature_bit_map[15]

RSI_FEAT_EAP_TLS_V1P2

To select EAP TLS 1.2 version

Disable

Enable

config_feature_bit_map[16]

Not defined

Active high or low interrupt mode selection for wake on wireless operation If it is disabled active low interrupt is used in wake on wireless operation. If it is enabled active high interrupt is used in wake on wireless operation.

Disable

Enable

config_feature_bit_map[17]

FEAT_CONC_STA_AP_DYN_SWITCH_SEL

Reserved

config_feature_bit_map[18]

ULP_GPIO9_FOR_UART2_TX

To select ULP_GPIO_9 as UART2 port for device network processor debug prints

Disable

Enable

If this bit is not set, then by default UART2-TX GPIO_6 will be used.

config_feature_bit_map[19]

RSI_FEAT_DISABLE_MCS_5_6_7_DATARATES

To disable MCS-5,6,7 data rates

Disable

Enable

config_feature_bit_map[20]

RSI_FEAT_DISABLE_SHORT_GI

To disable Short-GI

Disable

Enable

config_feature_bit_map[21]

PTA_3WIRE_EN

To enable PTA-3WIRE

Disable

Enable

Should be set to enable and use the PTA 3 wire feature followed by available configurations

config_feature_bit_map[23:22]

PTA_3WIRE_CONFIG_SEL

To choose PTA-3WIRE config1 config2 config3

Configurability options for config selection among 1,2 & 3

Pta 3wire OptionsPta 3wire Options
0 kept reserved for future. 3wire used at dut as ULP_GPIO_0(Grant pin driven by dut), ULP_GPIO_1(Request i/p pin for dut) and ULP_GPIO_6(Priority i/p pin for dut)
Pta 3wire Options DefPta 3wire Options Def

config_feature_bit_map[25:24]

RSI_XTAL_GOODTIME_1000us RSI_XTAL_GOODTIME_2000us RSI_XTAL_GOODTIME_3000us RSI_XTAL_GOODTIME_600us

Configurability options for 40 MHz XTAL good time in us.

Xtal Good TimeXtal Good Time

These bits are used to select XTAL good time. These changes are available from Release 2.3.0 onwards. Release prior to 2.3.0 these config_feature_bitmap[31:17] are reserved. Its only applicable for customers using chip not the device. Contact Support for more details Default value is 1000 us.

config_feature_bit_map[26]

ENABLE_ENHANCED_MAX_PSP

To enable Enhanced Max PSP

Disable

Enable

Enabling this and setting psp_type to Fast PSP will enable Enhanced Max PSP.

config_feature_bit_map[31:27]

-

Reserved for LMAC


Note! 32KHz external clock connection and power save pins

From May 2019, the 32KHz external clock and the power save pins connections changed. To keep software compatibility between initial designs and new designs, there are currently 2 options for connecting the 32KHz external clock and the power save pins:

Option 1 External 32KHz clock connection pins : XTAL_32KHZ_P & XTAL_32KHZ_N Power Save connection pins : HOST_BYP_ULP_WAKEUP & UULP_VBAT_GPIO_3

Option 2 External 32KHz clock connection pin : UULP_VBAT_GPIO_3 Power Save connection pins : HOST_BYP_ULP_WAKEUP & UULP_VBAT_GPIO_0

Option 2 must be used for External 32KHz external clock and Power save connections in new designs.


Other Configuration Parameters#

Scan Parameters#

Macro

Usage

RSI_SCAN_CHANNEL_BIT_MAP_2_4

To select channels in 2.4GHz band for selective channel scan. This macro is valid only if channel 0 is selected in rsi_wlan_scan API.

RSI_SCAN_CHANNEL_BIT_MAP_5

To select channels in 5GHz band to do selective channel scan. This macro is valid only if channel 0 is selected in rsi_wlan_scan API.

RSI_SCAN_FEAT_BITMAP

RSI_ENABLE_QUICK_SCAN - If enabled, module scans for the AP given in scan API and posts the scan results immediately to the host after finding the access point.
This bit is valid only if specific channel and ssid to scan is given.
RSI_SCAN_RESULTS_TO_HOST - if enabled additional scan results are given to host, but after getting scan results host has to issue another scan request with this bit disabled before join.

AP Mode Parameters#

Macro

Usage

RSI_AP_KEEP_ALIVE_ENABLE

To Enable keep alive functionality in AP mode.

RSI_AP_KEEP_ALIVE_TYPE

RSI_NULL_BASED_KEEP_ALIVE – To perform keep alive by sending Null data packet to stations
RSI_DEAUTH_BASED_KEEP_ALIVE – To perform keep alive based on packets received from stations within time out.

RSI_AP_KEEP_ALIVE_PERIOD

To configure keep alive period.

RSI_MAX_STATIONS_SUPPORT

To configure maximum stations supported.

Radio_Config Parameters#

Description#

These parameters are used in rsi_send_feature_frame API to select internal RF type or external RF type and clock frequency.

pll_mode (1 byte)

  • 0 - PLLMODE. To run Network Processor (NWP) at 80 MHz Clock frequency.

  • 1 - PLLMODE. To run Network Processor (NWP) at 120/160 MHz Clock frequency.

  • 2 - PLLMODE. Reserved

Note!

rf_type (1 byte)

  • 1 - Internal RF (Reserved). This should always be set to 1.

wireless_mode (1 byte)

  • 0 - LP chain disable (default)

  • 12 - Enable LP chain for PER mode

enable_ppp (1 byte)

  • Always set to 0 (Reserved).

afe_type (1 byte)

  • 1 - Internal AFE (Reserved). This should always be set to 1.

feature_enables (4 bytes)

  • BIT[0] - To Enable Preamble duty cycling.

  • BIT[4] - To Enable LP chain.

  • BIT[5] - To Enable hardware beacon drop.

  • Above 3 parameters are valid only in Standby Associated Power Save mode.

  • BIT[1] to BIT[3] and BIT[6] to BIT[31] are not user configurable


Note!

- 40 MHz bandwidth is not supported.#

US Domain Regulations#

Rule No

Band

First Channel

#channels

Last Channel

Max power in dBm

Scan type

1

2.4GHz

1

11

11

27

Active

2

5GHz

36

4

48

16

Active

3

5GHz

52

4

64

23

Passive

4

5GHz

100

5

116

23

Passive

5

5GHz

132

3

140

23

Passive

6

5GHz

149

5

165

29

Active

Europe Domain Regulations#

Rule No

Band

First Channel

#channels

Last Channel

Max power in dBm

Scan type

1

2.4GHz

1

13

13

20

Active

2

5GHz

36

4

48

23

Active

3

5GHz

52

4

64

23

Passive

4

5GHz

100

10

140

30

Passive

5

5GHz

149

5

165

13

Active

Japan Domain Regulations#

Rule No

Band

First Channel

#channels

Last Channel

Max power in dBm

Scan type

1

2.4GHz

1

13

13

20

Active

2

5GHz

36

4

48

20

Active

3

5GHz

52

4

64

20

Passive

4

5GHz

100

10

140

30

Passive

Korea Domain Regulations#

Rule No

Band

First Channel

#channels

Last Channel

Max power in dBm

Scan type

1

2.4GHz

1

13

13

20

Active

2

5GHz

36

4

48

20

Active

3

5GHz

52

4

64

20

Passive

4

5GHz

100

11

140

30

Passive

5

5GHz

149

5

165

30

Active

Set Region Parameters#

Macro

Usage

RSI_SET_REGION_SUPPORT

Enable to send set region command during Wi-Fi client connection.

RSI_SET_REGION_FROM_USER_OR_BEACON

1 - region configurations taken from user.
0 - region configurations taken from beacon.

RSI_REGION_CODE

0 - Default Region domain
1 - US
2 - EUROPE
3 - JAPAN
4 - WORLDWIDE
5 - KOREA


Note!

  • The UNII-3 band(Rule No:5) specified in the Europe domain regulation table is not supported in RS9116 1.3 silicon(M7DB6) Dual Band modules.

  • For RS9116AC0 and RS9116AC1 module as STA :-

    • Region configuration from user is not allowed.

    • In 2.4GHz, USA is configuerd as default country domain and in addition to this, channels 12 and 13 are passively scanned.

    • Country inforamtion is updated as per connecting AP's beacon before authentication.

    • Upon disconnection with the AP, STA will switch to USA domain along with channels 12 and 13 are passively scanned.

    • While doing passive scan (channel 12 and 13) if any beacon is found in that channel STA will switch to active scan.

- If there is no country IE in the beacon of the AP to which STA is going to connect, STA will switch to USA/EU country based on the channel in which the AP exists. For example if the AP in channel between 1 to 11, STA will configure to USA else if the current channel number is 12 or 13 STA will be configured to EU.#

Set Region AP Parameters#

Macro

Usage

RSI_SET_REGION_AP_SUPPORT

Enable to send set region AP command during AP start.

RSI_SET_REGION_AP_FROM_USER

1 - region configurations taken from user.
0 - region configurations taken from firmware.

RSI_COUNTRY_CODE

Country code which is supposed to be in Upper case. If the first parameter is 1, the second parameter should be one of the these 'US','EU','JP','KR' country codes


Note!

  • If the country code's length is two characters, then the 3rd character should be a <space>.

  • If the region configurations are taken from user, The UNII-3 band(Rule No:5) specified in the Europe domain regulation table is not applied in RS9116 1.3 silicon(M7DB6) Dual Band modules.

  • For RS9116AC0/RS9116AC1 module as AP:-

    • In AP alone mode USA is configured as default country.

- In concurrent mode, country domain is configured to that of AP's country domain to which the STA has connected.#

Rejoin Parameters#

Macro

Usage

RSI_REJOIN_PARAMS_SUPPORT

Enable to send rejoin parameters command during Wi-Fi client connection.

RSI_REJOIN_MAX_RETRY

To set number of retries to be attempted.
Note:
If this macro is 0, rejoin is retried infinite times.

RSI_REJOIN_SCAN_INTERVAL

To set periodicity of rejoin attempt.
Note:
Rejoin scan interval is in seconds.

RSI_REJOIN_BEACON_MISSED_COUNT

To set the number of beacons missed before triggering rejoin process.
Note:
Default beacon missed count is 40.
A unicast probe request will be sent from the midpoint of the given beacon missed count.
For example, if the beacon count is 40, the unicast probe request will be sent from the module to the AP at the midpoint, which is the 21st beacon. This will also occur at the 31st beacon count.

RSI_REJOIN_FIRST_TIME_RETRY

ENABLE or DISABLE retry for the first time join failure.


Note!

- By default, the rejoin feature is turned off. However, it will still be triggered once, even when disabled.#

| RSI_REJOIN_SCAN_INTERVAL| To set periodicity of rejoin attempt.| | RSI_REJOIN_BEACON_MISSED_COUNT| To set the number of beacons missed before triggering rejoin process.| | RSI_REJOIN_FIRST_TIME_RETRY | ENABLE or DISABLE retry for the first time join failure.
Note:
Recommended to enable RSI_REJOIN_FIRST_TIME_RETRY to minimize join failures, especially in scenarios such as abnormal connection termination caused by a module reset.|

BG Scan Parameters#

Macro

Usage

RSI_BG_SCAN_SUPPORT

Enable to send BG scan command after Wi-Fi client connection.

RSI_BG_SCAN_ENABLE

To enable or disable BG Scan.

RSI_INSTANT_BG

Enable or disable instant BG scan.

RSI_BG_SCAN_THRESHOLD

This is the threshold in dBm to trigger the BG scan.

RSI_RSSI_TOLERANCE_THRESHOLD

This is the minimum difference between the last RSSI of connected AP and the current RSSI of connected AP to trigger a BG scan irrespective of BG scan periodicity.
Here, last RSSI is the RSSI calculated at the last beacon received and current RSSI is the RSSI calculated at current beacon received.

RSI_BG_SCAN_PERIODICITY

To set the periodicity of BG scan in seconds.

RSI_ACTIVE_SCAN_DURATION

This is the active scan duration per channel in milli seconds.

RSI_PASSIVE_SCAN_DURATION

This is the passive scan duration per DFS channel in 5GHz in milli seconds.

RSI_MULTIPROBE

If it is set to one, then module will send two probe request - one with specific SSID provided during join command and other with NULL SSID (to scan all the access points).

Roaming Parameters#

Macro

Usage

RSI_ROAMING_SUPPORT

Enable to send roaming command after Wi-Fi client connection.

RSI_ROAMING_THRESHOLD

If connected AP, RSSI falls below this then module will search for new AP from background scanned list.

RSI_ROAMING_HYSTERISIS

If module found new AP with same configuration (SSID, Security etc) and if (connected_AP_RSSI – Selected_AP_RSSI ) is greater than RSI_ROAMING_HYSTERISIS then it will try to roam to the new selected AP.


Note!

  1. WLAN - RS9116 supports Wi-Fi L2 roaming.

  2. Selection of 'sending de authentication' or 'informing Power save' to the connected AP while roaming can be done by CUSTOM_FEAT_ROAM_WITH_DEAUTH_OR_NULLDATA flag in RSI_CUSTOM_FEATURE_BIT_MAP bitmap. By default de authentication will be sent.


HT capabilities#

Macro

Usage

RSI_MODE_11N_ENABLE

Enable to send Ht capabilities command during AP start.

RSI_HT_CAPS_BIT_MAP

Bit map corresponding to high throughput capabilities.
ht_caps_bit_map[10:15]: All set to '0'
ht_caps_bit_map[8:9]:Rx STBC support
00- Rx STBC support disabled
01- Rx STBC support enabled
ht_caps_bit_map[6:7]: Set to '0'
ht_caps_bit_map[5]: short GI for 20Mhz support
0- short GI for 20Mhz support disabled
1- short GI for 20Mhz support enabled
ht_caps_bit_map[4]: Green field support
0 -Green field support disabled
1 -Green field support enabled
ht_caps_bit_map[0:3]:Set to '0'

Enterprise Mode Parameters#

Macro

Usage

RSI_EAP_METHOD

Should be one among TLS, TTLS, FAST or PEAP. It should be ASCII character string.

RSI_EAP_INNER_METHOD

This field is valid only in TTLS/PEAP. In case of TTLS/PEAP, the supported inner methods are MSCHAP/MSCHAPV2.
In case of TLS/FAST, it should be fixed to MSCHAPV2.

Join Parameters#

Macro

Usage

RSI_POWER_LEVEL

This fixes the Transmit Power level of the module. This value can be set as follows:
At 2.4GHz
0– Low power (7+/-1) dBm
1– Medium power (10 +/-1) dBm
2– High power (18 + /- 2) dBm
At 5 GHz
0– Low power (5+/-1) dBm
1– Medium power (7 +/-1) dBm
2– High power (12 +/- 2) dBm

RSI_JOIN_FEAT_BIT_MAP

BIT[0]: To enable b/g only mode in station mode, host has to set this bit.
0 – b/g/n mode enabled in station mode.
1 – b/g only mode enabled in station mode
BIT[1]: To take listen interval from join command.
0 – Listen interval invalid
1 – Listen interval valid
BIT[2]: To enable/disable quick join feature.
1 - To enable quick join feature.
0 - To disable quick join feature.
BIT[3]: Set this bit enable CCXV2 extension for client to work with cisco APs.
BIT[4]: Host sets this bit to join an AP based on BSSID.
BIT[5]: Host sets this bit to enable Management Frame Protection Capable feature.
BIT[6]: Set this bit to enable Management Frame Protection Required feature.
BIT[7]: To configure listen interval from rsi_wlan_power_save_with_listen_interval SAPI.

RSI_JOIN_FEAT_BIT_MAP_AP

This feature bit map is for AP join parameters in Concurrent mode only. The bit map description is same as RSI_JOIN_FEAT_BIT_MAP

RSI_LISTEN_INTERVAL

This is valid only if BIT (1) in join_feature_bit_map is set. This value is given in Time units (1024 microsecond). This parameter is used to configure maximum sleep duration in power save.

RSI_DATA_RATE

To select Auto or Fixed data rate. Recommended to use Auto rate.
RSI_DATA_RATE_AUTO: Auto rate

Curve IDs Supported#

Curve ID

Description

Support

15

secp160k1

Yes

16

secp160r1

Yes

17

secp160r2

Yes

18

secp192k1

Yes

19

secp192r1

Yes

20

secp224k1

Yes

21

secp224r1

Yes

22

secp256k1

Yes

23

secp256r1

Yes

24

secp384r1

Yes

25

secp521r1

Yes

26

brainpoolP256r1

Yes

27

brainpoolP384r1

Yes

28

brainpoolP512r1

Yes

Power Save Parameters#

Macro

Usage

RSI_HAND_SHAKE_TYPE

To set handshake type of power mode MSG_BASED/GPIO_BASED

RSI_SELECT_LP_OR_ULP_MODE

0 - LP, 1- ULP mode with RAM retention and 2 - ULP without RAM retention

RSI_DTIM_ALIGNED_TYPE

set DTIM alignment required
0 - module wakes up at beacon which is just before or equal to listen_interval.
1 - module wakes up at DTIM beacon which is just before or equal to listen_interval.

RSI_MONITOR_INTERVAL

Monitor interval for the FAST PSP mode.
Default is 50 ms, and this parameter is valid for FAST PSP only.

RSI_WMM_PS_ENABLE

To set wmm enable or disable.

RSI_WMM_PS_TYPE

To set wmm type
0 - TX BASED
1 - PERIODIC

RSI_WMM_PS_WAKE_INTERVAL

To set wmm wake up interval.

RSI_WMM_PS_UAPSD_BITMAP

To set wmm UAPSD bitmap

RSI_NUM_OF_DTIM_SKIP

If this macro is n then module will wake up at (n+1)th DTIM.

Configure 10 TCP Sockets when Device is in AP mode#

Macro

Usage

HIGH_PERFORMANCE_ENABLE

To make RSI_ENABLE or RSI_DISABLE high performance sockets.

TOTAL_SOCKETS

To Set total number of Sockets - TCP_TX + TCP_RX + UDP_TX + UDP_RX
10 - To Open 10 Sockets in total

TOTAL_TCP_SOCKETS

To Set total TCP Sockets - TCP_TX + TCP_RX
10 - To open 10 TCP Sockets

TOTAL_UDP_SOCKETS

To Set total UDP Sockets
0 - Disable
1 - Enable

TCP_TX_ONLY_SOCKETS

To Set total TCP TX only Sockets - TCP TX

TCP_RX_ONLY_SOCKETS

To Set TCP RX only Sockets - TCP RX
10 - To Open 10 TCP_RX sockets

UDP_TX_ONLY_SOCKETS

To Set UDP TX only Sockets - UDP TX
0 - Disable
1 - Enable

UDP_RX_ONLY_SOCKETS

To Set UDP RX only Sockets - UDP RX
0 - Disable
1 - Enable

TCP_RX_HIGH_PERFORMANCE_SOCKETS

To Set TCP_RX high performance Sockets
10 - To open 10 TCP_RX_HIGH_PERFORMANCE_SOCKETS

TCP_RX_WINDOW_SIZE_CAP

To Set TCP RX window size
10 - To make the TCP RX window size to 10

TCP_RX_WINDOW_DIV_FACTOR

To Set TCP_RX window division factor
10 - To make TCP RX window division factor to 10

RSI_NUMBER_OF_LTCP_SOCKETS

To Set the number of LTCP sockets
10 - To open 10 LTCP sockets

RSI_NUMBER_OF_SOCKETS

Default number of Sockets supported. Set this to, 10 + RSI_NUMBER_OF_LTCP_SOCKETS

Note! Need to call rsi_socket_config API to configure the above parameters. Used to increase the TCP receive window based on available buffers

IP Parameters#

Macro

Usage

RSI_DHCP_HOST_NAME

Define this macro in config file to set DHCP client host name - A 31-byte string

Chip Version#

User can get the chip version using the rsi_mem_rd API by reading one byte of data at the address 0x04000437 into the buffer pointed by *buf. rsi_mem_rd(0x04000437, 1, buf)

Chip version

Read data

1.3

0x13

1.4

0x14

1.5

0x15

SSL/TLS Version#

  • If BSD_COMPATIBILITY is defined then SSL/TLS version can be chosen using rsi_setsockopt() API option_name parameter.

    • The option_name passes SO_SSL_ENABLE to open an SSL/TLS connection over TCP socket. By default supports versions of both TLS 1.0 and TLS 1.2

    • When the user wants to open an SSL/TLS connection over TCP socket with TLS version 1.0, they should use the SO_SSL_V_1_0_ENABLE macro.

    • When the user wants to open an SSL/TLS connection over TCP socket with TLS version 1.1, they should use the SO_SSL_V_1_1_ENABLE macro.

    • When the user wants to open an SSL/TLS connection over TCP socket with TLS version 1.2, they should use the SO_SSL_V_1_2_ENABLE macro.

  • In case if the BSD_COMPATIBILITY is not defined, add rsi_socket() protocol parameter is used to choose TLS versions

    • The protocol passes PROTOCOL_DFLT_VERSION to open an SSL/TLS connection over TCP socket. By default supports versions of both TLS 1.0 and TLS 1.2.

    • When the user wants to open an SSL/TLS connection over TCP socket with TLS version 1.0, they should use the PROTOCOL_TLS_1_0 macro.

    • When the user wants to open an SSL/TLS connection over TCP socket with TLS version 1.1, they should use the PROTOCOL_TLS_1_1 macro.

    • When the user wants to open an SSL/TLS connection over TCP socket with TLS version 1.2, they should use the PROTOCOL_TLS_1_2 macro.