You are viewing documentation for version:2.15.0 (latest)Public Attributes#uint32_tiduint16_tchar_set_iduint16_tattr_text_lenuint8_tatt_textPublic Attribute Documentation#id#uint32_t idSpecifies the attribute/Value ID to be written char_set_id#uint16_t char_set_idSpecifies the character set ID to be displayed on CT attr_text_len#uint16_t attr_text_lenLength of the player application setting attribute/Value string att_text#uint8_t att_text[31]Specifies the player application setting attribute/Value string in specified character set.