You are viewing documentation for version:2.15.0 (latest)Public Attributes#uint32_tiduint16_tchar_set_iduint16_tattr_lenuint8_tattr_valPublic Attribute Documentation#id#uint32_t idSpecifies the attribute ID to be written char_set_id#uint16_t char_set_idSpecifies the character set ID to be displayed on CT attr_len#uint16_t attr_lenLength of the value of the attribute attr_val#uint8_t attr_val[50]Attribute Name in specified character set Limiting to 50 bytes