You are viewing documentation for version:2.15.0 (latest)Public Attributes#uint8_tdev_addr_typeuint8_tdev_addruint16_tle_scan_intervaluint16_tle_scan_windowuint16_tconn_interval_minuint16_tconn_interval_maxuint16_tconn_latencyuint16_tsupervision_toutPublic Attribute Documentation#dev_addr_type#uint8_t dev_addr_typedev_addr#uint8_t dev_addr[RSI_DEV_ADDR_LEN]le_scan_interval#uint16_t le_scan_intervalle_scan_window#uint16_t le_scan_windowconn_interval_min#uint16_t conn_interval_minconn_interval_max#uint16_t conn_interval_maxconn_latency#uint16_t conn_latencysupervision_tout#uint16_t supervision_tout