Public Attribute Documentation#
scan_type#
uint8_t scan_type
Scanning type
#define SCAN_TYPE_ACTIVE 0x01
#define SCAN_TYPE_PASSIVE 0x00
filter_type#
uint8_t filter_type
To filter incoming advertising reports
FILTERING_DISABLED = 0 (default)
ACCEPTLIST_FILTERING = 1 Note
In order to allow only acceptlisted devices, need to add bd_addr into acceptlist by calling rsi_ble_addto_acceptlist() API
own_addr_type#
uint8_t own_addr_type
Address type of the local device
#define LE_PUBLIC_ADDRESS 0x00
#define LE_RANDOM_ADDRESS 0x01
#define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02
#define LE_RESOLVABLE_RANDOM_ADDRESS 0x03
scan_int#
uint16_t scan_int
Scan interval
This is defined as the time interval from when the Controller started its last LE scan until it begins the subsequent LE scan.
Range: 0x0004 to 0x4000
scan_win#
uint16_t scan_win
Scan window
The duration of the LE scan. LE_Scan_Window shall be less than or equal to LE_Scan_Interval
Range: 0x0004 to 0x4000