Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
union rsi_rsp_socket_create_s::@37
union rsi_rsp_socket_create_s::@38
uint8_t

Public Attribute Documentation#

ip_version#

uint8_t ip_version[2]

socket_type#

uint8_t socket_type[2]

socket_id#

uint8_t socket_id[2]

module_port#

uint8_t module_port[2]

dst_port#

uint8_t dst_port[2]

ipv4_addr#

uint8_t ipv4_addr[4]

ipv6_addr#

uint8_t ipv6_addr[16]

module_ip_addr#

union rsi_rsp_socket_create_s::@37 module_ip_addr

dest_ip_addr#

union rsi_rsp_socket_create_s::@38 dest_ip_addr

mss#

uint8_t mss[2]

window_size#

uint8_t window_size[4]