You are viewing documentation for version:2.15.0 (latest)Public Attributes#uint8_tsock_iduint8_tsock_typeuint8_tsource_portuint8_tdest_portuint8_tipv4_addressuint8_tipv6_addressunion rsi_sock_info_query_s::@44dest_ip_addressPublic Attribute Documentation#sock_id#uint8_t sock_id[2]sock_type#uint8_t sock_type[2]source_port#uint8_t source_port[2]dest_port#uint8_t dest_port[2]ipv4_address#uint8_t ipv4_address[4]ipv6_address#uint8_t ipv6_address[16]dest_ip_address#union rsi_sock_info_query_s::@44 dest_ip_address