Low Power Standby Associated Station and BLE Advertising Tera Term Script#

This application demonstrates the procedure about how to configure the RS9116W Module in coex mode (WLAN STA + BLE)mode and putting module in low power (WLAN standby associated) state and ble connected power save.

Connecting the RS9116 EVK to your PC to the perform current measurements#

To do this you will perform the following:

  1. Connect the EVK’s UART port to your PC using the included USB A to USB Micro cable.

  2. Connect the EVK to your current meter through its “MEASUREMENT” port.

Note: To measure lowest possible power, it is recommended to use UART to issue commands. It allows device to go to its lowest power states. USB-CDC keeps the USB port alive, and USB is not a low power interface.

Your current meter’s positive and negative terminals should be connected as shown in the picture below. This picture also shows the connection of the USB cable between your PC and the EVK board

Tera Term MacroTera Term Macro

Performing the current measurement#

Before continuing, ensure the RS9116 EVK is plugged into your computer and TeraTerm is connected as described in Getting Started with PC using AT Commands.

After doing so, start your current meter in continuous DC current measurement mode with a range of 1 A.

As an example, the Keithley DMM6500 current meter was used. It is set as shown below using its PC-based Kickstart interface software.

Tera Term MacroTera Term Macro

Running the Example#

STEP 1. Reset the RS9116 EVK.

STEP 2. In the Tera Term menu select Control->Macro.

Tera Term MacroTera Term Macro

STEP 3. Navigate to the folder <SDK>/examples/at_commands/teraterm/wlan_low_power_with_ble and select the file low_power_station_with_ble.ttl.

Tera Term Script to be selectedTera Term Script to be selected

STEP 4. Opermode command configures the module as Wi-Fi Station and BLE operating mode. The module responds with “OK” & “bt_loaded”.

at+rsi_opermode=851968,20,2147483652,2147483648,2159542272,3221225472,2147483648,1075773440,0,1

Opermode command successOpermode command success

STEP 5. Feat_frame command configures to use LP chain in standby associcated mode. Feat_frame Successful pop will come and you confirm by selecting “OK”

Feature frame command successFeature frame command success

Now Module will be configured to start BLE advertising using following commands. Once success, observe the pop up “Device is now advertising as a RS9116W_BLE.....". You can use Silabs "EFR Connect" Mobile app to check for the same.

1. Set Local Name

2. Get a local BD address.

3. Set Advertise Data

4. Advertise command.

BLE AdvertiseBLE Advertise

STEP 7. Now we configure the WLAN Station starting with the 2.4GHz band configuration and the module responds with “OK”.

Band successBand success

STEP 8. at+rsi_init command initializes the RF of the module. The module responds with OK<MAC_Address> (can be seen in Hex)

init command successinit command success

STEP 9. Pop up comes to provide input for SSID of the AP to be connected, select 'OK' to proceed (make sure SSID is entered correectly),

at+rsi_scan=0,Silicon_labs

This command scans for particular Access Point operating in all channels. The module responds with information of the Access Points scanned.

The data received might have some unreadable characters because of ASCII conversion.

SSID input promptSSID input prompt

STEP 10. Once “scan successful” comes, select “OK”.

Scan successScan success

STEP 11. Next pop up asks for pre shared key (PSK) input from the user, enter the PSK of desired Access Point and hit 'OK',

PSK Input promptPSK Input prompt

STEP 12.

at+rsi_join=Silicon_labs,0,2,6

This command connects the Wi-Fi client to the Access Point with SSID "Silicon_labs”. On successful association, the module responds with OK.

AP join successAP join success

STEP 13. After join successful next command will get the IP address from the DHCP server running on AP.

at+rsi_ipconf=1

ipconfig successipconfig success

STEP 14. After successfully getting the IP address module can now enter in low power mode (Standby Associated Mode). Power save success pop up will come. Go with "ok" response.

Power save successPower save success

User can now measure the power consumption if power meter is connected on EVK Jumper J19 "Measurement".