Snippet Examples#
Snippet examples are small projects that demonstrate one particular RS9116 feature or API.  The snippet examples are found in the WiSeConnectâ„¢ SDK at the path:  <SDK>/examples/snippets and are categorized by the feature that they demonstrate.
Details on the configuration and operation of each snippet example are available in the readme.md file that is found with the example source code and at the following links:
BLE Examples#
ble-central
ble-datalength
ble-dual-role
ble-heart-rate-profile
ble-ibeacon
ble-longrange-2mbps
ble-multiconnection-gatt-test
ble-power-save
ble-privacy
ble-secureconnection
ble-white-list
ble-hid-on-gatt
Bluetooth Examples#
bt-power-save
bt-spp-dual-role-with-secure-pairing
Dual Mode Bluetooth Examples#
bt-ble-dual-mode
bt-ble-update-gain-table
Debug Utility Examples#
Wi-Fi Examples#
wlan-access-point
wlan-calibration-app
wlan-device-shadow-logging-stats
wlan-aws-iot-mqtt
wlan-azure-iot
wlan-concurrent-mode
wlan-embedded-mqtt
wlan-enterprise-client
wlan-ftp-client
wlan-http-otaf
wlan-mqtt-client
wlan-power-save-deep-sleep
wlan-socket-select-app
wlan-station-ping
wlan-tcp-logging-stats
wlan-three-ssl-concurrent-client-sockets
wlan-tls-client
Wi-Fi + BLE Examples#
wlan-station-ble-bridge
wlan-station-ble-provisioning
wlan-station-ble-provisioning-AWS
Wi-Fi + Dual Mode Bluetooth Examples#
wlan-https-bt-spp-ble-dual-role
wlan-throughput-bt-spp-ble-dual-role