Common APIs#
Functions#
Set the device BD address. This is blocking API.
Enable and disable BER. This is blocking API.
Set the given name to local device. This is blocking API.
Update gain table offset/max power. This is blocking API.
Get the local device name. This is blocking API.
Get the RSSI of the remote device. This is blocking API.
Get the local device address. This is blocking API.
Get the BT stack version. This is blocking API.
Initialize the BT device. This is blocking API.
Deinitialize the BT device. This is blocking API.
Select either internal / external antenna on the chip. This is blocking API.
Enable/Disable the mentioned features. This is blocking API.
Select the power save profile mode for BT / BLE. This is blocking API.
Function Documentation#
rsi_bt_set_bd_addr#
int32_t rsi_bt_set_bd_addr (uint8_t * dev_addr)
Set the device BD address. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | dev_addr | - public address of the device to be set |
needs to be called immediately after rsi_wireless_init() OPERMODE command.
Returns
0 - Success
Non-Zero Value - Failure
-3 - Command is given in wrong state(i.e not immediate after opermode)
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_ber_enable_or_disable#
int32_t rsi_bt_ber_enable_or_disable (struct rsi_bt_ber_cmd_s * ber_cmd)
Enable and disable BER. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| struct rsi_bt_ber_cmd_s * | [in] | ber_cmd | - pointer address which contains the command structure. Please refer rsi_bt_ber_cmd_s structure for more info |
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_set_local_name#
int32_t rsi_bt_set_local_name (uint8_t * local_name)
Set the given name to local device. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | local_name | - Name to be set to the local device. |
rsi_wireless_init() API need to be called before this API.
Note
For BLE alone Opermode : When the name of the local device is set to a value with length more than 16 bytes then error is returned with an error code 0x4E66.
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_cmd_update_gain_table_offset_or_max_pwr#
int32_t rsi_bt_cmd_update_gain_table_offset_or_max_pwr (uint8_t node_id, uint8_t payload_len, uint8_t * payload, uint8_t req_type)
Update gain table offset/max power. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | node_id | - Node ID (0 - BLE, 1 - BT). |
| uint8_t | [in] | payload_len | - Length of the payload. |
| uint8_t * | [in] | payload | - Payload containing table data of gain table offset/max power |
| uint8_t | [in] | req_type | - update gain table request type (0 - max power update, 1 - offset update) |
rsi_wireless_init() API need to be called before this API.
Note
This API is applicable for High performance(HP) mode only.
Returns
0 - Success
0x4F01 - Invalid gain table payload length
0x4F02 - Invalid region.
0x4F03 - Invalid gain table offset request type
0x4F04 - Invalid node id.
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_get_local_name#
int32_t rsi_bt_get_local_name (rsi_bt_resp_get_local_name_t * bt_resp_get_local_name)
Get the local device name. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| rsi_bt_resp_get_local_name_t * | [out] | bt_resp_get_local_name | - This parameter is the response buffer to hold the response of this API. Please refer rsi_bt_resp_get_local_name_s structure for more info. |
rsi_wireless_init() API need to be called before this API.
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_get_rssi#
int32_t rsi_bt_get_rssi (uint8_t * dev_addr, int8_t * resp)
Get the RSSI of the remote device. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | dev_addr | - Remote device address. |
| int8_t * | [out] | resp | - Parameter to hold the response of this API, rssi is filled in this resp parameter. |
rsi_bt_connect() API need to be called before this API.
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_get_local_device_address#
int32_t rsi_bt_get_local_device_address (uint8_t * resp)
Get the local device address. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | resp | - Parameter to hold the response of this API, local bd_addr is filled in this resp parameter. |
rsi_wireless_init() API needs to be called before this API.
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_get_bt_stack_version#
int32_t rsi_bt_get_bt_stack_version (rsi_bt_resp_get_bt_stack_version_t * bt_resp_get_bt_stack_version)
Get the BT stack version. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| rsi_bt_resp_get_bt_stack_version_t * | [out] | bt_resp_get_bt_stack_version | - Response buffer to hold the response of this API. Please refer rsi_bt_resp_get_bt_stack_version_s structure for more info |
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_init#
rsi_bt_init (void )
Initialize the BT device. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
rsi_wireless_init() API needs to be called before this API.
If the device is in powersave, get back the device to ACTIVE MODE by using rsi_bt_power_save_profile()
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_deinit#
rsi_bt_deinit (void )
Deinitialize the BT device. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
rsi_wireless_init() API needs to be called before this API.
If the device is in powersave, get back the device to ACTIVE MODE by using rsi_bt_power_save_profile()
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_set_antenna#
int32_t rsi_bt_set_antenna (uint8_t antenna_value)
Select either internal / external antenna on the chip. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | antenna_value | - Parameter is used to select either internal or external antenna. Possible values: |
rsi_wireless_init() API needs to be called before this API.
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_set_antenna_tx_power_level#
int32_t rsi_bt_set_antenna_tx_power_level (uint8_t protocol_mode, int8_t tx_power)
Enable/Disable the mentioned features. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | protocol_mode | - protocol mode |
| int8_t | [in] | tx_power | - power value |
rsi_wireless_init() API need to be called before this API
Note
The default value will vary based on country region and board
Returns
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes Error Codes .
rsi_bt_power_save_profile#
int32_t rsi_bt_power_save_profile (uint8_t psp_mode, uint8_t psp_type)
Select the power save profile mode for BT / BLE. This is blocking API.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | psp_mode | Following psp_mode is defined. |
| uint8_t | [in] | psp_type | Following psp_type is defined. |
rsi_wireless_init() API needs to be called before this API
Returns
0 - Success
Non-Zero Value - Failure
Note
If the user wants to enable power save in CoEx mode (WLAN + BT LE) mode - It is mandatory to enable WLAN power save along with BT LE power save.
The device will enter into power save if and only if both protocol (WLAN, BLE) power save modes are enabled.
Refer Error Codes section for above error codes Error Codes .
psp_type is only valid in psp_mode 2.
BT/BLE doesnot support in RSI_SLEEP_MODE_1.
BT/BLE supports only RSI_MAX_PSP mode. Remaining modes are not supported.