Snippet Examples#
Snippet examples are small projects that demonstrate one particular RS9116 feature or API. The snippet examples are found in the WiSeConnectâ„¢ SDK at the path: <SDK>/examples/snippets and are categorized by the feature that they demonstrate.
Details on the configuration and operation of each snippet example are available in the readme.md file that is found with the example source code and at the following links:
Wi-Fi + BLE Examples#
wlan-station-ble-provisioning-AWS
wlan-station-ble-bridge
wlan-station-ble-provisioning
Debug Utility Examples#
Wi-Fi Examples#
wlan-access-point-v6
wlan-power-save-deep-sleep
wlan-concurrent-mode
wlan-ftp-client
wlan-station-ping
wlan-socket-select-app
wlan-enterprise-client
wlan-station-ping-v6
wlan-mqtt-client
wlan-http-client-v6
wlan-http-otaf
wlan-mqtt-client-v6
wlan-calibration-app
wlan-tcp-logging-stats
wlan-throughput-v6
wlan-three-ssl-concurrent-client-sockets
wlan-access-point
wlan-aws-iot-mqtt
wlan-device-shadow-logging-stats
wlan-azure-iot
wlan-tls-client
wlan-sntp-client-v6
wlan-embedded-mqtt
Wi-Fi + Dual Mode Bluetooth Examples#
wlan-throughput-bt-spp-ble-dual-role
wlan-https-bt-spp-ble-dual-role
BLE Examples#
ble-central
ble-ibeacon
ble-multiconnection-gatt-test
ble-hid-on-gatt
ble-dual-role
ble-power-save
ble-white-list
ble-secureconnection
ble-privacy
ble-longrange-2mbps
ble-datalength
ble-heart-rate-profile
Dual Mode Bluetooth Examples#
bt-ble-update-gain-table
bt-ble-dual-mode