WLAN Station BLE Provisioning with AWS cloud#

1. Purpose / Scope#

This example demonstrates how to configure/connects RS9116W EVK to get the WLAN connection functionality using BLE provisioning. In this application, the Module starts advertising and with BLE Provisioning the Access Point details are fetched

The RS9116W EVK module is configured as a station, which associates to an access point and then communicates with an AWS server using MQTT. Data will be continuously published until the device is disconnected from the access point.

2. Prerequisites / Setup Requirements#

Before running the application, the user will need the following things to setup.

2.1 Hardware Requirements#

  • Windows PC with Host interface (UART / SPI).

  • Silicon labs RS9116 Wi-Fi Evaluation Kit

  • Host MCU Eval Kit. This example has been tested with:

  • Wireless Access point

  • Android Mobile Phone with Silicon labs Connect App.

    (or)

  • Windows PC with windows Silicon labs connect application.

Setup diagram of WLAN Station BLE Provisioning with AWS cloud

2.2 Software Requirements#

  • WiSeConnect SDK

  • Embedded Development Environment

  • User can install any of the below apps to verify WLAN Station BLE Provisioning.

    1. Install Android based Silicon labs Connect APK:

    • Access the apk provided in the path: <SDK>/utilities/Silicon_lab_connectApp.apk

    1. Install windows Silicon labs connect application in laptop.

    • Refer the application provided in the path: <SDK>/utilities/windows_ble_provisioning_app

    • Follow the instructions provided in the document: <SDK>/utilities/windows_ble_provisioning_app/Installation_steps_to_run_silabs_connect_windows_application.docx

3. Application Build Environment#

3.1 Platform#

The Application can be built and executed on below Host platforms

3.2 Host Interface#

  • By default, the application is configured to use the SPI bus for interfacing between Host platforms and the RS9116W EVK.

  • The SAPI driver provides APIs to enable other host interfaces if SPI is not suitable for your needs.

3.3 Project Configuration#

The Application is provided with the project folder containing Keil and Simplicity Studio project files.

  • Keil Project:

    • The Keil project can be executed on STM32 platform.

    • Project path: <SDK>/examples/snippets/wlan_ble/wlan_station_ble_provisioning_AWS/projects/wlan_station_ble_provisioning_AWS-nucleo-f411re.uvprojx

  • Simplicity Studio:

    • The Simplicity Studio project can be executed on EFR32MG21.

    • Project path:

      • If the Radio Board is BRD4180A or BRD4181A, then access the path <SDK>/examples/snippets/wlan_ble/wlan_station_ble_provisioning_AWS/projects/wlan_station_ble_provisioning_AWS/projects-brd4180a-mg21.slsproj

      • If the Radio Board is BRD4180B or BRD4181B, then access the path <SDK>/examples/snippets/wlan_ble/wlan_station_ble_provisioning_AWS/projects/wlan_station_ble_provisioning_AWS/projects-brd4180b-mg21.slsproj

      • User can find the Radio Board version as given below

EFR Radio Boards

3.4 Bare Metal Support#

This application supports only bare metal configuration. By default, the application project files (Keil and Simplicity Studio) are provided with bare metal environment in the SDK.

4. Application Configuration Parameters#

The application can be configured to suit your requirements and development environment. Read through the following sections and make any changes needed.

4.1 Open rsi_wlan_app.c file and update/modify following macros

Modify the MQTT topics and give different names for both topics RS9116 is subscribed to MQTT_TOPIC1 and publishing to MQTT_TOPIC2. MQTT web application is subscribed to MQTT_TOPIC2 and publishing on MQTT_TOPIC1.

#define MQTT_TOPIC1           "$aws/things/SmartLockWebApp-v01/shadow/update/device_status"
#define MQTT_TOPIC2           "$aws/things/SmartLockWebAppv01/shadow/update/delta/temperature_reading"

NOTE: If you would like to change the topic names, then you can modify only the last keyword of the topic, which are device_status and temperature_reading.

To configure the IP address

Memory length for driver

#define GLOBAL_BUFF_LEN                          15000

Memory length for the send buffer

#define BUF_SIZE                                 1400

The following parameters are configured if OS is used. WLAN task should be of low priority

#define RSI_WLAN_TASK_PRIORITY                   1

Driver task should have the highest priority among all threads

#define RSI_DRIVER_TASK_PRIORITY                 4

WLAN Task stack size is configured by this macro

#define RSI_WLAN_TASK_STACK_SIZE                 500

Driver Task stack size is configured by this macro

#define RSI_DRIVER_TASK_STACK_SIZE               500

4.1.1 Open rsi_wlan_config.h file and update/modify the following macros

#define CONCURRENT_MODE                          RSI_DISABLE
#define RSI_FEATURE_BIT_MAP                      (FEAT_SECURITY_OPEN  | FEAT_AGGREGATION | FEAT_ULP_GPIO_BASED_HANDSHAKE)
#define RSI_TCP_IP_BYPASS                        RSI_DISABLE 
#define RSI_TCP_IP_FEATURE_BIT_MAP               (TCP_IP_FEAT_DHCPV4_CLIENT | TCP_IP_FEAT_SSL | TCP_IP_FEAT_DNS_CLIENT | TCP_IP_TOTAL_SOCKETS_1 | TCP_IP_FEAT_EXTENSION_VALID)
#define RSI_CUSTOM_FEATURE_BIT_MAP               FEAT_CUSTOM_FEAT_EXTENTION_VALID
#define RSI_EXT_CUSTOM_FEATURE_BIT_MAP           (EXT_FEAT_384K_MODE | EXT_FEAT_LOW_POWER_MODE | EXT_FEAT_RSA_KEY_WITH_4096_SUPPORT | EXT_FEAT_SSL_CERT_WITH_4096_KEY_SUPPORT)  
define RSI_EXT_TCPIP_FEATURE_BIT_MAP             ( EXT_DYNAMIC_COEX_MEMORY | EXT_TCP_IP_FEAT_SSL_MEMORY_CLOUD | CONFIG_FEAT_EXTENTION_VALID)    
define RSI_CONFIG_FEATURE_BITMAP                 RSI_FEAT_SLEEP_GPIO_SEL_BITMAP 
define RSI_BT_FEATURE_BITMAP                     (BT_RF_TYPE | ENABLE_BLE_PROTOCOL)
define RSI_BAND                                  RSI_BAND_2P4GHZ 

Note: rsi_wlan_config.h file is already set with the desired configuration in respective example folders, user need not change for each example.

4.2 Open rsi_ble_app.c file and update/modify following macros

Configuring the BLE Application

RSI_BLE_CHAR_SERV_UUID refers to the attribute type of the characteristics to be added in a service.

#define  RSI_BLE_CHAR_SERV_UUID                         0x2803

RSI_BLE_CLIENT_CHAR_UUID refers to the attribute type of the client characteristics descriptor to be added in a service.

#define RSI_BLE_CLIENT_CHAR_UUID                        0x2902

RSI_BLE_NEW_SERVICE_UUID refers to the attribute value of the newly created service.

#define  RSI_BLE_NEW_SERVICE_UUID                       0xAABB

RSI_BLE_ATTRIBUTE_1_UUID refers to the attribute type of the first attribute under this service (RSI_BLE_NEW_SERVICE_UUID).

#define  RSI_BLE_ATTRIBUTE_1_UUID                        0x1AA1

RSI_BLE_ATTRIBUTE_2_UUID refers to the attribute type of the second attribute under this service (RSI_BLE_NEW_SERVICE_UUID).

#define RSI_BLE_ATTRIBUTE_2_UUID                         0x1BB1

RSI_BLE_ATTRIBUTE_3_UUID refers to the attribute type of the third attribute under this service (RSI_BLE_NEW_SERVICE_UUID).

#define RSI_BLE_ATTRIBUTE_3_UUID                         0x1CC1

RSI_BLE_MAX_DATA_LEN refers to the Maximum length of the attribute data.

#define RSI_BLE_MAX_DATA_LEN                               20

RSI_BLE_APP_DEVICE_NAME refers to the name of the Silicon Labs device to appear during scanning by remote devices.

#define  RSI_BLE_APP_DEVICE_NAME               "BLE_CONFIGURATOR"

The following are the non-configurable macros in the application.

RSI_BLE_ATT_PROPERTY_READ is used to set the READ property to an attribute value.

#define  RSI_BLE_ATT_PROPERTY_READ                    0x02

RSI_BLE_ATT_PROPERTY_WRITE is used to set the WRITE property to an attribute value.

#define RSI_BLE_ATT_PROPERTY_WRITE                       0x08

RSI_BLE_ATT_PROPERTY_NOTIFY is used to set the NOTIFY property to an attribute value.

#define  RSI_BLE_ATT_PROPERTY_NOTIFY                      0x10

BT_GLOBAL_BUFF_LEN refers to the number of bytes required by the application and the driver.

#define  BT_GLOBAL_BUFF_LEN                              15000

4.3 Open aws_iot_config.h file and change the AWS_IOT_MQTT_CLIENT_ID to your choice (Make sure this is unique, if more than one user use has same client id it might get conflict at server side).

  //AWS Host name 
  #define AWS_IOT_MQTT_HOST          "a25jwtlmds8eip-ats.iot.us-east-2.amazonaws.com"  

  //default port for MQTT
  #define AWS_IOT_MQTT_PORT          "8883"
  
  #define AWS_IOT_MQTT_CLIENT_ID     "Redp"
  
  // Thing Name of the Shadow this device is associated with 
  #define AWS_IOT_MY_THING_NAME      "AWS-IoT-C-SDK"    

4.4 To Load Certificate

rsi_wlan_set_certificate() API expects the certificate in the form of linear array. Convert the pem certificate into linear array form using python script provided in the SDK <SDK>/resources/certificates/certificate_script.py.

For example : If the certificate is ca-certificate.pem, enter the command in the following way: python certificate_script.py ca-certificate.pem The script will generate ca-certificate.pem.h in which one linear array named ca-certificate contains the certificate. Root CA certificate, Device private key and Device client certificate needs to be converted as mentioned above

After the conversion, place the converted files in <SDK>/resources/certificates/ path and include the certificate files in rsi_wlan_app.c

Replace the default Device certificate and Private key certificate include in the application with the converted pem file name.

// Certificate includes
#include "aws_client_certificate.pem.crt.h"
#include "aws_client_private_key.pem.key.h"

Replace the default Device certificate and Private key certificate given in `rsi_wlan_set_certificate()` API in the application with the converted pem array.

// Load Security Certificates
status = rsi_wlan_set_certificate(RSI_SSL_CLIENT, aws_client_certificate, (sizeof(aws_client_certificate) - 1));

status =
rsi_wlan_set_certificate(RSI_SSL_CLIENT_PRIVATE_KEY, aws_client_private_key, (sizeof(aws_client_private_key) - 1));

NOTE : For AWS connectivity, StarField Root CA Class 2 certificate has the highest authority being at the top of the signing hierarchy.

The StarField Root CA Class 2 certificate is an expected/required certificate which usually comes pre-installed in the operating systems and it plays a key part in certificate chain verification when a device is performing TLS authentication with the IoT endpoint.

On RS9116 device, we do not maintain root CA trust repository due to memory constraints, so it is mandatory to load StarField Root CA Class 2 certificate for successful mutual authentication to AWS server.

The certificate chain sent by AWS server is as below: id-at-commonName=Amazon,id-at-organizationalUnitName=Server CA 1B,id-at-organizationName=Amazon,id-at-countryName=US id-at-commonName=Amazon Root CA 1,id-at-organizationName=Amazon,id-at-countryName=US id-at-commonName=Starfield Services Root Certificate Authority ,id-at-organizationName=Starfield Technologies, Inc.,id-at-localityName=Scottsdale,id-at- stateOrProvinceName=Arizona,id-at-countryName=US)

On RS9116 to authenticate the AWS server, firstly Root CA is validated (validate the Root CA received with the Root CA loaded on the device). Once the Root CA is validation is successful , other certificates sent from the AWS server are validated. RS9116 don't authenticate to AWS server if intermediate CA certificates are loaded instead of StarField Root CA Class 2 certificate and would result in Handshake error. StarField Root CA Class 2 certificate is at https://certs.secureserver.net/repository/sf-class2-root.crt

Reference links : https://aws.amazon.com/blogs/security/how-to-prepare-for-aws-move-to-its-own-certificate-authority/

5. Testing the Application#

Follow the below steps for the successful execution of the application.

5.1 Loading the RS9116W Firmware#

Refer Getting started with PC to load the firmware into RS9116W EVK. The firmware binary is located in <SDK>/firmware/

5.2 Building the Application on the Host Platform#

5.2.1 Using STM32#

Refer STM32 Getting Started

  • Open the project <SDK>/examples/snippets/wlan_ble/wlan_station_ble_provisioning_AWS/projects/wlan_station_ble_provisioning_AWS-nucleo-f411re.uvprojx in Keil IDE.

  • Build and Debug the project

  • Check for the RESET pin:

    • If RESET pin is connected from STM32 to RS9116W EVK, then user need not press the RESET button on RS9116W EVK before free run.

    • If RESET pin is not connected from STM32 to RS9116W EVK, then user need to press the RESET button on RS9116W EVK before free run.

  • Free run the project

  • Then continue the common steps from Section 5.3

5.2.2 Using EFX32#

Refer EFx32 Getting Started

  • Import the project from <SDK>/examples/snippets/wlan_ble/wlan_station_ble_provisioning_AWS/projects

  • Select the appropriate .slsproj as per Radio Board type mentioned in Section 3.3

  • Compile and flash the project in to Host MCU

  • Debug the project

  • Check for the RESET pin:

    • If RESET pin is connected from EFX32 to RS9116W EVK, then user need not press the RESET button on RS9116W EVK before free run

    • If RESET pin is not connected from EFX32 to RS9116W EVK, then user need to press the RESET button on RS9116W EVK before free run

  • Free run the project

  • Then continue the common steps from Section 5.3

5.3 Execution of AWS IoT with BLE Provisioning#

5.3.1 BLE Provisioning with Windows Application#

  1. Configure the Access point with internet connection in OPEN/WPA-PSK/WPA2-PSK mode to connect the RS9116W EVK in STA mode.

  2. Connect any serial console for prints.

    Note Turn on BT in the PC.

  3. Go to folder <SDK>/utilities/windows_ble_provisioning_app and Run Silabs_Connect.py in the command prompt.

  4. Executing the application in the command prompt as stated in the above point will open the GUI (with the “BLE SCAN ON� button.

Silicon labs connect GUI

  1. Check for the configured name in the BLE scanned list and connect to the ‘SILABS_BLE_CONFIGURATOR’, by clicking on it.

Silicon labs BLE Configurator

  1. Once the BLE connection is successful, Wi-Fi access points scan list will be populated. Click on the Access Point (AP) SSID and enter the password of the AP, to which you would like to connect.

 Silicon labs Wi-Fi access points

Note Now go to section 5.3.3 MQTT connection for AWS connection

5.3.2 BLE Provisioning with Android Application#

  1. Silicon Labs Connect app is available in the <SDK>/utilities/ folder. Currently, this app will be available for Android devices only.

  2. Once the application gets executed, launch the Android application which you have already installed on Android mobile.

  3. Click on BLE Provisioning.

BLE Provisioning BLE connect app

  1. It will scan for the RS9116 module, and it appears in the list. For example, “SILABS_BLE_Configurator� on the UI, select this.

Module appears in the list

  1. Now, RS9116 module will start as a station and scan for the access points (AP) nearby.

  2. Once the list of AP scan results is displayed on the screen, you can select the SSID of the AP to which you want to connect.

Module SSID

  1. Click on the SSID of the AP, enter “password� if the AP is in security mode. Click on “Connect� to associate with the access point.

  2. Once Silicon labs RS9116 module is connected to the access point, you can notice on the GUI as below.

Module Access

  1. This completes the BLE provisioning using Android application, next step is the MQTT communication.

5.3.3 MQTT Connection#

  1. Once MQTT connection completed , device subscribed to specific Topic and waits for data from the Cloud. if any data received through AWS cloud from subscribed clients, then module publishes temperature sensor reading to MQTT client in case of EFR32. While in case of STM32 random temperature readings ranges from 25-40 is published to MQTT client through AWS cloud.

  2. You can use any MQTT client and connect to the AWS cloud, for subscribe and publishing messages.

Module connected log

Compressed Debug Logging#

To enable the compressed debug logging feature please refer to Logging User Guide