Public Attributes#

uint32_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

clock#

uint32_t clock

LMAC timer BT Clock


tx_poll#

uint16_t tx_poll

Num of TXed POLLS


tx_null#

uint16_t tx_null

Num of TXed NULLS


rx_poll#

uint16_t rx_poll

Num of RXed POLLS


rx_null#

uint16_t rx_null

Num of RXed NULLS


dm1_pkt#

uint16_t dm1_pkt[2]

dm1_pkt[0] - Num of TXed dm1 Pkts
dm1_pkt[1] - Num of RXed dm1 Pkts


dm3_pkt#

uint16_t dm3_pkt[2]

dm3_pkt[0] - Num of TXed dm3 Pkts
dm3_pkt[1] - Num of RXed dm3 Pkts


dm5_pkt#

uint16_t dm5_pkt[2]

dm5_pkt[0] - Num of TXed dm5 Pkts
dm5_pkt[1] - Num of RXed dm5 Pkts


dh1_pkt#

uint16_t dh1_pkt[2]

dh1_pkt[0] - Num of TXed dh1 Pkts
dh1_pkt[1] - Num of RXed dh1 Pkts


dh3_pkt#

uint16_t dh3_pkt[2]

dh3_pkt[0] - Num of TXed dh3 Pkts
dh3_pkt[1] - Num of RXed dh3 Pkts


dh5_pkt#

uint16_t dh5_pkt[2]

dh5_pkt[0] - Num of TXed dh5 Pkts
dh5_pkt[1] - Num of RXed dh5 Pkts


edr_2dh1_pkt#

uint16_t edr_2dh1_pkt[2]

2dh1_pkt[0] - Num of TXed 2dh1 Pkts
2dh1_pkt[1] - Num of RXed 2dh1 Pkts


edr_2dh3_pkt#

uint16_t edr_2dh3_pkt[2]

2dh3_pkt[0] - Num of TXed 2dh3 Pkts
2dh3_pkt[1] - Num of RXed 2dh3 Pkts


edr_2dh5_pkt#

uint16_t edr_2dh5_pkt[2]

2dh5_pkt[0] - Num of TXed 2dh5 Pkts
2dh5_pkt[1] - Num of RXed 2dh5 Pkts


edr_3dh1_pkt#

uint16_t edr_3dh1_pkt[2]

3dh1_pkt[0] - Num of TXed 3dh1 Pkts
3dh1_pkt[1] - Num of RXed 3dh1 Pkts


edr_3dh3_pkt#

uint16_t edr_3dh3_pkt[2]

3dh3_pkt[0] - Num of TXed 3dh3 Pkts
3dh3_pkt[1] - Num of RXed 3dh3 Pkts


edr_3dh5_pkt#

uint16_t edr_3dh5_pkt[2]

3dh5_pkt[0] - Num of TXed 3dh5 Pkts
3dh5_pkt[1] - Num of RXed 3dh5 Pkts


no_of_crc_fail#

uint16_t no_of_crc_fail

Num of CRC Failed Packets


no_of_retries#

uint16_t no_of_retries

Num of Retransmission Packets


no_of_hdr_err#

uint16_t no_of_hdr_err

Num of Header Error Packets


no_of_seq_repeat#

uint16_t no_of_seq_repeat

Num of Duplicate Packets Received
(If previous sequence number is received again)


ack_delay#

uint16_t ack_delay[11]

Num of ack packets received with delay of 10ms to 100ms and more that 100ms
10 - ack_delay[10] ......... >100 - ack_delay[10]


ack_received#

uint16_t ack_received

Num of ACK packets Received


nak_received#

uint16_t nak_received

Num of NAK packets Received


no_of_rx_missed#

uint16_t no_of_rx_missed

Num of missed response packets in the RX Slot


no_of_rx_error#

uint16_t no_of_rx_error

Num of RXed error packets in the RX Slot


tx_attempts#

uint16_t tx_attempts

Num of TX Attempts


tx_done#

uint16_t tx_done

Number of Packets TXed on Air